Post Go back to editing

LT1236 NC pin

Hi

According to LT1236 datasheet, NC pin is connected internally. Where NC pin is connected internally ? How much the resistance is between NC and GND ? The customer measured it. One is 1.82kohm another one is only 1.57ohm. What's happened the IC ?

As additional info, there is a capacitor between NC and GND on the pcb because they used MAX6250 on their old version pcb instead of LT1236. Does the capacitor cause any problem ?

Regards,

Hiroyuki

Edit Notes

write additional info.
[edited by: Hiroyuki.D at 1:46 AM (GMT 0) on 13 May 2019]