AD8436: FAQ

  • Created
  • Updated
Was this helpful?
  • AD8436 - Down conversion to 100 uV

    Question You advertise conversion down to 100μV. Why would anyone need this type of level? Answer As it happens, there are many applications for this kind of dynamic range. Safety protection includes…
  • AD8436 - Power consumption for added amplifiers

    Question What about power consumption for the added amplifiers? Answer In power-sensitive applications the amplifier power-supplies are simply disconnected, preserving the core conversion.
  • AD8436 - Power supply

    Question My hand-held meter project has only a battery for a power supply. Must I provide a separate negative power supply for the AD8436? Answer A unique feature is the ability of the AD8436 to operate…
  • AD8436 - What is unique about this device?

    Question What is unique about the AD8436? Answer It’s the first product of its type to incorporate buffers at the input and the output, in a single package. The value proposition is exceptional for this…
  • AD8436: output buffer with higher gain than unity

    Question Is it possible to use the output amplifier with higher gain than unity? Answer We tested the output buffer for gain > unity: We set up an eval board for G = 10. It works fine. We also established…
  • AD8436: single supply or dual supply

    Question Do you recommend to use AD8436 with single or dual supply? Answer The AD8436 is fully specified for dual supplies but will also operate over single supply range of 4V to 36V. It doesn’t matter…
  • EVAL-AD8436 evaluation board operation with single supply

    Question I have an AD8436 EVAL board and use it with single supply. The board does not work as expected. Have you any ideas why? Answer Please note, single supply operation requires removal of Resistor…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.