AD633: FAQ

  • Created
  • Updated
Was this helpful?
  • AD633 Vos drift over temperature

    Question What is the figure for the offset voltage drift of AD633? We have found such parameter shown in AD632 as below. Would you kindly offer this parameter to us if it is convenient. Answer We performed…
  • AD633: input coupling

    Question I have connected AD9850 and AD633 like in the attached diagram. AD9850 outputs 0-1000mV sine wave, and a 0.1uF capacitor is placed between AD9850 and AD633. The AD633 is powered by +-5V, and…
  • AD633: Operates with unsymmetrical power supply

    Question The transfer funciton with +-15V power supply is W=(x*Y)/10 +Z - Is the transfer function unaffected when operating with +-8V power supply ? e.g X=3V, Y=3V resulting in W=0.9V. What happens…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.