When Hot-Plug Detect (HPD) is low the HDMI Tx will automatically go into power down mode.
After an HPD interrupt, register 0x41[6] must be set to ‘0’ to power up the part
During power down all registers except for 0x97 – 0xAF are reset to defaults
- Most HDMI Tx devices (except AD9889, AD9389, AD9387, ADV7520, ADV7521) have an "HPD Override" function
- These devices will operate same as if HPD = 1 when HPD "override" is enabled
-
On the ADV7510, the registers will reset on an HPD = 1 -> 0 transition
- On the rest of these HDMI Tx devices the registers will not reset on an HPD = 1 -> 0 transition
-
-
HPD state and interrupt registers remain avaiable even of HPD Override is enabled
- These devices will operate same as if HPD = 1 when HPD "override" is enabled