Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

ADV7441A Design Support Files

Attached and linked are several files supporting the development of systems using the ADV7441A.

You can download zipped file collections.

We recommend that if you download and use these documents, you also subscribe to email notifications for either the entire forum or at least this FAQ by clicking on the menu to the right.  In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents.  If the menu choice is "Stop email notifications," then you are already subscribed.

File Content
PRODUCT SUPPORT
ADV7441A Product Page Link to Product Information Web Page
ADV7441A Datasheet Link to Product Shortform Datasheet
ADV7441A_HW_RevJ.pdf Hardware Design Manual
ADV7441A_SW_RevD.pdf Software Design Manual
ADV7441A_AD9388A_Setting_Recomendations_RevM.pdf Register setting recommendations for various operating modes
ADV7441A-AD9388A_Layout_Recommendations_RevA.pdf Layout considerations for the ADV7441A
ADV7441A_Rev0.1.ibs IBIS models of the ADV7441A I/O
ADV7441A EDID_Rev0.pdf Design considerations for the ADV7441A Internal EDID
ADV7441A_AD9388A_Investigation_Procedure_For_Audio_Issues_6_2_09.pdf Suggestions for investigating audio issues
EVALUATION BOARD SUPPORT
AD9388A_ADV7441A_Eval_Platform_Guide_RevA.pdf

Description of the ADV7441A/ADV9388A Evaluation Platform (requires ATV Motherboard)

ADV7441A_FrontEndBoard_QuickStart_Guide_Rev0.pdf Evaluation Platform QuickStart Guide
ADV7441A_Eval_Note_RevA.pdf Evaluation Platform Operating Manual
ADV7441A_ADV7441A@_ADV7441AVDP_ADV7441AHDMI_ADV7341-VER.MB2.0.TXT Scripts for the ATV Motherboard with Firmware 47.3 and Rev.B (AD9889B Output Module)
ADV7441A_ADV7441A@_ADV7441AVDP_ADV7441AHDMI_ADV7341-VER.MB3.0.TXT Scripts for the ATV Motherboard with Firmware 50.3 and Rev.E (ADV7511 Output Module)
AD9388A_ADV7441A_Front_End_Evaluation_Board_Rev.A_Layout.pdf Evaluation Board Layout
AD9388A_ADV7441A_Front_End_Evaluation_Board_Rev.A_Schematics.pdf Evaluation Board Schematics
AD9388A_ADV7441A Front End Evaluation Board - Rev. A - Gerber Files.zip Gerber files for ADV7441A Evaluation Board (revA)
     ADV7441A_Evaluation_Board_Documents.zip     ZIP file of the documents above
Comments
Anonymous
Parents
  • Hi,

    I'm using ADV7441A in my design with HDMI, VGA and component video inputs, I'm currently writting the software driver, but I'm not clear on the flow of the chip operation. For example, in my software, I want first know which port (e.g., HDMI or VGA) has video input, and what is the resolution and other parameters, but the sample code provided by ADV7441 seems that you should know everything then do the configurations, e.g., you should know the resolution is 1024x768 @ 65M from VGA, then configure the HDMI to that resolution. My question is for the receiver chip, the input resolution is unknow, how do you detect it? Does ADV7441A has some mechanism to detect it?

    Thanks!

    Sibing

Comment
  • Hi,

    I'm using ADV7441A in my design with HDMI, VGA and component video inputs, I'm currently writting the software driver, but I'm not clear on the flow of the chip operation. For example, in my software, I want first know which port (e.g., HDMI or VGA) has video input, and what is the resolution and other parameters, but the sample code provided by ADV7441 seems that you should know everything then do the configurations, e.g., you should know the resolution is 1024x768 @ 65M from VGA, then configure the HDMI to that resolution. My question is for the receiver chip, the input resolution is unknow, how do you detect it? Does ADV7441A has some mechanism to detect it?

    Thanks!

    Sibing

Children
Related