Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

ADV7802 Design Support Files

Attached and linked are several files supporting the development of systems using the ADV7802.

We recomment that, if you download and use these documents, you subscribe to Email notifications for either the entire forum or at least this post by selecting your preferred option from the the Actions -> Following In drop-down menu to the right. In this way, you will be automatically notified if there are any comments or changes to this post or attached documents.

File Content
ADV7802 Product Page Link to Product Page
ADV7802 Datasheet Link to ADV7802 Datasheet
Additional Support Documents
ADV7802_HW_RevB.pdf Hardware Manual (file attached below in ADV7800 Manuals.zip)
ADV7802_SW_RevC.pdf Software Manual (file attached below in ADV7800 Manuals.zip)
ADV7802_2D_only_operation.pdf

Guidelines for operating the ADV7802 in 2D mode without external memory

(file attached below)

ADV7802 Memory BIST test

Document listing a Built-in self test for memory interface

(file attached below)

IBIS Model
ADV7802.ibs Link to IBIS model
Evaluation Board Support

ADV7802ES2IO_ADV7802ES2SDP_ADV7802ES2CP_

ADV7802ES2VDP_ADV7341B-VER.3.03dDDR.txt

Scripts to run on the evaluation board with the DDR memory option

(file attached below in ADV7802 Evaluation Board Documents.zip)

ADV7802ES2IO_ADV7802ES2SDP_ADV7802ES2CP_

ADV7802ES2VDP_ADV7341B-VER.3.03dSDR.txt

Scripts to run on the evaluation board with the SDR memory option

(file attached below in ADV7802 Evaluation Board Documents.zip)

Comments
Anonymous
Parents
  • Hello,

    In the 2D only operation document, there is an example script at the end. However, the addresses are extremely strange for me. For example:

    54 17 02 ; Software Reset

    What is 54?! According to the SW manual there is no such address, but regarding the comment I would guess it is the I/O block, since that one has a "Resets" register, but then the next byte is 0x17 which should be 0x60 for the "Resets" address....

    Please correct me if I have a big mistake in my mind.

    Thank you very much in advance!

    Best Regards,

    Krisztian Bakos

Comment
  • Hello,

    In the 2D only operation document, there is an example script at the end. However, the addresses are extremely strange for me. For example:

    54 17 02 ; Software Reset

    What is 54?! According to the SW manual there is no such address, but regarding the comment I would guess it is the I/O block, since that one has a "Resets" register, but then the next byte is 0x17 which should be 0x60 for the "Resets" address....

    Please correct me if I have a big mistake in my mind.

    Thank you very much in advance!

    Best Regards,

    Krisztian Bakos

Children
Related