This FAQ applies to EVAL-ADV7842-7511 and EVAL-ADV7842-7511P. All support files in their latest versions will be attached below.
Below are the support files for these evaluation board. We recommend that, if you download and use these files, you subscribe to EMail notifications for either the entire forum or at least this FAQ by clicking on the menu to the right. In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.
| File | Content |
|---|---|
| UG-235 | User guide for this evaluation board. |
| EVAL-ADV7842-7511_rev1p2_schems_20140930.pdf | Schematics (in PDF format) for this evaluation board |
| EVAL-ADV7842-7511_rev1p2_schems_OrCAD_20140930.zip | Schematics (in OrCAD format) for this evaluation board |
| EVAL-ADV7842-7511_rev1p2_layout_Allegro_20110106.zip | Layout (in Allegro format) for this evaluation board |
| EVAL-ADV7842-7511_BOM_20140930.pdf | BOM (in PDF format) for the EVAL-ADV7842-7511 evaluation board. |
| EVAL-ADV7842-7511P_BOM_20140930.pdf | BOM (in PDF format) for the EVAL-ADV7842-7511P evaluation board. |
| EVAL-ADV7842-7511_v1p55_boot_image.zip |
Complete firmware image for EVAL-ADV7842-7511 including u-boot bootloader and v1p55 application binary. In order to program this on the board you will need at least ADZS-ICE-1000 and the test drive version of VisualDSP++. This file is in Intel-Hex format. |
| 7842_7511_LA1.55RC2_20120611.zip | Application binary v1p55 for EVAL-ADV7842-7511. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295. This file is in binary format. |
| AVES |
Legacy link to AVES installer. For new installations please use AVESBlue |
| AVES3 | Legacy link to AVES3 installer. For new installation please us Avesblue |
| AVESBLUE | Link to AVESBLUE installer. Used in conjunction with AVES3_Folder_EVAL-ADV7842-7511.zip |
| AVES3_Folder_EVAL-ADV7842-7511.zip | Folder of files to be used by AVES3, includes scripts |
| Hardware Config Update for Rev 1p0_1p1.pdf |
Hardware Configuration Update for using component video with Revision 1.1 versions of the eval board. (Note: If YPbPr / Component Video is important for your application, read this first!) |
| AdvantivVideo.zip | USB Driver for Advantiv™ Video Evaluation Boards |
| VDSP_BF524_M25P80_flash_programmer.dxe | VisualDSP 5.1.1 flash programmer driver file for EVAL-ADV7842-7511 and EVAL-ADV7842-7511-P |
| Software package for evaluation board | You can request the source code project for the EVAL-ADV7842-7511/EVAL-ADV7842-7511P here. |