This FAQ applies to EVAL-ADV7612-7511 and EVAL-ADV7612-7511P. All support files in their latest versions will be attached below.
Below are the support files for these evaluation boards. If you use these files, we recommend that you subscribe to EMail notifications for either the entire forum or at least this FAQ by clicking on the menu to the right. In this way you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.
File | Content |
---|---|
EVAL-ADV7612-7511_rev0p1_schems.pdf | Schematics (PDF) for EVAL-ADV7612-7511/EVAL-ADV7612-7511P |
EVAL-ADV7612-7511_build_files.zip | This zip contains ORCAD schematic, Allegro board files, gerbers, and BOMs for the evaluation boards |
EVAL-ADV7612-7511_BOM_20151211.pdf | BOM (in PDF format) for the EVAL-ADV7612-7511 evaluation board |
EVAL-ADV7612-7511P_BOM_20151211.pdf | BOM (in PDF format) for the EVAL-ADV7612-7511P evaluation board |
UG-295 | User Guide for the EVAL-ADV7612-7511 |
EVAL-ADV7612-7511_v1p55_boot_image.zip | Complete firmware image for EVAL-ADV7612-7511 including u-boot bootloader and v1p55 application binary. In order to program this on the board you will need at least ADZS-ICE-1000 and the test drive version of VisualDSP++ or CCES. Note this loader file is in Intel hex format. |
7612_7511_LR1.55RC2_20120611.zip | Application binary v1p2 for EVAL-ADV7612-7511. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295. Note: This loader file is in binary format in order to be compatible with u-boot. |
AVES | Legacy link to AVES installer. For new installations please use AVESBlue |
AVES3 | Legacy link to AVES installer. For new installations please use AVESBlue |
AVESBLUE | Link to AVESBLUE installer. Used in conjunction with AVES3_Folder_EVAL-ADV7842-7511.zip |
AVES3_Folder_EVAL-ADV7612-7511.zip | Folder of files to be used by AVES3/AVESBLUE |
AdvantivVideo.zip | USB Driver for Advantiv |
VDSP_BF524_M25P80_flash_programmer.dxe | VisualDSP 5.1.1 flash programmer driver file for EVAL-ADV7612-7511 and EVAL-ADV7612-7511-P |
Software package for evaluation board | You can request the source code project for the EVAL-ADV7612-7511/EVAL-ADV7612-7511P here. |