Attached and linked are several files supporting the development of systems using the AD9889B (HDCP keys stored externally in EEPROM) or the AD9389B (HDCP keys stored internally).
We recommend if you download and use these documents that you subscribe to email notifications for either the entire forum or at least this FAQ by clicking on the menu to the right. In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.
Those are CEA resolutions and should be mostly the same as the 1080p preset that was provided. The part should recognize them.
I see that there initial setup values for the more common resolutions like VGA, SXGA, etc. I need to have initial preset values for 576i, 576p, 720p en 1080i.
Can ADI provide me with these register values?