Q.
Is there an evaluation board for the ADV7513?
-----------------------------------------------------------------------------
A.
We do not currently have an evaluation board that features the ADV7513.
However, you can use the evaluation board for ADV7611 / ADV7511:
* EVAL-ADV7611EB1Z (HDCP-enabled receiver)
* EVAL-ADV7611EB2Z (non-HDCP receiver)
Since the ADV7611 has a 24-bit pixel bus (similar to the ADV7513), the attached scripts configure the ADV7511 to only use these pins.
You can also use the following evaluation boards to evaluate the functionality of the ADV7513 (using the attached script):
* EVAL-ADV7612EB1Z (HDCP-enabled receiver)
* EVAL-ADV7612EB2Z (non-HDCP receiver)
* EVAL-ADV7612-7511 (HDCP-enabled receiver)
* EVAL-ADV7612-7511P (non-HDCP receiver)
Regards,
Matt