This FAQ applies to EVAL-ADV8005-SMZ. All support files in their latest versions will be attached below.
Below are the support files for these evaluation board. We recommend that, if you download and use these files, you subscribe to email notifications for either the entire forum or at least this FAQ by clicking on the menu to the right. In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.
| EVAL-ADV8005-SMZ_User_Guide_RevPrB_20140606.pdf | Preliminary User Guide for the EVAL-ADV8005-SMZ evaluation board |
| EVAL-ADV8003-SMZ_rev0p2_schems_20150116.pdf | Schematics (in PDF format) for this evaluation board |
| EVAL-ADV8005-SMZ_BOM_20140911.pdf | BOM for this evaluation board |
|
EVAL-ADV8003-SMZ_rev0p2_schems_OrCAD_20150116.zip |
Schematics (in OrCAD format) for this evaluation board |
| BF_7625_8005_VSP_1.91RC1_20160526.zip |
Firmware 1.91.1 for the EVAL-ADV8005-SMZ. You will need to program both the application binary (BF_7625_8005_VSP_1.91RC1_20160526.bin) and the the OSD binary (OSD_1.90SP1_20151125.bin) in order for this firmware to work correctly. |
| EVAL-ADV8003-SMZ_rev0p2_layout_Allegro_20140630.zip | Layout (in Allegro format) for this evaluation board |
| EVAL-ADV8005-SMZ_20140703.zip | AVES3 folder for the EVAL-ADV8005-SMZ evaluation board |
| FAQ: How can I restore u-boot on EVAL-ADV8005-SMZ? | This page explains the hardware/software that is required and process to follow in order to restore u-boot in case it is accidentally deleted. |
| BF_800x_System_Commands_20150312.pdf | List of commands for the current release of firmware for this evaluation board. |
| EVAL-ADV8003-SMZ_FPGA_files_20130325.zip | Source files for the FPGA on this evaluation board. |
| Software package for evaluation board | You can request the source code project for the EVAL-ADV8005-SMZ here. |