Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

Are Multiple Video Streams over Single MIPI CSI-2 Link Possible on the ADV728x ?

The following post applies to the ADV7280-M, ADV7281-M, ADV7281-MA and ADV7282-M.

Hi All,

I have been asked a few times if it is possible to feed multiple video sources into the ADV728x-M and output them all over a single MIPI CSI-2 stream and use the virtual channel identifier to differentiate between each video source.

Unfortunately this is not possible on the ADV728x-M.

Multiple analog video sources can be connected to the ADV728x-M (upto 8 CVBS inputs on some ADV728x models). The ADV728x-M will then output a MIPI CSI-2 stream.

The Virtual Channel of the ADV728x-M MIPI CSI-2 output can also be programmed to one of four values.

However the ADV728x-M contains a single ADC. It can therefore only process one analog video source at a time. Therefore only one video source can be fed over the MIPI CSI-2 link at a time.

So is it possible to quickly switch back and forth between analog video sources and output all over the MIPI CSI-2 stream? Unfortunately this is also not possible on the ADV728x-M. Locking to analog video is not a straightforward task as many analog video standards are very similar. Even in fast switch mode it can take the ADV728x-M upto 250 ms to lock to an analog video source.

It is also not possible to connect the MIPI CSI-2 outputs from two or more ADV728x-M's together. MIPI CSI-2 is designed to be a single point to point standard (i.e. a single Tx to a single Rx). The input/output termination of the Tx/Rx are constantly changing in a MIPI CSI-2 stream as the high speed and low power states are being entered/exited. Connecting more than one MIPI CSI-2 Tx together will cause the termination scheme to violate the MIPI D-PHY specification. 

Regards,

Robert Hinchy,

Senior Applications Engineer,

Automotive Infotainment Group,

Analog Devices Inc.

Comments
Anonymous
Parents Comment Children
No Data
Related