Q
I wanted to know if AD9889B supports the Video Format 1080i-50?
A
Yes, the AD9889B does support 1080i50. As long as a format is within themaximum clock range (150MHz), then it can be supported. There is nothing that
is specific to the support of a given mode. Although we do not specifically
address VESA graphics modes, they are also supported in all forms through the
AD9889B.