Post Go back to editing

ADV7611 in dual link mode

I have following queries on ADV7611:

1. I need to know if AD7611  can be used in dual link mode, with one ADV7611 receiving even/odd pixel and second ADV7611 receiving odd pixels.User guide for the part mentions dual link mode (REFER ADI UG-180, pg 38). Please share the details of the solution where this is incorporated

2. ADV7611 has in-built equalizer, as per the datasheet. Can you share more specifications on the equalizer part?

Regards,

jyoti

Parents
  • Hi Mohit,

    The answer is no different for ADV7619.  There is no support or reference design for dual-link mode.  Greater than 170Mhz, the output of the ADV7619 is dual-pixel-- two pixels per clock on a double wide bus.  This has nothing to do with daul-link.

    We have no parts that have any special support for dual-link.  Customers have done this externally.

    There is no additional documentation for the EQ than what is in the hardware guide-- same as ADV7611/12.

    Dave

Reply
  • Hi Mohit,

    The answer is no different for ADV7619.  There is no support or reference design for dual-link mode.  Greater than 170Mhz, the output of the ADV7619 is dual-pixel-- two pixels per clock on a double wide bus.  This has nothing to do with daul-link.

    We have no parts that have any special support for dual-link.  Customers have done this externally.

    There is no additional documentation for the EQ than what is in the hardware guide-- same as ADV7611/12.

    Dave

Children
No Data