Post Go back to editing

ADV7611 in dual link mode

I have following queries on ADV7611:

1. I need to know if AD7611  can be used in dual link mode, with one ADV7611 receiving even/odd pixel and second ADV7611 receiving odd pixels.User guide for the part mentions dual link mode (REFER ADI UG-180, pg 38). Please share the details of the solution where this is incorporated

2. ADV7611 has in-built equalizer, as per the datasheet. Can you share more specifications on the equalizer part?

Regards,

jyoti

Parents
  • Hi Dave,

    The questions Jyoti has asked were in refernce to ADV7619. The datasheet says it supports a dual link in case of pixel clocks higher than 170MHz. Could you please help us know if the same is compliant to the DVI 1.0 dual link standard or will the part support DVI 1.0 in dual link/up to 300MHz pixel clock.

    Also, the other question in regard to the Equalizer performance is again for ADV7619. Please suggest.

    Regards

    Mohit

Reply
  • Hi Dave,

    The questions Jyoti has asked were in refernce to ADV7619. The datasheet says it supports a dual link in case of pixel clocks higher than 170MHz. Could you please help us know if the same is compliant to the DVI 1.0 dual link standard or will the part support DVI 1.0 in dual link/up to 300MHz pixel clock.

    Also, the other question in regard to the Equalizer performance is again for ADV7619. Please suggest.

    Regards

    Mohit

Children
No Data