please tell me about when do not use the following pin.
does it have done what processing?
SFL(12pin)、INT(11pin)、P0~P9(19,20,21,22,23,24,32,33,34,35)
Thank you.
ADV7188
Production
The ADV7188 integrated video decoder automatically detects and converts standard analog baseband television signals compatible with worldwide NTSC, PAL...
Datasheet
ADV7188 on Analog.com
please tell me about when do not use the following pin.
does it have done what processing?
SFL(12pin)、INT(11pin)、P0~P9(19,20,21,22,23,24,32,33,34,35)
Thank you.
All these pins are output pins. They can be left floating or unconnected if they are not being used.
Hello.
There is material that I want you to offer.
Please send IBIS or SPICE.
Thank you.
We don't have an ibis file for the ADV7188 however you can extract some of the parameters from the ADV7189 ibis file found at this link.
Hi,
The REFOUT pin should only be connected as described in the datasheet. The external filtering capacitors are required for the internal reference to operate correctly.
No other circuitry should be connected to this pin.
This voltage reference is set internally as part of the ADI recommended settings.
Changing the voltage reference or adding external noise to this pin will affect the ADC performance.
Regards,
Derek
HI.
About a voltage output pin of the built-in reference, Please tell me a method of use.
Please tell me the electrical specifications of the REFOUT pin.
Does this have a mention to a data sheet?
Thank you.
Hi,
I am going to forward this the the ADV7188 expert.