Post Go back to editing

HDMI TX ADV7511W

Hi,

I am using HDMI TX ADV7511W with its digital inputs interfaced to FPGA (Virtex 7).

The datasheet mentions that its video/audio logic accepts levels from 1.8V to 3.3V.

The IC ADV7511W has 1.8V Supply Voltage (DVDD, AVDD, PVDD, BGVDD) and 3.3V Supply Voltage (DVDD_3V). There is no specific IO voltage pin (like DVDD_IO for some other interfaces). So how does it know which IO Voltage its working with? 

Can I interface its digital inputs with LVCMOS18 IO standard working on 1.8V IO interfaced to FPGA?

-Chinmay

Parents
  • I have a similar question, in the datasheet mentions that the voltage level of digital inputs are between 1.35V and 3.5V, but in Hardware User's Guide indicates that: 

    " The digital inputs (video, audio) on the ADV7511W work with 1.8V and 3.3V signal levels. The I2C ports
    (DDCSDA/DDCSCL and SDA/SCL) and (Consumer Electronic Control) CEC port work with 1.8V and 3.3V and are
    tolerant of 5V logic levels. "

    So I would like to know if it is possible interface digital IO with 2.5 V to FPGA.

    Thanks.

Reply
  • I have a similar question, in the datasheet mentions that the voltage level of digital inputs are between 1.35V and 3.5V, but in Hardware User's Guide indicates that: 

    " The digital inputs (video, audio) on the ADV7511W work with 1.8V and 3.3V signal levels. The I2C ports
    (DDCSDA/DDCSCL and SDA/SCL) and (Consumer Electronic Control) CEC port work with 1.8V and 3.3V and are
    tolerant of 5V logic levels. "

    So I would like to know if it is possible interface digital IO with 2.5 V to FPGA.

    Thanks.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.