Post Go back to editing

ADV7513 scripts for 1080p25 & 1080p29/30 formats

Thread Summary

The user inquired about DE generation, sync adjustment, and embedded sync processing settings for 1080p25 and 1080p29/30 modes in the ADV7513 programming guide. The final answer stated that these settings are not provided but can be derived from CEA standards, with the rest of the settings similar to 720p. The accompanying answer confirmed that no specific scripts are available but suggested using CEA standards for DE generation settings.
AI Generated Content

Hello,

In the ADV7513 programming guide, the tables for setting the DE generation, sync adjustment and embedded sync processing (i.e. tables 26, 27, & 28) do not show the settings for both 1080p25 nor 1080p29/30. 

Is it possible to provide scripts or the settings for the ADV7513 for these modes of operation?  I reviewed the data indicating that the ADV7511 is very similar to the ADV7513 in this regards but the ADV7511 programming guide also did not show these modes. 

Any help is significantly appreciated.

Parents
  • FormerMember
    FormerMember
on Apr 9, 2014 3:03 AM
+1

Check these scripts out.  There's a section that does 1080i30 & 1080i25 for embedded sync which regen DE for the 7511 (same part as 7513)

Reply
  • FormerMember
    FormerMember
on Apr 9, 2014 3:03 AM
+1

Check these scripts out.  There's a section that does 1080i30 & 1080i25 for embedded sync which regen DE for the 7511 (same part as 7513)

Children
No Data