Post Go back to editing

understanding ADV7513 CSC behavior

I'm taking in YCbCr 4:2:2 input video from our FPGA (ID=1, style 3, 24 bit) where only the Y[11:0] bits are being used to represent grayscale video, the Cb/Cr[11:0] bits are static at 0x880 (ideally it would be 0x800 but the 8 LSBs are hard-wired).  At the moment I don't have a way to capture 12 bit color depth video so I'm letting the ADV7513 stay in DVI mode which forces the output to be RGB, and I've tried using both 4:2:2 and 4:4:4 output formats for the sake of this question.

I'm setting these register values (note this is a subset of my initialization settings):


0x15 = 0x01
0x16 = 0x2E
0x55 = 0x12
0xAF = 0x04

Since I don't want Cb/Cr to influence my output colormap, I've enabled and set up the CSC coefficients like this (CSC_mode=1):

A1 A2 A3 A4
0 2047 0 0


B1 B2 B3 B4
0 2048 0 0


C1 C2 C3 C4
0 2047 0 0

i.e., zeroing out all but A2,B2,C2 makes it so only Y applies.  With this I get a good black to white grayscale video output, and the above coefficients make all 3 CSC output channels span 0-4095 as Y goes from 0-4095.

I can also set the coefficients to give an inverted video output like this:

A1 A2 A3 A4
0 -2047 0 2047


B1 B2 B3 B4
0 -2047 0 2047


C1 C2 C3 C4
0 -2047 0 2047

All 3 CSC output channels span 4094-1 as Y goes from 0-4095, so video goes white to black.

From the above I'm presuming that no clipping is being done to the output channels since at no time does the 12 bit output go below 0 or above 4095.  Further, I'm presuming that the ADV7513 is automatically scaling the 12 bit outputs down to 8 bits for RGB 4:4:4 output format.

Now I want to make some pseudocolor maps, so I tried this (CSC_mode=0):

A1 A2 A3 A4
0 4095 0 -2047


B1 B2 B3 B4
0 4095 0 -1023


C1 C2 C3 C4
0 4095 0 0

The equations yield Red channel output going -2047 to 2047, Green channel output going -1023 to 3071, and Blue channel output going 0 to 4094.  If I assume negative values will be clipped to 0 by the CSC, then I should get video that goes from black into brightening shades of blue as Y goes 0-4095.  However, when implemented I get video going from orange into white.  Shouldn't the clipping registers 0xC0-0xC7 take care of negative output values (i.e. less than the programmed 0x000)?

Another scheme I tried:

A1 A2 A3 A4
0 4095 0 0


B1 B2 B3 B4
0 0 0 0


C1 C2 C3 C4
0 -4096 0 4095

This keeps Green channel output at 0, Red goes 0-4094 and Blue goes 4095-0.  I would expect this would yield video going from blue through red as Y goes 0-4095.  However, when implemented I get video going from green through yellow.  Am I not understanding something about how the CSC is computing RGB output?

Thanks.

Parents
  • Hi,

     The case where YCbCr with a code range from -128 to 127 is input, setting bit 0xD5[1] to 1 will shift the code ranges to 0-255. If the user requires a black image to be sent across the HDMI link register 0xD5[0] should be set to 1 and register 0x16[0] should be set according to the output color space.The black image can be useful for protecting copyrighted content during HDCP authentication.

     The offset values gives 128 for the Pr and Pb components. The value of 128 equates to half the range on an 8-bit system. It must be noted that the CSC operates on a 12-bit range. The offsets, therefore, must be changed from 128 to half the range of a 12-bit system, which equates to 2048.

      Please refer section 6.5.1 of the ADV7403 Datasheet Manual (ADV7403_Manual_RevB.pdf) that provides more details about CSC coefficient calculation, which is available at ADV7403 Design Support Files.

      

    Thanks,

    Poornima

Reply
  • Hi,

     The case where YCbCr with a code range from -128 to 127 is input, setting bit 0xD5[1] to 1 will shift the code ranges to 0-255. If the user requires a black image to be sent across the HDMI link register 0xD5[0] should be set to 1 and register 0x16[0] should be set according to the output color space.The black image can be useful for protecting copyrighted content during HDCP authentication.

     The offset values gives 128 for the Pr and Pb components. The value of 128 equates to half the range on an 8-bit system. It must be noted that the CSC operates on a 12-bit range. The offsets, therefore, must be changed from 128 to half the range of a 12-bit system, which equates to 2048.

      Please refer section 6.5.1 of the ADV7403 Datasheet Manual (ADV7403_Manual_RevB.pdf) that provides more details about CSC coefficient calculation, which is available at ADV7403 Design Support Files.

      

    Thanks,

    Poornima

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.