Post Go back to editing

hs adjust and VBI adjust problem

adv7842 or adv7441a

vga output:1366*768@60

In the output image on the left a small piece missing, and the color is wrong, I look at the signal and found that the effective number of pixels of each line of video over the 1366 pixels(1377)


my problem is how to set follwing register:I doubt that this phenomenon is due to this


DE_H_START = Vary the leading edge position of DE control register, CP map, 0x8B [3:2], 0x8D [7:0]
DE_H_END = Vary the trailing edge position of DE control register, CP map, 0x8B [1:0], 0x8C [7:0]
DE_V_START = Vary the start position of the VBI region control register, CP map, 0x8E [7:4]
DE_V_END = Vary the end position of the VBI region control register, CP map, 0x8E [3:0]


i saw this doc:ADV7844_ADV7842_Autographics_Pr0_031109

i can not get any useful infomation to set these register.....

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.