Post Go back to editing

adv7280m doesn't work at the temperature of -15 centigrade

Thread Summary

The user reports that the ADV7280BCPZ-M does not work at temperatures below -15°C, specifically with MIPI clock issues. The final answer confirms the device is rated for -40°C and suggests troubleshooting steps, including entering free run mode, probing signals with a multi-channel oscilloscope, using ADI recommended scripts, and checking for a 1 MOhm resistor between XTALP and XTALN pins. The user is also directed to ADI's Linux driver repository for further support.
AI Generated Content

Hi:

   i found that adv7280m cann't work on the temperature below -15 centigrade. the detail is as below:

1. the crystal is still working on the -15 centigrade, but the mipi clock has problem, the cpu(omap4) shows that it doesn't receive MIPI HS BYTE CLOCK.

2. if the temperature is decreased from 0 centigrade to -15 centigrade gradually, the cpu(omap4) can receive the mipi hs byte clock on the temperatue of -15 centigrade, but if we stop the video capturing at the time , and restart the adv7280m to capture video, it doesn't work.

   since my scope can only watch the 28.636M signal from crystal, it cann't watch the differential mipi clock signal, so i don't make sure that the mipi clock at -15 centigrade is the same as the one at 0 centigrade.

   so, could any one help me?

   thanks very much.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.