Hello all,
Clock source on evaluation boar of ADV7612 is crystal of 28.63636MHz.
Question1
Can I use oscillator ?
Question2
If possible, could you give me your advice about using oscillator
Regards,
ADV7612
Recommended for New Designs
The ADV7612 is offered in automotive, professional (no HDCP), and industrial versions. The operating temperature range is
−40°C to +85°C.
The UG-216...
Datasheet
ADV7612 on Analog.com
Hello all,
Clock source on evaluation boar of ADV7612 is crystal of 28.63636MHz.
Question1
Can I use oscillator ?
Question2
If possible, could you give me your advice about using oscillator
Regards,
Hello,
Yes you can use an oscillator to clock the ADV7612.
The oscillator should be fed into the XTALP pin of the ADV7612. XTALN pin should be left floating.
The oscillator should be 1.8V pp.
I advise using an oscillator with a 28.63636MHz frequency.
The oscillator must have an accuracy of 50 ppm over the entire temperature range of operation.
We have seen issues before where programmable oscillators have not had this level of accuracy. I advise using a non-programmable oscillator.
Regards,
Robert Hinchy
Applications Engineer,
Analog Devices Inc.
Hello,
Thank you for your advice.
Regards.