ADV7627 product page and design support files

Hi,

Firstly, am I blind or is there no link to the ADV7625/6/7 on the main HDMI interface products page?  Looking here:

http://www.analog.com/en/audiovideo-products/analoghdmidvi-interfaces/products/index.html

I don't see any links to those products, just to the older ones like the ADV7623.

Secondly, are there any design support files for the ADV7627?  This link:

ADV7627 Design Support Files

says it will be available "in a few weeks", but that was a year ago.  Is there a hardware manual for this product?  If not in the public domain, is it available after signing an NDA?  And if there aren't any other docs, is it sufficiently similar (aside from the second HDMI out) to the ADV7625 that we can design off the ADV7625's docs?

Thank you very much.

JK

Parents
  • 0
    •  Analog Employees 
    on Feb 9, 2015 9:22 PM over 5 years ago

    The ADV7625 is a newer part then the ADV7623.  The ADV7627 is a subset of the ADV7625 and we use the ADV7625 manuals with the exception of only one transmitter for the 7627.  As a matter of fact the EVAL-ADV7625-SMZ board can be made to operate the same as with a ADV7627 installed with a slight binary code change.

    I would base my decision on the ADV7625 manuals and decide whether I needed a 5x2, 2x2, or 5x1 chip.  Basically they are the same chip with just different bond outs and packages.

Reply
  • 0
    •  Analog Employees 
    on Feb 9, 2015 9:22 PM over 5 years ago

    The ADV7625 is a newer part then the ADV7623.  The ADV7627 is a subset of the ADV7625 and we use the ADV7625 manuals with the exception of only one transmitter for the 7627.  As a matter of fact the EVAL-ADV7625-SMZ board can be made to operate the same as with a ADV7627 installed with a slight binary code change.

    I would base my decision on the ADV7625 manuals and decide whether I needed a 5x2, 2x2, or 5x1 chip.  Basically they are the same chip with just different bond outs and packages.

Children
No Data