ADV7180
Not Recommended for New Designs
The ADV7180 automatically detects and converts standard analog baseband television signals compatible with worldwide NTSC, PAL, and SECAM standards into...
Datasheet
ADV7180 on Analog.com
I get this response (or varieties of it) when I try to access the ftp.analog.com site to download ADV7180 files with FileZilla Client on Windows 7 Pro:
Status: Resolving address of ftp.analog.com
Status: Connecting to 137.71.25.119:21...
Status: Connection established, waiting for welcome message...
Status: Initializing TLS...
Status: Verifying certificate...
Status: TLS connection established.
Status: Server does not support non-ASCII characters.
Status: Connected
Status: Retrieving directory listing...
Command: PWD
Response: 257 "/" is current directory
Command: TYPE I
Response: 200 Transfer mode set to BINARY
Command: PASV
Response: 227 Entering Passive Mode (137,71,25,119,234,168).
Command: LIST
Error: The data connection could not be established: ETIMEDOUT - Connection attempt timed out
Error: Connection timed out after 200 seconds of inactivity
Error: Failed to retrieve directory listing
Status: Resolving address of ftp.analog.com
Status: Connecting to 137.71.25.119:21...
Status: Connection established, waiting for welcome message...
Status: Initializing TLS...
Status: Verifying certificate...
Status: TLS connection established.
Status: Server does not support non-ASCII characters.
Status: Connected
Status: Retrieving directory listing...
Command: PWD
Response: 257 "/users/decoders" is current directory
Command: TYPE I
Response: 200 Transfer mode set to BINARY
Command: PASV
Response: 227 Entering Passive Mode (137,71,25,119,234,191).
Command: LIST
Error: The data connection could not be established: ETIMEDOUT - Connection attempt timed out.
Anyone had a similar problem and been able to fix it? I can download the files I need using the Terminal window on a Mac, but I'd rather use FileZilla Client if possible.
I've been having trouble recently also when accessing these files from certain locations. I asked our IT team to look into it. I will ask them for an update.
-Matt
Matt - an aside. I'm trying to download the file "ADV Register Control Ver 7.0 Installation.zip". I can switch to the ADV7180 directory but can't download this archive using a Terminal Window (Mac) or a Command Prompt; I get the message "File not found" . I can download the file "ADV7180_Installation_Guide_4.0.pdf" and the .lnk file from the parent directory. I'm not sure where to go from here, but we've spent about two days trying to sort this out and we still don't have our eval board running. Any thoughts?
Hi Julian,
I was able to get command prompt FTP (in Windows 7 Professional) to work with ftp.analog.com. There were two programs in my Windows Firewall settings marked "File Transfer Program" and the bottom one was not checked. As soon as I checked it and applied my changes, command prompt FTP started working correctly.
Maybe this will be useful for you.
BTW: I was able to download ADV Register Control Ver 7.0 Installation.zip without any issues.
-Matt
Try changing FileZilla Site Manager's General tab -> Encryption from "Use explicit FTP over TLS if available" to "Only use plain FTP (insecure)". That fixed the issue on my PC.
-Matt
Thanks Matt - will give it a go. While I have your attention, can you tell me how to get a posting of mine past moderation? I've been in a discussion with Rob.Analog for some time now and my last posting to him is still being moderated after 5 days. Any thoughts? As far as I know, i'm not being abusive or unreasonable in any way, so I can't understand why this discussion has stalled. It's a big problem for us!
Sorry about that. We were having moderation issues where threads were not going where expected for moderation. It's all fixed now and we're working through the backlog as quickly as we can.
Dave
Hi, I'm Kwon live in korea.
I have a problem. I bought EVAL-ADV739XFEZ for ADC7393 test.
But, fail to connect FileZilla.
명령: PWD
응답: 257 "/users/encoders" is current directory
명령: TYPE I
응답: 200 Transfer mode set to BINARY
명령: PASV
응답: 227 Entering Passive Mode (137,71,25,119,229,71).
명령: MLSD
오류: Connection timed out after 20 seconds of inactivity
Can you help me, how solve this problem?
Best Regard.
Kwon.