Post Go back to editing

(ADV7612)Can ADV7612 ouput High-Resolution Audio with I2S?

Hi!

If ADV7612 receive the HDMI with High-Resolution Audio ,

can the device output the High-Resolution Audio with I2S ?

* High-Resolution Audio (Higher than 24bit/96kHz)

If it can output High-Resolution Audio, does the device sustain the dat rlate?


And could you tell me the I2S maximum date rate?


Thank you.

Best regards.

Kawa

Parents
  • FormerMember
    0 FormerMember
on Jun 8, 2015 1:03 PM

Audio standards only require 24 bit.  Refer to IEC60958 and IEC61937 to how the audio is encoded.  A lot depends on output format you need.

Reply
  • FormerMember
    0 FormerMember
on Jun 8, 2015 1:03 PM

Audio standards only require 24 bit.  Refer to IEC60958 and IEC61937 to how the audio is encoded.  A lot depends on output format you need.

Children
No Data