Post Go back to editing

(ADV7612)Can ADV7612 ouput High-Resolution Audio with I2S?

Thread Summary

The user inquired if the ADV7612 can output High-Resolution Audio (24bit/96kHz and above) via I2S. The final answer confirms that the ADV7612 supports sampling frequencies up to 192kHz and sample widths up to 24 bits. The I2S maximum bandwidth is 31 bits, but the usable limit is 24 bits due to audio standards.
AI Generated Content

Hi!

If ADV7612 receive the HDMI with High-Resolution Audio ,

can the device output the High-Resolution Audio with I2S ?

* High-Resolution Audio (Higher than 24bit/96kHz)

If it can output High-Resolution Audio, does the device sustain the dat rlate?


And could you tell me the I2S maximum date rate?


Thank you.

Best regards.

Kawa

Parents Reply Children
No Data