Post Go back to editing

(ADV7612)Can ADV7612 ouput High-Resolution Audio with I2S?

Hi!

If ADV7612 receive the HDMI with High-Resolution Audio ,

can the device output the High-Resolution Audio with I2S ?

* High-Resolution Audio (Higher than 24bit/96kHz)

If it can output High-Resolution Audio, does the device sustain the dat rlate?


And could you tell me the I2S maximum date rate?


Thank you.

Best regards.

Kawa

Parents
  • FormerMember
    0 FormerMember
on Jun 4, 2015 2:33 PM

The ADV7612 can extract L-PCM, IEC 61937 compressed or DST audio data from the audio packets.  These standards set the limits.  It can support sampling frequncies up to 192kHz.  Sample width is limited to 24 bits.

Reply
  • FormerMember
    0 FormerMember
on Jun 4, 2015 2:33 PM

The ADV7612 can extract L-PCM, IEC 61937 compressed or DST audio data from the audio packets.  These standards set the limits.  It can support sampling frequncies up to 192kHz.  Sample width is limited to 24 bits.

Children
No Data