Post Go back to editing

DVI Dual Link operation with ADV7619

Hello,

I'm thinking that there is no DVI Dual Link operation of solutions on this site information.

For example, Is it possible to be implemented using external control hardware with ADV7619?

When configuring in the ADV7619 and external hardware

If the output of the phase is shifted, Is there a way to shift the value to grasp?


Regards,

Hitoshi

Parents
  • FormerMember
    0 FormerMember
on Jul 27, 2015 12:35 PM

The ADV7619 does not support Dual link DVI.  It would require 2 chips and a method to re-synchronize the outputs.  The ADV7619 will decode 4K x 2K @30 to a 48-bit bus

Reply
  • FormerMember
    0 FormerMember
on Jul 27, 2015 12:35 PM

The ADV7619 does not support Dual link DVI.  It would require 2 chips and a method to re-synchronize the outputs.  The ADV7619 will decode 4K x 2K @30 to a 48-bit bus

Children
No Data