Hi!
I have some questions about ADV739*.
(1)=========================================================
I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.
Does ADV7390/1 support that Video-format?
Or must I use ADV7392/3?
At the data sheet P7(Table4),
it says that the spec is
SD/ED 27MHz
ED(at 54MHz)
I think this means , ADV739* supports
SD-SDR 27MHz
SD-DDR 27MHz
ED-SDR 27MHz
ED-DDR 27MHz
ED-SDR 54MHz
and the point is ED-DDR 54MHz is not support.
Is my understanding is correct?
============================================================
(2)=========================================================
And the date sheet P28(Tabele 18) says ED/HD-SDR is supported
by only ADV7392/3 because the ADV7390/1 can support 8bit input.
Is my understanging is correct?
============================================================
(3)=========================================================
Can you tell me what is the difference between
"ED/HD-SDR input" and "ED(at 54MHz)input"?
============================================================
(4)=========================================================
At date sheet P31(Table 20),
it says that ADV739* can support BTA-1004.
Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?
Or must I use ADV7392/3?
============================================================
(5)=========================================================
If I input the ED video support(which is supported by the devices),
is there any different signal process and output signal?
I want to understand what is the differnce between ADV7390/1 and ADV7392/3 besides Macrovision.
============================================================
The point is , I want to know that
Does ADV7390/1 can support BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit)?
Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?
Or must I use ADV7392/3?
I would really appreciate if you don't mind to teach me about this.
Best regards.
Kawa