Post Go back to editing

(ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

Hi!

I have some questions about ADV739*.

(1)=========================================================

I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

Does ADV7390/1 support that Video-format?

Or must I use ADV7392/3?

At the data sheet P7(Table4),

it says that the spec is

SD/ED 27MHz

ED(at 54MHz)

I think this means , ADV739* supports

SD-SDR 27MHz

SD-DDR 27MHz

ED-SDR 27MHz

ED-DDR 27MHz

ED-SDR 54MHz

and the point is ED-DDR 54MHz is not support.

Is my understanding is correct?

============================================================

(2)=========================================================

And the date sheet P28(Tabele 18) says ED/HD-SDR is supported

by only ADV7392/3 because the ADV7390/1 can support 8bit input.

Is my understanging is correct?

============================================================

(3)=========================================================

Can you tell me what is the difference between

"ED/HD-SDR input" and "ED(at 54MHz)input"?

============================================================

(4)=========================================================

At date sheet P31(Table 20),

it says that ADV739* can support BTA-1004.

Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Or must I use ADV7392/3?

============================================================

(5)=========================================================

If I input the ED video support(which is supported by the devices),

is there any different signal process and output signal?

I want to understand what is the differnce between ADV7390/1 and ADV7392/3 besides Macrovision.

============================================================

The point is , I want to know that

Does ADV7390/1 can support BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Or must I use ADV7392/3?

I would really appreciate if you don't mind to teach me about this.

Best regards.

Kawa

Parents
  • Hi Dave!

    Thank you for your answer.

    5)

    So, if I maintain the timing ,does the device can handle BT656 or BTA-T-1004?

    6)

    I understood with your answer that the device can support 8-bit ED-SDR 54MHz.

    And also I am searching the Configuration Scripts with using ED-SDR 54MHz(BT656 or BTA-T-1004).

    And from Table.63 to 131, there is no example using ED-SDR 54MHz 8-bit.

    Can you show me the example Scripts using ED-SDR 54MHz 8-bit?

    I would really appreciate if you don't mind to teach me about this.

    Best regards.

    Kawa

Reply
  • Hi Dave!

    Thank you for your answer.

    5)

    So, if I maintain the timing ,does the device can handle BT656 or BTA-T-1004?

    6)

    I understood with your answer that the device can support 8-bit ED-SDR 54MHz.

    And also I am searching the Configuration Scripts with using ED-SDR 54MHz(BT656 or BTA-T-1004).

    And from Table.63 to 131, there is no example using ED-SDR 54MHz 8-bit.

    Can you show me the example Scripts using ED-SDR 54MHz 8-bit?

    I would really appreciate if you don't mind to teach me about this.

    Best regards.

    Kawa

Children
No Data