Post Go back to editing

(ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

Hi!

I have some questions about ADV739*.

(1)=========================================================

I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

Does ADV7390/1 support that Video-format?

Or must I use ADV7392/3?

At the data sheet P7(Table4),

it says that the spec is

SD/ED 27MHz

ED(at 54MHz)

I think this means , ADV739* supports

SD-SDR 27MHz

SD-DDR 27MHz

ED-SDR 27MHz

ED-DDR 27MHz

ED-SDR 54MHz

and the point is ED-DDR 54MHz is not support.

Is my understanding is correct?

============================================================

(2)=========================================================

And the date sheet P28(Tabele 18) says ED/HD-SDR is supported

by only ADV7392/3 because the ADV7390/1 can support 8bit input.

Is my understanging is correct?

============================================================

(3)=========================================================

Can you tell me what is the difference between

"ED/HD-SDR input" and "ED(at 54MHz)input"?

============================================================

(4)=========================================================

At date sheet P31(Table 20),

it says that ADV739* can support BTA-1004.

Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Or must I use ADV7392/3?

============================================================

(5)=========================================================

If I input the ED video support(which is supported by the devices),

is there any different signal process and output signal?

I want to understand what is the differnce between ADV7390/1 and ADV7392/3 besides Macrovision.

============================================================

The point is , I want to know that

Does ADV7390/1 can support BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Or must I use ADV7392/3?

I would really appreciate if you don't mind to teach me about this.

Best regards.

Kawa

Parents
  • Hi Dave!

    Thank you for your answer.

    I understood almost.

    I have two questions again.

    3)

    At your answer ,ED(54MHz) is 8-bit, but at the data sheet Figure10 and 11 said ,

    the device can support 8bit or 10bit .

    With my understanding , it is not important if the input is 8-bit or 10-bit.

    The point is the input-format.

    So, if I want to use 8bit-Input , I can choose ADV7390/1

    but if I want to use 10bit-Input, I have to choose ADV7392/3.

    Is my understanding is correct?

    4)

    With your answer and form the data sheet,

    I understood that ADV7390/1 can support BT.656 and BTA-1004 with 54MHz-SDR(8bit).

    If I want to use these formats ,only I have to do is select the right register(0x30).

    If I want to use BTA-1004 , I think I have to choose

    0x30 = 00010

    And if I want to use BT.656 which register should I choose?

    I would really appreciate if you don't mind to teach me about this.

    Best regards.

    Kawa

Reply
  • Hi Dave!

    Thank you for your answer.

    I understood almost.

    I have two questions again.

    3)

    At your answer ,ED(54MHz) is 8-bit, but at the data sheet Figure10 and 11 said ,

    the device can support 8bit or 10bit .

    With my understanding , it is not important if the input is 8-bit or 10-bit.

    The point is the input-format.

    So, if I want to use 8bit-Input , I can choose ADV7390/1

    but if I want to use 10bit-Input, I have to choose ADV7392/3.

    Is my understanding is correct?

    4)

    With your answer and form the data sheet,

    I understood that ADV7390/1 can support BT.656 and BTA-1004 with 54MHz-SDR(8bit).

    If I want to use these formats ,only I have to do is select the right register(0x30).

    If I want to use BTA-1004 , I think I have to choose

    0x30 = 00010

    And if I want to use BT.656 which register should I choose?

    I would really appreciate if you don't mind to teach me about this.

    Best regards.

    Kawa

Children
No Data