Post Go back to editing

(ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

Hi!

I have some questions about ADV739*.

(1)=========================================================

I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

Does ADV7390/1 support that Video-format?

Or must I use ADV7392/3?

At the data sheet P7(Table4),

it says that the spec is

SD/ED 27MHz

ED(at 54MHz)

I think this means , ADV739* supports

SD-SDR 27MHz

SD-DDR 27MHz

ED-SDR 27MHz

ED-DDR 27MHz

ED-SDR 54MHz

and the point is ED-DDR 54MHz is not support.

Is my understanding is correct?

============================================================

(2)=========================================================

And the date sheet P28(Tabele 18) says ED/HD-SDR is supported

by only ADV7392/3 because the ADV7390/1 can support 8bit input.

Is my understanging is correct?

============================================================

(3)=========================================================

Can you tell me what is the difference between

"ED/HD-SDR input" and "ED(at 54MHz)input"?

============================================================

(4)=========================================================

At date sheet P31(Table 20),

it says that ADV739* can support BTA-1004.

Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Or must I use ADV7392/3?

============================================================

(5)=========================================================

If I input the ED video support(which is supported by the devices),

is there any different signal process and output signal?

I want to understand what is the differnce between ADV7390/1 and ADV7392/3 besides Macrovision.

============================================================

The point is , I want to know that

Does ADV7390/1 can support BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Does ADV7390/1 can support BTA-1004 ED(525p)-SDR 54MHz 8bit(not 16bit)?

Or must I use ADV7392/3?

I would really appreciate if you don't mind to teach me about this.

Best regards.

Kawa

Parents
  • Hello Kawa,

    1) There is no ED-DDR at 54Mhz anyway. ED-DDR at 54Mhz makes no sense-- that would mean a format with a pixel clock of 108Mhz. What I think you are talking about is what we are calling ED-SDR (54Mhz)-- 8bit components interleaved with 1 component per clock at 2x the real clock rate. What I think you want to do is supported.

    ED-DDR 27Mhz and ED-SDR 54Mhz are basically the same thing, only one is a 27Mhz clock and you sample on both edges and the other is a 54Mhz clock and you sample on only one edge.

    2) Correct

    3) ED-HD-SDR is a 16-bit wide interface with components in parallel with one pixel (2 components) per clock.

    ED at 54Mhz is an 8-bit wide interface with 8-bit components interleaved at 2x the pixel clock.

    4) There is no difference in the parts in terms of that format support, it's only that the video bus is 8-bit versus 16-bit.

    5) It's only the video bus size and macrovision that is different.

    Dave

Reply
  • Hello Kawa,

    1) There is no ED-DDR at 54Mhz anyway. ED-DDR at 54Mhz makes no sense-- that would mean a format with a pixel clock of 108Mhz. What I think you are talking about is what we are calling ED-SDR (54Mhz)-- 8bit components interleaved with 1 component per clock at 2x the real clock rate. What I think you want to do is supported.

    ED-DDR 27Mhz and ED-SDR 54Mhz are basically the same thing, only one is a 27Mhz clock and you sample on both edges and the other is a 54Mhz clock and you sample on only one edge.

    2) Correct

    3) ED-HD-SDR is a 16-bit wide interface with components in parallel with one pixel (2 components) per clock.

    ED at 54Mhz is an 8-bit wide interface with 8-bit components interleaved at 2x the pixel clock.

    4) There is no difference in the parts in terms of that format support, it's only that the video bus is 8-bit versus 16-bit.

    5) It's only the video bus size and macrovision that is different.

    Dave

Children
No Data