ADV7481 as test pattern generator

I want to use the ADV7481 only as video test pattern generator with output on transmitter A. The device is controlled by I2C. Which clocks have I to provide? Is the XTAL enough?

  • Can you provide some more details on what you plan to provide to the ADV7481 and get from the ADV7481?

    -Matt

  • Hi Matt, there was a unintended submit during edit. Here the correct response:

    This is the only function planned for this ADV7481 application:

      generate internal pattern (controlled by reg 0x37 in CP MAP) output on MIPI Transmitter A

    used blocks:

      I2C Slave control (programming interface)

      MIPI Transmitter A used in x2 mode

        used signals: CLKAP/N, DA0P/N, DA1P/N

        unused signals: DA2P/N, DA3P/N

    unused blocks:

      SPI

      HDMI in (data + control)

      Analog in

      DIAG

      MIPI Transmitter B

      Audio output

      8-Bit digital in/out Port

    All names refer to DETAILED FUNCTIONAL BLOCK DIAGRAM (figure 2) in the datasheet.

    Which signals of the unused blocks can be left open / require pullup/pulldown?

    Since the internal pattern are generated in the CP Block is there a RXCP/N required?

    --Günter

  • Hi Günter,

    Sorry for the delay. Our ADV7481 expert was out of office but is back now.

    Do you have our ADV7481 evaluation board?

    -Matt

  • I see several of the scripts in our recommended scripts file (http://www.analog.com/media/en/engineering-tools/design-tools/ADV7481ES3C-VER.3.6c.txt) have a color bar pattern enabled:

    :08-01 Free-run MIPI TxA CSI 1-Lane - YUV422 8-Bit, 720x480p:

    44 37 81 ; Output Colorbars Pattern

    :08-02 Free-run MIPI TxA CSI 2-Lane - YUV422 8-Bit, 720x480p:

    44 37 81 ; Output Colorbars Pattern

    :08-03 Free-run MIPI TxA CSI 1-Lane - YUV422 8-Bit, 720x576p:

    44 37 81 ; Output Colorbars Pattern

    :08-04 Free-run MIPI TxA CSI 2-Lane - YUV422 8-Bit, 720x576p:

    44 37 81 ; Output Colorbars Pattern

    :08-05 Free-run MIPI TxA CSI 1-Lane - RGB888, VGA 640x480 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-06 Free-run MIPI TxA CSI 2-Lane - RGB888, VGA 640x480 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-07 Free-run MIPI TxA CSI 2-Lane - YUV422 8-Bit, 1280x720p 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-08 Free-run MIPI TxA CSI 4-Lane - YUV422 8-Bit, 1280x720p 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-09 Free-run MIPI TxA CSI 2-Lane - RGB888, 1280x720p 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-10 Free-run MIPI TxA CSI 4-Lane - RGB888, 1280x720p 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-11 Free-run MIPI TxA CSI 2-Lane - RGB888, WVGA 800x480 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-12 Free-run MIPI TxA CSI 4-Lane - RGB888, WVGA 800x480 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-13 Free-run MIPI TxA CSI 4-Lane - RGB888, WXGA-SONY 1280x768 60Hz:

    44 37 81 ; Output Colorbars Pattern

    :08-14 Free-run MIPI TxA CSI 4-Lane - RGB888, 1920x1080p 60Hz:

    44 37 81 ; Output Colorbars Pattern

    -Matt

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin