Post Go back to editing

ADV7513 Video Clock

Thread Summary

The user inquires about the compatibility of the MAX9276 deserializer output with the input of the ADV7513 for converting HDMI data as RGB 24-bit color depth back into an HDMI signal. The final answer confirms that the CLK pin on the ADV7513 is the pixel clock for the input pixel bus, which can be 24/16/8 bits wide in RGB or YCbCr color space. The user is advised to connect the MAX9276 PPCLK to the ADV7513 CLK and DOUT to D[23:0], with further verification pending from Maxim support.
AI Generated Content

Hello,

I need some help in understanding the function of the video input clock CLK (Pin 53). Which pins and signals are supported by this clock? Regarding the description and functional block diagram in the datasheet it looks like CLK is for 24Bit color D[23:0] and HSYNC/VSYNC/DE at the same time. If this is correct so far, would it then fit with the output of an deserializer as the Max9276?

What im trying to do is to send HDMI data as RGB 24Bit color depth serialized from the output of ADV7619, deserialize it on the receiver side with Max9276 and convert it back into an HDMI signal with ADV7513. Therefore i would like to know if the output of Max9276 is compatible with the input of ADV7513.

Thanks for any helpful advice.

Best regards

Stell

MAX9276-MAX9280.pdf
Parents Reply Children
No Data