Hi all,
I want to develop one VGA interface.
My input is 24-bit parallel RGB data, HSYNC & VSYNC.
My output is VGA (Analog RGB data, HSYNC & VSYNC) on a standard DE-15 VGA connector.
My question is:
If I use any of the 2 encoders (ADV7120 or ADV7125) to convert the digital RGB inputs to analog RGB outputs,
will there be any problem if I do not provide the sync signals (HSYNC & VSYNC) to any of these encoders & directly
pass the sync signals (HSYNC & VSYNC) to the VGA connector ??
Will such a system work??