Post Go back to editing

ADV7181D Evaluation Board

For my application, I want to digitize black & white RS-170 video (essentially NTSC).  I have two different video types with slightly different timing.  Both are 640x480 active video.  I only have to digitize one at a time; I will have a mux in my actual design.  Here are the specs for each of my video signals:

Video #1

  • HSYNC: 15.750 kHz
  • VSYNC: 60 Hz
  • Active Resolution: 640x480
  • Total Resolution: 772x525
  • H: 63.49 us
  • H Active: 52.62 us

Video #2

  • HSYNC: 15.703 kHz
  • VSYNC: 60 Hz
  • Active Resolution: 640x480
  • Total Resolution: 796x525
  • H: 63.68 us
  • H Active: 51.2 us

Which input should I connect this video type to on the ADV7181D Evaluation Board?  Should I use the Standard Definition Processor or the Component Processor path in the ADV1781D chip?  Is there a predefined script that will allow me to output the digitized video onto the HDMI output?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.