Sir ,
I'm looking for video DAC instead of ADV7162 because of EOL.
Spec
1) Don't need Even/Odd pin
2) Parallel input and analog RGB output
Option
Is it possible Interlaced output ( *1280x1024 24bit 30frames )
Do you have similar device ?
Regards,
ADV7162
Obsolete
The ADV7160/ADV7162® is a 96-bit pixel port Video RAM-DAC with color enhanced triple 10-bit DACs. The device also includes a PLL and 64 x 64 hardware...
Datasheet
ADV7162 on Analog.com
Sir ,
I'm looking for video DAC instead of ADV7162 because of EOL.
Spec
1) Don't need Even/Odd pin
2) Parallel input and analog RGB output
Option
Is it possible Interlaced output ( *1280x1024 24bit 30frames )
Do you have similar device ?
Regards,
Have you looked at the AD9884A:
Thank you for your reply.
AD9984A is ADC. Do you have DAC solution ?
Regards,
Sorry about the mix up
The only video DACs available would be the ADV739x
ADV734x
But neither of these handle 24 bit RGB inputs.
Past this point you would have to use a standard DAC
Thank you for your advice !