Post Go back to editing

AD9984A+ADV8003

I would like to use AD9984A as the RGB input source, but i found that it can't output the DE signal or embed SAV/EAV signals. And the ADV8003's TTL input port needs the DE signal or the AV-CODE(SAV/EAV) signal. so how can i connect them in my design. 

Parents
  • Thanks all, and now i don't care using the ADV8005 or ADV8003, because the two device are compatible, my products need to receive a VGA signal which comes from the PC. and then converts the VGA signals to the 1080i50 or 576i50 format. so i must use a device which can receives the VGA' RGB signal ,such as the ADV7842 or the ADV7441, but i want to decrease   the cost, so i want to use the AD9984A instead of the ADV7842.

Reply
  • Thanks all, and now i don't care using the ADV8005 or ADV8003, because the two device are compatible, my products need to receive a VGA signal which comes from the PC. and then converts the VGA signals to the 1080i50 or 576i50 format. so i must use a device which can receives the VGA' RGB signal ,such as the ADV7842 or the ADV7441, but i want to decrease   the cost, so i want to use the AD9984A instead of the ADV7842.

Children
No Data