Post Go back to editing

Noise in the DVI Output of ADV7511W

Hi,

We are using ADV7511WBSWZ for DVI Output in our board. The set up is as shown in the attached image.

The cables used for connection are shielded.

We have observed that, there are white blinking dots on the output (On Monitor).

We tried to display only one primary color(any of the three) bar on the screen, with darker color the dots are not visible, but with lighter shades of the same color( with mix of other two primary color) dots are visible.

Have anyone have come across this kind of issue ?

Please help us to solve this issue ASAP.

Thanks & Regards,

Nanjunda M

Parents
  • Hi,

    We integrated the card in the system. The block diagram explains the situations after integrating the card 14 in the system.

    I have added block diagram of two situation.

    • Discontinuity at one location on external cable: Noise reduces completely
    • Discontinuity at two location on external cable: Noise still remains.

    Please can you look at the block diagram and comment on observation on noise.

    As per your below reply, touching pins add small capacitance.. can adding high frequency capacitor, btn pins will be helpful?

    Any suggestion on attending this type of noise?

    Regards,

    Vijetha

Reply
  • Hi,

    We integrated the card in the system. The block diagram explains the situations after integrating the card 14 in the system.

    I have added block diagram of two situation.

    • Discontinuity at one location on external cable: Noise reduces completely
    • Discontinuity at two location on external cable: Noise still remains.

    Please can you look at the block diagram and comment on observation on noise.

    As per your below reply, touching pins add small capacitance.. can adding high frequency capacitor, btn pins will be helpful?

    Any suggestion on attending this type of noise?

    Regards,

    Vijetha

Children
No Data