Hi,
I have some problem with separating capacitor C3. There is some distortions in videosignal, that you can see in the pictures.
Maybe you know the cause of this distortion?
Is there some way to solve this problem?
Thanks,
Dmitrii.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD9051
Production
The AD9051 is a complete 10-bit monolithic sampling analog-to-
digital converter (ADC) with an onboard track-and-hold and
reference. The unit is designed...
Datasheet
AD9051 on Analog.com
Hi,
I have some problem with separating capacitor C3. There is some distortions in videosignal, that you can see in the pictures.
Maybe you know the cause of this distortion?
Is there some way to solve this problem?
Thanks,
Dmitrii.
Hi,
We are looking in to your question.
Best Regards,
Jeyasudha.M
Hi Dmitrii,
There are several things that can contribute to elevated noise/distortion in High Speed ADC Applications. Assuming you have followed the High Speed ADC PCB layout best practices guidance provided at http://www.analog.com/en/search.html?q=High+Speed+ADC+Layout you may also want to consider the frequency characteristics of your Analog Input Source, and whether it is rated to drive a direct 0.1uF capacitance without additional buffering. In your schematic C3 serves to block the default DC bias coming from your source signal which allows the AC coupled input to assume the fixed 2.5V internal common mode of the AD9051 Analog Input (see Analog Input topic on d/s page 9). You also need to make sure your ADC CLK source is clean/low jitter to insure your analog input is being sampled correctly.
Best Regards,
TonyM