According to the table 1-1 in ITU-R BT.470-6, the line-blanking interval of PAL B/D/H/I/K/L should be 12us:


But when I measure the output of ADV7390, I found that it is about 10us. I have config ADV7390 by using the scripts in table 82. I think this is correct for ADV7390 when the input is set to BT656, because according to figure 104 in datasheet, the line-blanking interval should be 288 clock ( frequency is 27MHz and period is 37.037ns) , that is 288 x 37.037 = 10.6us.
But it is not conform to th BT470, and have ariased problems in some monitors ( most monitor is OK). How can I changed the line blanking interval to 12us?