Post Go back to editing

ADV7613 Control Code of FPGA

Hi All,

 

The ADV7613 Evaluation Board Schematic, in ADV7613 Design Support Files web page, shows that the ADV7613 is controlled by FPGA.

Could you send us the FPGA Source Code of the FPGA for controlling ADV7613?

My customer would like to use it as a reference code for his design.

 

Best Regards,

Ricky

Parents
  • Just to clarify: we do not give FPGA code design to customers/anyone using the EVAL-ADV7613FEBZ platform. The evaluation board is already programmed with the FPGA code. The use case of the ADV7613 is HDMI input in, LVDS output. The FPGA on-board allows us to interface to an HDMI output device (such as the ADV7511W) and nothing else.

Reply
  • Just to clarify: we do not give FPGA code design to customers/anyone using the EVAL-ADV7613FEBZ platform. The evaluation board is already programmed with the FPGA code. The use case of the ADV7613 is HDMI input in, LVDS output. The FPGA on-board allows us to interface to an HDMI output device (such as the ADV7511W) and nothing else.

Children
No Data