Post Go back to editing

ADV7513 recommended control flow and reference sample code for the I2C register settings

Thread Summary

The user seeks advice on the control flow and I2C register settings for configuring an ADV7513 to set output resolutions based on the EDID of a connected monitor. The final answer confirms that the register settings for ADV7511 and ADV7513 are similar, and suggests cross-checking the configuration with the ADV7511W Programming Guide and a reference script for additional video formats. The user's draft settings are generally correct but should be verified against the guide.
AI Generated Content
Category: Hardware

We are developing the FPGA-side I2C configuration for an ADV7513, where the output resolution is set according to the EDID of the connected monitor.

Target resolutions: Full HD@60Hz, XGA@60Hz, VGA@60/59.94Hz

The FPGA handles the following:

  • ADV7513 initialization
  • Monitor connect detection via the HPD signal
  • EDID readout after connection
  • Resolution setting per the EDID
  • ADV7513 reconfiguration on resolution change
  • HDMI output stop on disconnection

Q1. Could you advise a recommended control flow for this sequence, and provide any reference sample code for the I2C register settings?

Q2. Below are our initial settings, still in draft, based on the Quick Start guide. Please point out anything missing or unnecessary.

Offset Register Name Value Note
0x41 Power Down Control 0x10 Release power-down
0x98 Fixed Register 0x03 Internal analog core driver optimization (fixed)
0x9A Fixed Register (PLL) 0xE0 Internal PLL stabilization (enable high-speed serial clock)
0x9C Fixed Register 0x30 PLL filter / internal timing optimization (fixed)
0x9D Fixed Register 0x61 Clock line drive strength (fixed)
0xA2, 0xA3 Fixed Register 0xA4 Buffer bias adjustment (fixed)
0xE0 Fixed Register 0xD0 Internal state machine initialization
0xF9 Fixed Register 0x00 I2C address conflict prevention
0x3B Video Identification Code 0x00 VIC mode: Auto
0x94 Interrupt Enable 0xC0 Enable HPD interrupt
0x15 Video Input Format 0x00 24-bit RGB
0x16 Video Output Format / Input Option 0x30 Color Depth: 8-bit
0x17 Aspect Ratio 0x02 Aspect ratio 16:9
Thanks.

Regards,
Fujita

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.