Post Go back to editing

ADV7511 Sync Output Polarity Control

Thread Summary

The user is confused about the sync signal output polarity control of the ADV7511 when Sync Adjustment Register (0x41[1]) is disabled. The final answer confirms that 0x17[6:5] = 2'b00 results in pass-through polarity, while 2'b11 inverts the polarity. For 0x41[1] = 0, the settings 0x17[6:5] = 2'b00 and 2'b11 are correct for maintaining and inverting the input sync polarity, respectively.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADV7511


Hi all,

I am having some confusion regarding the sync signal output polarity control of the ADV7511 and would appreciate your help.

For my application using the ADV7511, I need to invert the polarity of the output sync signals.

However, in the ADV7511 Programming User Guide Rev. G, page 157, Register 0x17, the descriptions for Bit[6] Vsync Polarity and Bit[5] Hsync Polarity appear inconsistent when Sync Adjustment Register (0x41[1]) = 0 (Case 2).

I found the following two different descriptions:

0 = sync polarity pass through
1 = sync polarity invert


and

0 = High polarity
1 = Low polarity

This has caused some confusion.

(1)

For Case 2 (0x41[1] = 0), do you think the following description is a typo?

0 = High polarity
1 = Low polarity

(2)

My current settings are:

0x17[6:5] = 2'b00
0x41[1] = 0


With these settings, the behavior is as follows:

Negative-polarity VSYNC input → Negative-polarity VSYNC output
Negative-polarity HSYNC input → Negative-polarity HSYNC output

If I change the settings to:

0x17[6:5] = 2'b11
0x41[1] = 0


will the behavior become:

Negative-polarity VSYNC input → Positive-polarity VSYNC output
Negative-polarity HSYNC input → Positive-polarity HSYNC output

Could you please confirm whether this understanding is correct?

Thank you in advance for your support.

Best regards,

aimPoint

Parents
  • Hi,

      Please find the response below ,

    For Case 2 (0x41[1] = 0), do you think the following description is a typo?

      0 = High polarity
      1 = Low polarity

     Sync Adjustment Disabled:

         When sync adjustment register is disabled 0x41[1]=0, then ADV7511 does not generate any syncs. It either passthrough the input or inverts it.

      Please refer below timing diagram for reference,

    a. 0x17[6] = '0'(Passthrough) , Output polarity = Input polarity.

    b. 0x17[6] = '1'(Invert) , Output polarity = Opposite of Input polarity.

    Sync Adjustment Enabled:

        However when sync adjustment register is enabled 0x41[1]=1, ADV7511 internally regenerates the syncs. Here, 0x17[6] directly selects the polarity.

    0x17[6]=0 (Force Active high) , Regardless of the input polarity, the regenerated VSYNC is active high.

    0x17[6]=1 (Force Active low) , Regardless of the input polarity, the regenerated VSYNC is active low.

    Could you please confirm whether this understanding is correct ?

        Yes, the settings which related to "0x17[6:5] = 2'b00"  & "0x17[6:5] = 2'b11" are expected one.

    Thanks,

    Poornima S

  • Hi  Poornima-san 

    Thank you for your reply. It was very helpful.

    Best regards.

    aimPoint

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.