Post Go back to editing

Cannot output YCbCr 4:2:2 10-bit at 4K@30Hz.

Thread Summary

The user reports that 4K 30Hz YCbCr 4:2:2 10-bit output does not work on their setup, showing a free-run signal instead. The support engineer confirms that the ADV7625 evaluation board supports this format and suggests checking the register configuration. The user notes that the TMDS clock for YCbCr 4:2:2 is 297 MHz, which should be within the ADV7626's limit, and asks about the 4:2:2 to 4:4:4 up-conversion function.
AI Generated Content
Category: Hardware
Product Number: ADV7626

Outputting YCbCr 4:2:2 10-bit at 1080p 60Hz works fine.

However, at 4K 30Hz with YCbCr 4:2:2 10-bit, the display does not show an image; instead, a free-run signal is output.

It should be supported under the HDMI 1.4 standard—does the ADV7626 not support this?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.