KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADV7125
Production
The ADV7125 (ADV®) is a triple high speed, digital-to-analog
converter (DAC) on a single monolithic chip. It consists of three
high speed, 8-bit video...
Datasheet
ADV7125 on Analog.com
Hi,
We are using the ADV7125 For RGB-VGA Conversion in our Existing Design. However ,the device is now mentioned as NRND (Not Recommended for New Design) in ADI site.
Could you please suggest any suitable alternative part for the ADV7125 ?
Preferably, We are looking for Resolution - 1024 (W) x 768 (H) Max.
And also,Please suggest alternate part for ADV7393.
Thanks in advance,
G.Vigneshwari
024 (W) x 768 (H)
Hi All,
The recommended alternative for ADV7125 is ADV7123, and the recommended alternative for ADV7393 is ADV7392.
Thanks,
Ebin
Hi,
Please consider the ADV800x series. It offers many functionalities, however, it is bit costlier part.
Thanks,
Poornima S
Hi ,
The device (ADV7123) is now mentioned as NRND (Not Recommended for New Design) in ADI site.
Could you please suggest any suitable alternative part for the ADV7123 ?
Is ADV7123-EP part also NRND?
Thanks,
Vigneshwari G
Hi,
Please check whether the ADV8005(It has DAC as well as HDMI output) can meet your requirements since all other DAC parts are currently under NRND.
Thanks,
Poornima S
Hi mam,
I need a RGB-VGA converter DAC encoder Part, ADV8005 part mentioned Video Signal Processor.
Please Suggest the video DAC encoder alone.
Thanks,
Vigneshwari G
Hi,
This is the only part which is under recommended for new designs(RND) since rest of the DAC encoder are under 'Not recommended for new design(NRND)'.
Kindly note that, in the ADV8005, the pixel port can accept multiple input formats in both RGB and YPrPb color spaces.
If you are not willing to use ADV8005 then please check with ADV7802 ADC Part since Graphics digitization is supported by the ADV7802 it is capable of digitizing RGB graphics signals from VGA to SXGA rates and converting them into a digital RGB or YCrCb pixel output stream
Thanks,
Poornima S