We have a design that incorporates an ADV7842 as a 12 bit per channel analog to digital converter for HD component video. When we supply an HD video signal at 1080p24 (pixel clock 74.25MHz) we see excessive broadband noise in the captured image data at ~12 LSB (12 bit). This is twice the level of noise that we've measured from a commercial device that also happens to use an ADV7842 in the same experimental setup.
The ADV7842 feeds its data over 36bit per pixel parallel single clock / single edge to another chip on the board from Macro Image Technologies (MIT), that outputs a TMDS stream which is captured by a BlackMagic Design UltraStudio as HDMI. We have verified that if I generate a test pattern within the MIT chip, the data captured by the UltraStudio is bit perfect. Likewise, I have verified that a test pattern generated internally by the ADV7842 shows no noise.
We have tested this with a variety of analog sources generating a 50% gray full frame field as Y/Pb/Pr with sync on Y. The Y signal has a tri-level sync pulse extending 300mV below and above blanking level. The video is 0-700mV above blanking. The peak to peak of sync + video is 1V. For the grey test image, Pb and Pr at at 0V (AC coupled) and Y is active at 350mV.

In the current measurement setup, the DAC is showing <900 uV RMS noise on each of those channels during the active video region.
The video signal goes into the ADC using the datasheet suggested divider network of 24R series, 51R shunt, AC coupled via 100nF. This is a 0.68x divider and provides the 75R termination to match the source impedance.

The ADV7842 is has clamping enabled, and configured for a 300mV sync tip for AGC. Capturing at 12bits for the range of 0-1V (sync tip clamp level referenced), the least significant bit is 244uV (1V / 2^12). With source noise at 900uV, it is scaled down by the divider to 0.68x, with 612uV of RMS noise reaching the AIN pin of the ADC. So, we would expect to see 2.5 LSB of noise.
Note, this assumes that the ADC is noiseless. Given that no noise figure is published, we'll go with that assumption - particularly given that we have another device from another manufacturer that uses an ADV7842, and it exhibits 2x less measured noise than my device. This implies that the noise is my fault, not that of the ADV7842 intrinsically. I have tested two of my boards, and they both show the same excess noise.
The ADV7842 is configured with Automatic Gain Control (AGC) enabled with sync tip tracking. Reading back CP_AGC_GAIN returns 0x30F or 1.53x. So the digital gain stage should take the 2.5 LSB of noise and multiply it up to 3.8 LSB. However, we are measuring over 3x that at 12 LSB.
Here is a zoomed in section of a capture of the 50% grey field (unsure how well this will survive compression, but you should see the random noise):

We have the MIT chip set up to output 12bit YUV 4:4:4 TMDS, as the UltraStudio is only capable of capturing 10bit 4:2:2. While it can capture RGB 12bit, the source into the ADV7842 is Y/Pb/Pr, so we want the channels in the captures to match the channels being input into the ADC. Loading a captured YUV lossless TIFF file into R to analyze the noise, we see the following output:

The main things to note is the width of the histograms compared to the source, with RMS readings of 2.9mV versus the ~900uV measured RMS noise from the source. The noise spectrum is flat for Y, with the expected rolloff seen for Pb/Pr given that this is a 4:2:2 capture.
This capture was taken with the internal anti-aliasing filter _disabled_ on the ADV7842. If we set the AA filter to a cutoff of 10MHz, the noise spectrum remains basically the same (with the addition of some spurs that don't meaningfully contribute to the overall RMS noise):

This suggests that the noise is coming from after the AA stage, and thus is not a reflection of noise present at the Analog In pins of the ADV7842.
The ADV7842 has separate low noise LDO's powering PVDD and AVDD. The noise measured on those lines is low, with less than 1uV noise in the 0-37MHz band. Furthermore, injecting orders of magnitude more broadband noise directly into PVDD or AVDD does not change the measured noise spectra. VDD and CVDD are supplied by the boards general 1V8 digital supply, and while that supply is noisy (16mV broadband AC RMS), again, injecting further noise into those rails does not change the measured noise spectrum of the ADC output. The board is a 6 layer board with a continuous power plane for 1V8 and continuous single ground planes. Decoupling for PVDD and AVDD is directly under the BGA on the back of the board. REFP/N are decoupled as per the datasheet, close to their pins.

So, in short, we am seeing 12LSB of broadband noise that doesn't reflect the noise in our sources. The noise is not impacted by AA filter settings and is not wholly explained by the 1.5x AGC digital gain. Nor can we see a source of the noise on the rails supplying the ADV7842.
We have included a full dump of the registers below.
What should I be looking at next?
# ADV7842 full register dump map,map_i2c_7bit,reg,value_hex,value_dec,value_bin io,0x20,0x00,0x1E,30,00011110 io,0x20,0x01,0x41,65,01000001 io,0x20,0x02,0x70,112,01110000 io,0x20,0x03,0x42,66,01000010 io,0x20,0x04,0x42,66,01000010 io,0x20,0x05,0x2C,44,00101100 io,0x20,0x06,0xB6,182,10110110 io,0x20,0x07,0x54,84,01010100 io,0x20,0x08,0x14,20,00010100 io,0x20,0x09,0x00,0,00000000 io,0x20,0x0A,0x90,144,10010000 io,0x20,0x0B,0x44,68,01000100 io,0x20,0x0C,0x00,0,00000000 io,0x20,0x0D,0x1E,30,00011110 io,0x20,0x0E,0x0F,15,00001111 io,0x20,0x0F,0x1E,30,00011110 io,0x20,0x10,0x00,0,00000000 io,0x20,0x11,0x00,0,00000000 io,0x20,0x12,0xC0,192,11000000 io,0x20,0x13,0x0D,13,00001101 io,0x20,0x14,0x6A,106,01101010 io,0x20,0x15,0x00,0,00000000 io,0x20,0x16,0x43,67,01000011 io,0x20,0x17,0x5A,90,01011010 io,0x20,0x18,0x34,52,00110100 io,0x20,0x19,0x9E,158,10011110 io,0x20,0x1A,0x02,2,00000010 io,0x20,0x1B,0x00,0,00000000 io,0x20,0x1C,0x00,0,00000000 io,0x20,0x1D,0x00,0,00000000 io,0x20,0x1E,0x00,0,00000000 io,0x20,0x1F,0x00,0,00000000 io,0x20,0x20,0xF0,240,11110000 io,0x20,0x21,0x00,0,00000000 io,0x20,0x22,0x00,0,00000000 io,0x20,0x23,0x03,3,00000011 io,0x20,0x24,0x00,0,00000000 io,0x20,0x25,0x00,0,00000000 io,0x20,0x26,0x00,0,00000000 io,0x20,0x27,0x00,0,00000000 io,0x20,0x28,0x00,0,00000000 io,0x20,0x29,0x00,0,00000000 io,0x20,0x2A,0x00,0,00000000 io,0x20,0x2B,0x00,0,00000000 io,0x20,0x2C,0x00,0,00000000 io,0x20,0x2D,0x00,0,00000000 io,0x20,0x2E,0x00,0,00000000 io,0x20,0x2F,0x00,0,00000000 io,0x20,0x30,0x88,136,10001000 io,0x20,0x31,0x00,0,00000000 io,0x20,0x32,0x00,0,00000000 io,0x20,0x33,0x40,64,01000000 io,0x20,0x34,0x00,0,00000000 io,0x20,0x35,0x00,0,00000000 io,0x20,0x36,0x00,0,00000000 io,0x20,0x37,0x00,0,00000000 io,0x20,0x38,0x00,0,00000000 io,0x20,0x39,0x00,0,00000000 io,0x20,0x3A,0x00,0,00000000 io,0x20,0x3B,0x00,0,00000000 io,0x20,0x3C,0x00,0,00000000 io,0x20,0x3D,0x00,0,00000000 io,0x20,0x3E,0x00,0,00000000 io,0x20,0x3F,0x00,0,00000000 io,0x20,0x40,0x20,32,00100000 io,0x20,0x41,0x30,48,00110000 io,0x20,0x42,0x94,148,10010100 io,0x20,0x43,0x00,0,00000000 io,0x20,0x44,0x00,0,00000000 io,0x20,0x45,0x00,0,00000000 io,0x20,0x46,0x00,0,00000000 io,0x20,0x47,0x00,0,00000000 io,0x20,0x48,0x00,0,00000000 io,0x20,0x49,0x00,0,00000000 io,0x20,0x4A,0x00,0,00000000 io,0x20,0x4B,0x00,0,00000000 io,0x20,0x4C,0x00,0,00000000 io,0x20,0x4D,0x00,0,00000000 io,0x20,0x4E,0x00,0,00000000 io,0x20,0x4F,0x00,0,00000000 io,0x20,0x50,0x00,0,00000000 io,0x20,0x51,0x00,0,00000000 io,0x20,0x52,0x00,0,00000000 io,0x20,0x53,0x00,0,00000000 io,0x20,0x54,0x00,0,00000000 io,0x20,0x55,0x00,0,00000000 io,0x20,0x56,0x85,133,10000101 io,0x20,0x57,0x00,0,00000000 io,0x20,0x58,0x00,0,00000000 io,0x20,0x59,0x00,0,00000000 io,0x20,0x5A,0x00,0,00000000 io,0x20,0x5B,0xBB,187,10111011 io,0x20,0x5C,0x00,0,00000000 io,0x20,0x5D,0x00,0,00000000 io,0x20,0x5E,0x00,0,00000000 io,0x20,0x5F,0x00,0,00000000 io,0x20,0x60,0x00,0,00000000 io,0x20,0x61,0x00,0,00000000 io,0x20,0x62,0x00,0,00000000 io,0x20,0x63,0x00,0,00000000 io,0x20,0x64,0x00,0,00000000 io,0x20,0x65,0x40,64,01000000 io,0x20,0x66,0x00,0,00000000 io,0x20,0x67,0x00,0,00000000 io,0x20,0x68,0x00,0,00000000 io,0x20,0x69,0x00,0,00000000 io,0x20,0x6A,0x00,0,00000000 io,0x20,0x6B,0x00,0,00000000 io,0x20,0x6C,0x00,0,00000000 io,0x20,0x6D,0x00,0,00000000 io,0x20,0x6E,0x00,0,00000000 io,0x20,0x6F,0x00,0,00000000 io,0x20,0x70,0x00,0,00000000 io,0x20,0x71,0x00,0,00000000 io,0x20,0x72,0x00,0,00000000 io,0x20,0x73,0x00,0,00000000 io,0x20,0x74,0x00,0,00000000 io,0x20,0x75,0x00,0,00000000 io,0x20,0x76,0x00,0,00000000 io,0x20,0x77,0x00,0,00000000 io,0x20,0x78,0x00,0,00000000 io,0x20,0x79,0x00,0,00000000 io,0x20,0x7A,0x00,0,00000000 io,0x20,0x7B,0x00,0,00000000 io,0x20,0x7C,0x00,0,00000000 io,0x20,0x7D,0x00,0,00000000 io,0x20,0x7E,0x00,0,00000000 io,0x20,0x7F,0x00,0,00000000 io,0x20,0x80,0x00,0,00000000 io,0x20,0x81,0x00,0,00000000 io,0x20,0x82,0x00,0,00000000 io,0x20,0x83,0x00,0,00000000 io,0x20,0x84,0x00,0,00000000 io,0x20,0x85,0x00,0,00000000 io,0x20,0x86,0x00,0,00000000 io,0x20,0x87,0x00,0,00000000 io,0x20,0x88,0x00,0,00000000 io,0x20,0x89,0x00,0,00000000 io,0x20,0x8A,0x00,0,00000000 io,0x20,0x8B,0x00,0,00000000 io,0x20,0x8C,0x00,0,00000000 io,0x20,0x8D,0x00,0,00000000 io,0x20,0x8E,0x00,0,00000000 io,0x20,0x8F,0x00,0,00000000 io,0x20,0x90,0x00,0,00000000 io,0x20,0x91,0x00,0,00000000 io,0x20,0x92,0x00,0,00000000 io,0x20,0x93,0x00,0,00000000 io,0x20,0x94,0x00,0,00000000 io,0x20,0x95,0x00,0,00000000 io,0x20,0x96,0x00,0,00000000 io,0x20,0x97,0x00,0,00000000 io,0x20,0x98,0x00,0,00000000 io,0x20,0x99,0x00,0,00000000 io,0x20,0x9A,0x00,0,00000000 io,0x20,0x9B,0x00,0,00000000 io,0x20,0x9C,0x00,0,00000000 io,0x20,0x9D,0x00,0,00000000 io,0x20,0x9E,0x00,0,00000000 io,0x20,0x9F,0x00,0,00000000 io,0x20,0xA0,0x00,0,00000000 io,0x20,0xA1,0x00,0,00000000 io,0x20,0xA2,0x00,0,00000000 io,0x20,0xA3,0x00,0,00000000 io,0x20,0xA4,0x00,0,00000000 io,0x20,0xA5,0x00,0,00000000 io,0x20,0xA6,0x00,0,00000000 io,0x20,0xA7,0x00,0,00000000 io,0x20,0xA8,0x00,0,00000000 io,0x20,0xA9,0x00,0,00000000 io,0x20,0xAA,0x00,0,00000000 io,0x20,0xAB,0x00,0,00000000 io,0x20,0xAC,0x00,0,00000000 io,0x20,0xAD,0x00,0,00000000 io,0x20,0xAE,0x00,0,00000000 io,0x20,0xAF,0x00,0,00000000 io,0x20,0xB0,0x00,0,00000000 io,0x20,0xB1,0x00,0,00000000 io,0x20,0xB2,0x00,0,00000000 io,0x20,0xB3,0x00,0,00000000 io,0x20,0xB4,0x00,0,00000000 io,0x20,0xB5,0x00,0,00000000 io,0x20,0xB6,0x00,0,00000000 io,0x20,0xB7,0x43,67,01000011 io,0x20,0xB8,0xE0,224,11100000 io,0x20,0xB9,0x00,0,00000000 io,0x20,0xBA,0x00,0,00000000 io,0x20,0xBB,0x00,0,00000000 io,0x20,0xBC,0x00,0,00000000 io,0x20,0xBD,0x00,0,00000000 io,0x20,0xBE,0x00,0,00000000 io,0x20,0xBF,0x00,0,00000000 io,0x20,0xC0,0x00,0,00000000 io,0x20,0xC1,0x0E,14,00001110 io,0x20,0xC2,0x00,0,00000000 io,0x20,0xC3,0x00,0,00000000 io,0x20,0xC4,0x00,0,00000000 io,0x20,0xC5,0x00,0,00000000 io,0x20,0xC6,0x00,0,00000000 io,0x20,0xC7,0x00,0,00000000 io,0x20,0xC8,0x00,0,00000000 io,0x20,0xC9,0x00,0,00000000 io,0x20,0xCA,0x00,0,00000000 io,0x20,0xCB,0x00,0,00000000 io,0x20,0xCC,0x00,0,00000000 io,0x20,0xCD,0x00,0,00000000 io,0x20,0xCE,0x00,0,00000000 io,0x20,0xCF,0x00,0,00000000 io,0x20,0xD0,0x00,0,00000000 io,0x20,0xD1,0x07,7,00000111 io,0x20,0xD2,0xEA,234,11101010 io,0x20,0xD3,0x82,130,10000010 io,0x20,0xD4,0x57,87,01010111 io,0x20,0xD5,0x00,0,00000000 io,0x20,0xD6,0x00,0,00000000 io,0x20,0xD7,0x00,0,00000000 io,0x20,0xD8,0x2D,45,00101101 io,0x20,0xD9,0x15,21,00010101 io,0x20,0xDA,0xF1,241,11110001 io,0x20,0xDB,0x5F,95,01011111 io,0x20,0xDC,0x40,64,01000000 io,0x20,0xDD,0x00,0,00000000 io,0x20,0xDE,0x00,0,00000000 io,0x20,0xDF,0x00,0,00000000 io,0x20,0xE0,0x00,0,00000000 io,0x20,0xE1,0x00,0,00000000 io,0x20,0xE2,0x04,4,00000100 io,0x20,0xE3,0x00,0,00000000 io,0x20,0xE4,0x01,1,00000001 io,0x20,0xE5,0x00,0,00000000 io,0x20,0xE6,0x00,0,00000000 io,0x20,0xE7,0x00,0,00000000 io,0x20,0xE8,0x04,4,00000100 io,0x20,0xE9,0x00,0,00000000 io,0x20,0xEA,0x20,32,00100000 io,0x20,0xEB,0x12,18,00010010 io,0x20,0xEC,0x00,0,00000000 io,0x20,0xED,0x00,0,00000000 io,0x20,0xEE,0x00,0,00000000 io,0x20,0xEF,0x00,0,00000000 io,0x20,0xF0,0x00,0,00000000 io,0x20,0xF1,0x44,68,01000100 io,0x20,0xF2,0x4A,74,01001010 io,0x20,0xF3,0x00,0,00000000 io,0x20,0xF4,0x00,0,00000000 io,0x20,0xF5,0x00,0,00000000 io,0x20,0xF6,0x00,0,00000000 io,0x20,0xF7,0x00,0,00000000 io,0x20,0xF8,0x48,72,01001000 io,0x20,0xF9,0x00,0,00000000 io,0x20,0xFA,0x00,0,00000000 io,0x20,0xFB,0x00,0,00000000 io,0x20,0xFC,0x00,0,00000000 io,0x20,0xFD,0x46,70,01000110 io,0x20,0xFE,0x00,0,00000000 io,0x20,0xFF,0x00,0,00000000 cp,0x23,0x00,0x00,0,00000000 cp,0x23,0x01,0x00,0,00000000 cp,0x23,0x02,0x00,0,00000000 cp,0x23,0x03,0x00,0,00000000 cp,0x23,0x04,0x00,0,00000000 cp,0x23,0x05,0x00,0,00000000 cp,0x23,0x06,0x00,0,00000000 cp,0x23,0x07,0x00,0,00000000 cp,0x23,0x08,0x00,0,00000000 cp,0x23,0x09,0x02,2,00000010 cp,0x23,0x0A,0x00,0,00000000 cp,0x23,0x0B,0x40,64,01000000 cp,0x23,0x0C,0x00,0,00000000 cp,0x23,0x0D,0x00,0,00000000 cp,0x23,0x0E,0x00,0,00000000 cp,0x23,0x0F,0x00,0,00000000 cp,0x23,0x10,0x08,8,00001000 cp,0x23,0x11,0x00,0,00000000 cp,0x23,0x12,0x00,0,00000000 cp,0x23,0x13,0x00,0,00000000 cp,0x23,0x14,0x00,0,00000000 cp,0x23,0x15,0x01,1,00000001 cp,0x23,0x16,0x00,0,00000000 cp,0x23,0x17,0x00,0,00000000 cp,0x23,0x18,0x00,0,00000000 cp,0x23,0x19,0x00,0,00000000 cp,0x23,0x1A,0x00,0,00000000 cp,0x23,0x1B,0x20,32,00100000 cp,0x23,0x1C,0x00,0,00000000 cp,0x23,0x1D,0x00,0,00000000 cp,0x23,0x1E,0x00,0,00000000 cp,0x23,0x1F,0x00,0,00000000 cp,0x23,0x20,0x20,32,00100000 cp,0x23,0x21,0x00,0,00000000 cp,0x23,0x22,0x00,0,00000000 cp,0x23,0x23,0x00,0,00000000 cp,0x23,0x24,0x00,0,00000000 cp,0x23,0x25,0x00,0,00000000 cp,0x23,0x26,0x00,0,00000000 cp,0x23,0x27,0x00,0,00000000 cp,0x23,0x28,0x00,0,00000000 cp,0x23,0x29,0x00,0,00000000 cp,0x23,0x2A,0x00,0,00000000 cp,0x23,0x2B,0x00,0,00000000 cp,0x23,0x2C,0x00,0,00000000 cp,0x23,0x2D,0x00,0,00000000 cp,0x23,0x2E,0x00,0,00000000 cp,0x23,0x2F,0x00,0,00000000 cp,0x23,0x30,0x00,0,00000000 cp,0x23,0x31,0x00,0,00000000 cp,0x23,0x32,0x00,0,00000000 cp,0x23,0x33,0x00,0,00000000 cp,0x23,0x34,0x00,0,00000000 cp,0x23,0x35,0x00,0,00000000 cp,0x23,0x36,0x00,0,00000000 cp,0x23,0x37,0x00,0,00000000 cp,0x23,0x38,0x00,0,00000000 cp,0x23,0x39,0x00,0,00000000 cp,0x23,0x3A,0x80,128,10000000 cp,0x23,0x3B,0x80,128,10000000 cp,0x23,0x3C,0x00,0,00000000 cp,0x23,0x3D,0x00,0,00000000 cp,0x23,0x3E,0x04,4,00000100 cp,0x23,0x3F,0x00,0,00000000 cp,0x23,0x40,0x82,130,10000010 cp,0x23,0x41,0x1A,26,00011010 cp,0x23,0x42,0x3B,59,00111011 cp,0x23,0x43,0xD4,212,11010100 cp,0x23,0x44,0x03,3,00000011 cp,0x23,0x45,0x33,51,00110011 cp,0x23,0x46,0x00,0,00000000 cp,0x23,0x47,0x00,0,00000000 cp,0x23,0x48,0x00,0,00000000 cp,0x23,0x49,0xA1,161,10100001 cp,0x23,0x4A,0x1C,28,00011100 cp,0x23,0x4B,0x2C,44,00101100 cp,0x23,0x4C,0x64,100,01100100 cp,0x23,0x4D,0x12,18,00010010 cp,0x23,0x4E,0x35,53,00110101 cp,0x23,0x4F,0xFF,255,11111111 cp,0x23,0x50,0xC0,192,11000000 cp,0x23,0x51,0x00,0,00000000 cp,0x23,0x52,0x40,64,01000000 cp,0x23,0x53,0x00,0,00000000 cp,0x23,0x54,0x00,0,00000000 cp,0x23,0x55,0x00,0,00000000 cp,0x23,0x56,0x00,0,00000000 cp,0x23,0x57,0x08,8,00001000 cp,0x23,0x58,0x00,0,00000000 cp,0x23,0x59,0x00,0,00000000 cp,0x23,0x5A,0x00,0,00000000 cp,0x23,0x5B,0x00,0,00000000 cp,0x23,0x5C,0x01,1,00000001 cp,0x23,0x5D,0x00,0,00000000 cp,0x23,0x5E,0x00,0,00000000 cp,0x23,0x5F,0x00,0,00000000 cp,0x23,0x60,0x00,0,00000000 cp,0x23,0x61,0x00,0,00000000 cp,0x23,0x62,0x20,32,00100000 cp,0x23,0x63,0x00,0,00000000 cp,0x23,0x64,0x00,0,00000000 cp,0x23,0x65,0x00,0,00000000 cp,0x23,0x66,0x00,0,00000000 cp,0x23,0x67,0x00,0,00000000 cp,0x23,0x68,0xF0,240,11110000 cp,0x23,0x69,0x04,4,00000100 cp,0x23,0x6A,0x00,0,00000000 cp,0x23,0x6B,0x00,0,00000000 cp,0x23,0x6C,0x10,16,00010000 cp,0x23,0x6D,0x00,0,00000000 cp,0x23,0x6E,0x00,0,00000000 cp,0x23,0x6F,0x00,0,00000000 cp,0x23,0x70,0x00,0,00000000 cp,0x23,0x71,0x00,0,00000000 cp,0x23,0x72,0x00,0,00000000 cp,0x23,0x73,0x50,80,01010000 cp,0x23,0x74,0x04,4,00000100 cp,0x23,0x75,0x01,1,00000001 cp,0x23,0x76,0x00,0,00000000 cp,0x23,0x77,0xFF,255,11111111 cp,0x23,0x78,0xFF,255,11111111 cp,0x23,0x79,0xFF,255,11111111 cp,0x23,0x7A,0xFF,255,11111111 cp,0x23,0x7B,0x05,5,00000101 cp,0x23,0x7C,0xC0,192,11000000 cp,0x23,0x7D,0x00,0,00000000 cp,0x23,0x7E,0x00,0,00000000 cp,0x23,0x7F,0x00,0,00000000 cp,0x23,0x80,0x00,0,00000000 cp,0x23,0x81,0xC0,192,11000000 cp,0x23,0x82,0x04,4,00000100 cp,0x23,0x83,0x00,0,00000000 cp,0x23,0x84,0x0C,12,00001100 cp,0x23,0x85,0x0B,11,00001011 cp,0x23,0x86,0x0B,11,00001011 cp,0x23,0x87,0x00,0,00000000 cp,0x23,0x88,0x00,0,00000000 cp,0x23,0x89,0x00,0,00000000 cp,0x23,0x8A,0x20,32,00100000 cp,0x23,0x8B,0x40,64,01000000 cp,0x23,0x8C,0x04,4,00000100 cp,0x23,0x8D,0x00,0,00000000 cp,0x23,0x8E,0x00,0,00000000 cp,0x23,0x8F,0x40,64,01000000 cp,0x23,0x90,0x00,0,00000000 cp,0x23,0x91,0x40,64,01000000 cp,0x23,0x92,0x00,0,00000000 cp,0x23,0x93,0x00,0,00000000 cp,0x23,0x94,0x00,0,00000000 cp,0x23,0x95,0x00,0,00000000 cp,0x23,0x96,0x00,0,00000000 cp,0x23,0x97,0xF0,240,11110000 cp,0x23,0x98,0x00,0,00000000 cp,0x23,0x99,0x00,0,00000000 cp,0x23,0x9A,0x00,0,00000000 cp,0x23,0x9B,0x00,0,00000000 cp,0x23,0x9C,0x00,0,00000000 cp,0x23,0x9D,0x00,0,00000000 cp,0x23,0x9E,0x00,0,00000000 cp,0x23,0x9F,0x00,0,00000000 cp,0x23,0xA0,0x00,0,00000000 cp,0x23,0xA1,0x00,0,00000000 cp,0x23,0xA2,0x00,0,00000000 cp,0x23,0xA3,0x00,0,00000000 cp,0x23,0xA4,0x00,0,00000000 cp,0x23,0xA5,0x00,0,00000000 cp,0x23,0xA6,0x00,0,00000000 cp,0x23,0xA7,0x00,0,00000000 cp,0x23,0xA8,0x00,0,00000000 cp,0x23,0xA9,0x00,0,00000000 cp,0x23,0xAA,0x00,0,00000000 cp,0x23,0xAB,0x00,0,00000000 cp,0x23,0xAC,0x00,0,00000000 cp,0x23,0xAD,0x00,0,00000000 cp,0x23,0xAE,0x60,96,01100000 cp,0x23,0xAF,0x00,0,00000000 cp,0x23,0xB0,0x00,0,00000000 cp,0x23,0xB1,0xA1,161,10100001 cp,0x23,0xB2,0x1C,28,00011100 cp,0x23,0xB3,0x2C,44,00101100 cp,0x23,0xB4,0x64,100,01100100 cp,0x23,0xB5,0xFD,253,11111101 cp,0x23,0xB6,0x00,0,00000000 cp,0x23,0xB7,0x4A,74,01001010 cp,0x23,0xB8,0x12,18,00010010 cp,0x23,0xB9,0x35,53,00110101 cp,0x23,0xBA,0x01,1,00000001 cp,0x23,0xBB,0x00,0,00000000 cp,0x23,0xBC,0x00,0,00000000 cp,0x23,0xBD,0x18,24,00011000 cp,0x23,0xBE,0x00,0,00000000 cp,0x23,0xBF,0x00,0,00000000 cp,0x23,0xC0,0x00,0,00000000 cp,0x23,0xC1,0x00,0,00000000 cp,0x23,0xC2,0x00,0,00000000 cp,0x23,0xC3,0x39,57,00111001 cp,0x23,0xC4,0x44,68,01000100 cp,0x23,0xC5,0x91,145,10010001 cp,0x23,0xC6,0x00,0,00000000 cp,0x23,0xC7,0x00,0,00000000 cp,0x23,0xC8,0x00,0,00000000 cp,0x23,0xC9,0x2C,44,00101100 cp,0x23,0xCA,0x00,0,00000000 cp,0x23,0xCB,0x60,96,01100000 cp,0x23,0xCC,0x42,66,01000010 cp,0x23,0xCD,0xFF,255,11111111 cp,0x23,0xCE,0x3F,63,00111111 cp,0x23,0xCF,0x00,0,00000000 cp,0x23,0xD0,0x00,0,00000000 cp,0x23,0xD1,0x00,0,00000000 cp,0x23,0xD2,0x00,0,00000000 cp,0x23,0xD3,0x00,0,00000000 cp,0x23,0xD4,0x00,0,00000000 cp,0x23,0xD5,0x00,0,00000000 cp,0x23,0xD6,0x00,0,00000000 cp,0x23,0xD7,0x00,0,00000000 cp,0x23,0xD8,0x00,0,00000000 cp,0x23,0xD9,0x00,0,00000000 cp,0x23,0xDA,0x00,0,00000000 cp,0x23,0xDB,0x19,25,00011001 cp,0x23,0xDC,0x64,100,01100100 cp,0x23,0xDD,0x12,18,00010010 cp,0x23,0xDE,0xC5,197,11000101 cp,0x23,0xDF,0x78,120,01111000 cp,0x23,0xE0,0x53,83,01010011 cp,0x23,0xE1,0xFF,255,11111111 cp,0x23,0xE2,0xFF,255,11111111 cp,0x23,0xE3,0x1C,28,00011100 cp,0x23,0xE4,0x00,0,00000000 cp,0x23,0xE5,0x00,0,00000000 cp,0x23,0xE6,0x99,153,10011001 cp,0x23,0xE7,0x02,2,00000010 cp,0x23,0xE8,0x33,51,00110011 cp,0x23,0xE9,0x01,1,00000001 cp,0x23,0xEA,0x03,3,00000011 cp,0x23,0xEB,0x09,9,00001001 cp,0x23,0xEC,0x3A,58,00111010 cp,0x23,0xED,0x10,16,00010000 cp,0x23,0xEE,0x0A,10,00001010 cp,0x23,0xEF,0x05,5,00000101 cp,0x23,0xF0,0x05,5,00000101 cp,0x23,0xF1,0x40,64,01000000 cp,0x23,0xF2,0x04,4,00000100 cp,0x23,0xF3,0xE4,228,11100100 cp,0x23,0xF4,0x00,0,00000000 cp,0x23,0xF5,0x00,0,00000000 cp,0x23,0xF6,0x00,0,00000000 cp,0x23,0xF7,0x15,21,00010101 cp,0x23,0xF8,0x03,3,00000011 cp,0x23,0xF9,0x33,51,00110011 cp,0x23,0xFA,0x06,6,00000110 cp,0x23,0xFB,0x57,87,01010111 cp,0x23,0xFC,0x04,4,00000100 cp,0x23,0xFD,0x65,101,01100101 cp,0x23,0xFE,0x03,3,00000011 cp,0x23,0xFF,0x08,8,00001000 afe,0x24,0x00,0x00,0,00000000 afe,0x24,0x01,0x06,6,00000110 afe,0x24,0x02,0xC0,192,11000000 afe,0x24,0x03,0x12,18,00010010 afe,0x24,0x04,0x30,48,00110000 afe,0x24,0x05,0x0F,15,00001111 afe,0x24,0x06,0x00,0,00000000 afe,0x24,0x07,0x1F,31,00011111 afe,0x24,0x08,0x00,0,00000000 afe,0x24,0x09,0x00,0,00000000 afe,0x24,0x0A,0x00,0,00000000 afe,0x24,0x0B,0x00,0,00000000 afe,0x24,0x0C,0x0D,13,00001101 afe,0x24,0x0D,0x13,19,00010011 afe,0x24,0x0E,0x00,0,00000000 afe,0x24,0x0F,0x90,144,10010000 afe,0x24,0x10,0x30,48,00110000 afe,0x24,0x11,0x82,130,10000010 afe,0x24,0x12,0xFF,255,11111111 afe,0x24,0x13,0x00,0,00000000 afe,0x24,0x14,0x09,9,00001001 afe,0x24,0x15,0x0A,10,00001010 afe,0x24,0x16,0x98,152,10011000 afe,0x24,0x17,0x00,0,00000000 afe,0x24,0x18,0x00,0,00000000 afe,0x24,0x19,0x00,0,00000000 afe,0x24,0x1A,0x00,0,00000000 afe,0x24,0x1B,0x00,0,00000000 afe,0x24,0x1C,0x00,0,00000000 afe,0x24,0x1D,0x6D,109,01101101 afe,0x24,0x1E,0x6D,109,01101101 afe,0x24,0x1F,0x6D,109,01101101 afe,0x24,0x20,0x6D,109,01101101 afe,0x24,0x21,0x6D,109,01101101 afe,0x24,0x22,0x6D,109,01101101 afe,0x24,0x23,0x6D,109,01101101 afe,0x24,0x24,0x6D,109,01101101 afe,0x24,0x25,0x00,0,00000000 afe,0x24,0x26,0x08,8,00001000 afe,0x24,0x27,0xFF,255,11111111 afe,0x24,0x28,0xFF,255,11111111 afe,0x24,0x29,0x00,0,00000000 afe,0x24,0x2A,0x00,0,00000000 afe,0x24,0x2B,0x00,0,00000000 afe,0x24,0x2C,0x00,0,00000000 afe,0x24,0x2D,0x00,0,00000000 afe,0x24,0x2E,0x00,0,00000000 afe,0x24,0x2F,0x00,0,00000000 afe,0x24,0x30,0x00,0,00000000 afe,0x24,0x31,0x00,0,00000000 afe,0x24,0x32,0x00,0,00000000 afe,0x24,0x33,0x00,0,00000000 afe,0x24,0x34,0x00,0,00000000 afe,0x24,0x35,0x00,0,00000000 afe,0x24,0x36,0x00,0,00000000 afe,0x24,0x37,0x00,0,00000000 afe,0x24,0x38,0x00,0,00000000 afe,0x24,0x39,0x00,0,00000000 afe,0x24,0x3A,0x00,0,00000000 afe,0x24,0x3B,0x00,0,00000000 afe,0x24,0x3C,0x00,0,00000000 afe,0x24,0x3D,0x00,0,00000000 afe,0x24,0x3E,0x00,0,00000000 afe,0x24,0x3F,0x00,0,00000000 afe,0x24,0x40,0x00,0,00000000 afe,0x24,0x41,0x00,0,00000000 afe,0x24,0x42,0x00,0,00000000 afe,0x24,0x43,0x00,0,00000000 afe,0x24,0x44,0x00,0,00000000 afe,0x24,0x45,0x00,0,00000000 afe,0x24,0x46,0x00,0,00000000 afe,0x24,0x47,0x00,0,00000000 afe,0x24,0x48,0x00,0,00000000 afe,0x24,0x49,0x00,0,00000000 afe,0x24,0x4A,0x00,0,00000000 afe,0x24,0x4B,0x00,0,00000000 afe,0x24,0x4C,0x00,0,00000000 afe,0x24,0x4D,0x00,0,00000000 afe,0x24,0x4E,0x00,0,00000000 afe,0x24,0x4F,0x00,0,00000000 afe,0x24,0x50,0x00,0,00000000 afe,0x24,0x51,0x00,0,00000000 afe,0x24,0x52,0x00,0,00000000 afe,0x24,0x53,0x00,0,00000000 afe,0x24,0x54,0x00,0,00000000 afe,0x24,0x55,0x00,0,00000000 afe,0x24,0x56,0x00,0,00000000 afe,0x24,0x57,0x00,0,00000000 afe,0x24,0x58,0x00,0,00000000 afe,0x24,0x59,0x00,0,00000000 afe,0x24,0x5A,0x00,0,00000000 afe,0x24,0x5B,0x00,0,00000000 afe,0x24,0x5C,0x00,0,00000000 afe,0x24,0x5D,0x00,0,00000000 afe,0x24,0x5E,0x00,0,00000000 afe,0x24,0x5F,0x00,0,00000000 afe,0x24,0x60,0x00,0,00000000 afe,0x24,0x61,0x00,0,00000000 afe,0x24,0x62,0x00,0,00000000 afe,0x24,0x63,0x00,0,00000000 afe,0x24,0x64,0x00,0,00000000 afe,0x24,0x65,0x00,0,00000000 afe,0x24,0x66,0x00,0,00000000 afe,0x24,0x67,0x00,0,00000000 afe,0x24,0x68,0x00,0,00000000 afe,0x24,0x69,0x00,0,00000000 afe,0x24,0x6A,0x00,0,00000000 afe,0x24,0x6B,0x00,0,00000000 afe,0x24,0x6C,0x00,0,00000000 afe,0x24,0x6D,0x00,0,00000000 afe,0x24,0x6E,0x00,0,00000000 afe,0x24,0x6F,0x00,0,00000000 afe,0x24,0x70,0x00,0,00000000 afe,0x24,0x71,0x00,0,00000000 afe,0x24,0x72,0x00,0,00000000 afe,0x24,0x73,0x00,0,00000000 afe,0x24,0x74,0x00,0,00000000 afe,0x24,0x75,0x00,0,00000000 afe,0x24,0x76,0x00,0,00000000 afe,0x24,0x77,0x00,0,00000000 afe,0x24,0x78,0x00,0,00000000 afe,0x24,0x79,0x00,0,00000000 afe,0x24,0x7A,0x00,0,00000000 afe,0x24,0x7B,0x00,0,00000000 afe,0x24,0x7C,0x00,0,00000000 afe,0x24,0x7D,0x00,0,00000000 afe,0x24,0x7E,0x00,0,00000000 afe,0x24,0x7F,0x00,0,00000000 afe,0x24,0x80,0x80,128,10000000 afe,0x24,0x81,0x20,32,00100000 afe,0x24,0x82,0x80,128,10000000 afe,0x24,0x83,0x02,2,00000010 afe,0x24,0x84,0x02,2,00000010 afe,0x24,0x85,0x0A,10,00001010 afe,0x24,0x86,0x0A,10,00001010 afe,0x24,0x87,0x0A,10,00001010 afe,0x24,0x88,0xF8,248,11111000 afe,0x24,0x89,0x66,102,01100110 afe,0x24,0x8A,0xFC,252,11111100 afe,0x24,0x8B,0x13,19,00010011 afe,0x24,0x8C,0xF8,248,11111000 afe,0x24,0x8D,0x15,21,00010101 afe,0x24,0x8E,0xDE,222,11011110 afe,0x24,0x8F,0x86,134,10000110 afe,0x24,0x90,0xC1,193,11000001 afe,0x24,0x91,0x91,145,10010001 afe,0x24,0x92,0x82,130,10000010 afe,0x24,0x93,0x70,112,01110000 afe,0x24,0x94,0x00,0,00000000 afe,0x24,0x95,0x00,0,00000000 afe,0x24,0x96,0x00,0,00000000 afe,0x24,0x97,0x00,0,00000000 afe,0x24,0x98,0xFF,255,11111111 afe,0x24,0x99,0x0F,15,00001111 afe,0x24,0x9A,0xFF,255,11111111 afe,0x24,0x9B,0x00,0,00000000 afe,0x24,0x9C,0x00,0,00000000 afe,0x24,0x9D,0x00,0,00000000 afe,0x24,0x9E,0x00,0,00000000 afe,0x24,0x9F,0x00,0,00000000 afe,0x24,0xA0,0x00,0,00000000 afe,0x24,0xA1,0x02,2,00000010 afe,0x24,0xA2,0x02,2,00000010 afe,0x24,0xA3,0xFF,255,11111111 afe,0x24,0xA4,0xFF,255,11111111 afe,0x24,0xA5,0xFF,255,11111111 afe,0x24,0xA6,0xF8,248,11111000 afe,0x24,0xA7,0x66,102,01100110 afe,0x24,0xA8,0xFC,252,11111100 afe,0x24,0xA9,0x13,19,00010011 afe,0x24,0xAA,0xF8,248,11111000 afe,0x24,0xAB,0x15,21,00010101 afe,0x24,0xAC,0xDE,222,11011110 afe,0x24,0xAD,0x86,134,10000110 afe,0x24,0xAE,0xC1,193,11000001 afe,0x24,0xAF,0x91,145,10010001 afe,0x24,0xB0,0x82,130,10000010 afe,0x24,0xB1,0x70,112,01110000 afe,0x24,0xB2,0xFF,255,11111111 afe,0x24,0xB3,0x0F,15,00001111 afe,0x24,0xB4,0xFF,255,11111111 afe,0x24,0xB5,0x01,1,00000001 afe,0x24,0xB6,0x00,0,00000000 afe,0x24,0xB7,0x00,0,00000000 afe,0x24,0xB8,0x00,0,00000000 afe,0x24,0xB9,0x00,0,00000000 afe,0x24,0xBA,0x00,0,00000000 afe,0x24,0xBB,0x00,0,00000000 afe,0x24,0xBC,0x00,0,00000000 afe,0x24,0xBD,0x6F,111,01101111 afe,0x24,0xBE,0x02,2,00000010 afe,0x24,0xBF,0xFA,250,11111010 afe,0x24,0xC0,0xC0,192,11000000 afe,0x24,0xC1,0x98,152,10011000 afe,0x24,0xC2,0x80,128,10000000 afe,0x24,0xC3,0x00,0,00000000 afe,0x24,0xC4,0x30,48,00110000 afe,0x24,0xC5,0x02,2,00000010 afe,0x24,0xC6,0x03,3,00000011 afe,0x24,0xC7,0x00,0,00000000 afe,0x24,0xC8,0x00,0,00000000 afe,0x24,0xC9,0x00,0,00000000 afe,0x24,0xCA,0x00,0,00000000 afe,0x24,0xCB,0x00,0,00000000 afe,0x24,0xCC,0x40,64,01000000 afe,0x24,0xCD,0x0A,10,00001010 afe,0x24,0xCE,0x96,150,10010110 afe,0x24,0xCF,0x00,0,00000000 afe,0x24,0xD0,0x25,37,00100101 afe,0x24,0xD1,0x23,35,00100011 afe,0x24,0xD2,0xE1,225,11100001 afe,0x24,0xD3,0xAE,174,10101110 afe,0x24,0xD4,0xFF,255,11111111 afe,0x24,0xD5,0xCC,204,11001100 afe,0x24,0xD6,0x05,5,00000101 afe,0x24,0xD7,0x00,0,00000000 afe,0x24,0xD8,0x00,0,00000000 afe,0x24,0xD9,0x1B,27,00011011 afe,0x24,0xDA,0x04,4,00000100 afe,0x24,0xDB,0x00,0,00000000 afe,0x24,0xDC,0x00,0,00000000 afe,0x24,0xDD,0x00,0,00000000 afe,0x24,0xDE,0x00,0,00000000 afe,0x24,0xDF,0x00,0,00000000 afe,0x24,0xE0,0x00,0,00000000 afe,0x24,0xE1,0x00,0,00000000 afe,0x24,0xE2,0x00,0,00000000 afe,0x24,0xE3,0x00,0,00000000 afe,0x24,0xE4,0x06,6,00000110 afe,0x24,0xE5,0x06,6,00000110 afe,0x24,0xE6,0x00,0,00000000 afe,0x24,0xE7,0x00,0,00000000 afe,0x24,0xE8,0x00,0,00000000 afe,0x24,0xE9,0x00,0,00000000 afe,0x24,0xEA,0x00,0,00000000 afe,0x24,0xEB,0x00,0,00000000 afe,0x24,0xEC,0x00,0,00000000 afe,0x24,0xED,0x00,0,00000000 afe,0x24,0xEE,0x00,0,00000000 afe,0x24,0xEF,0x00,0,00000000 afe,0x24,0xF0,0x00,0,00000000 afe,0x24,0xF1,0x00,0,00000000 afe,0x24,0xF2,0x00,0,00000000 afe,0x24,0xF3,0x00,0,00000000 afe,0x24,0xF4,0x00,0,00000000 afe,0x24,0xF5,0x00,0,00000000 afe,0x24,0xF6,0x00,0,00000000 afe,0x24,0xF7,0x00,0,00000000 afe,0x24,0xF8,0x00,0,00000000 afe,0x24,0xF9,0x00,0,00000000 afe,0x24,0xFA,0x00,0,00000000 afe,0x24,0xFB,0x00,0,00000000 afe,0x24,0xFC,0x00,0,00000000 afe,0x24,0xFD,0x00,0,00000000 afe,0x24,0xFE,0x00,0,00000000 afe,0x24,0xFF,0x00,0,00000000 sdp,0x22,0x00,0x02,2,00000010 sdp,0x22,0x01,0x36,54,00110110 sdp,0x22,0x02,0x27,39,00100111 sdp,0x22,0x03,0xC4,196,11000100 sdp,0x22,0x04,0x0B,11,00001011 sdp,0x22,0x05,0xC3,195,11000011 sdp,0x22,0x06,0xC0,192,11000000 sdp,0x22,0x07,0x8B,139,10001011 sdp,0x22,0x08,0x1A,26,00011010 sdp,0x22,0x09,0x00,0,00000000 sdp,0x22,0x0A,0xE5,229,11100101 sdp,0x22,0x0B,0xE5,229,11100101 sdp,0x22,0x0C,0xE5,229,11100101 sdp,0x22,0x0D,0xE4,228,11100100 sdp,0x22,0x0E,0x31,49,00110001 sdp,0x22,0x0F,0x00,0,00000000 sdp,0x22,0x10,0x01,1,00000001 sdp,0x22,0x11,0x10,16,00010000 sdp,0x22,0x12,0x01,1,00000001 sdp,0x22,0x13,0x80,128,10000000 sdp,0x22,0x14,0x00,0,00000000 sdp,0x22,0x15,0x80,128,10000000 sdp,0x22,0x16,0x00,0,00000000 sdp,0x22,0x17,0x00,0,00000000 sdp,0x22,0x18,0xFF,255,11111111 sdp,0x22,0x19,0xCD,205,11001101 sdp,0x22,0x1A,0x95,149,10010101 sdp,0x22,0x1B,0x1E,30,00011110 sdp,0x22,0x1C,0xC4,196,11000100 sdp,0x22,0x1D,0x02,2,00000010 sdp,0x22,0x1E,0x04,4,00000100 sdp,0x22,0x1F,0x12,18,00010010 sdp,0x22,0x20,0x00,0,00000000 sdp,0x22,0x21,0xFF,255,11111111 sdp,0x22,0x22,0x20,32,00100000 sdp,0x22,0x23,0x10,16,00010000 sdp,0x22,0x24,0x4C,76,01001100 sdp,0x22,0x25,0x00,0,00000000 sdp,0x22,0x26,0x8F,143,10001111 sdp,0x22,0x27,0xAA,170,10101010 sdp,0x22,0x28,0x02,2,00000010 sdp,0x22,0x29,0x00,0,00000000 sdp,0x22,0x2A,0x00,0,00000000 sdp,0x22,0x2B,0x00,0,00000000 sdp,0x22,0x2C,0x00,0,00000000 sdp,0x22,0x2D,0x3D,61,00111101 sdp,0x22,0x2E,0x00,0,00000000 sdp,0x22,0x2F,0x00,0,00000000 sdp,0x22,0x30,0x00,0,00000000 sdp,0x22,0x31,0x04,4,00000100 sdp,0x22,0x32,0x00,0,00000000 sdp,0x22,0x33,0x80,128,10000000 sdp,0x22,0x34,0xA0,160,10100000 sdp,0x22,0x35,0x4E,78,01001110 sdp,0x22,0x36,0x42,66,01000010 sdp,0x22,0x37,0x5A,90,01011010 sdp,0x22,0x38,0x49,73,01001001 sdp,0x22,0x39,0x00,0,00000000 sdp,0x22,0x3A,0x00,0,00000000 sdp,0x22,0x3B,0x40,64,01000000 sdp,0x22,0x3C,0x30,48,00110000 sdp,0x22,0x3D,0x0E,14,00001110 sdp,0x22,0x3E,0x8A,138,10001010 sdp,0x22,0x3F,0x73,115,01110011 sdp,0x22,0x40,0x4C,76,01001100 sdp,0x22,0x41,0xC6,198,11000110 sdp,0x22,0x42,0x33,51,00110011 sdp,0x22,0x43,0xA0,160,10100000 sdp,0x22,0x44,0x14,20,00010100 sdp,0x22,0x45,0x43,67,01000011 sdp,0x22,0x46,0x73,115,01110011 sdp,0x22,0x47,0xB3,179,10110011 sdp,0x22,0x48,0x01,1,00000001 sdp,0x22,0x49,0x40,64,01000000 sdp,0x22,0x4A,0x4B,75,01001011 sdp,0x22,0x4B,0xDF,223,11011111 sdp,0x22,0x4C,0x00,0,00000000 sdp,0x22,0x4D,0x00,0,00000000 sdp,0x22,0x4E,0x00,0,00000000 sdp,0x22,0x4F,0x00,0,00000000 sdp,0x22,0x50,0x00,0,00000000 sdp,0x22,0x51,0x00,0,00000000 sdp,0x22,0x52,0x00,0,00000000 sdp,0x22,0x53,0x00,0,00000000 sdp,0x22,0x54,0x04,4,00000100 sdp,0x22,0x55,0x00,0,00000000 sdp,0x22,0x56,0x78,120,01111000 sdp,0x22,0x57,0x10,16,00010000 sdp,0x22,0x58,0x00,0,00000000 sdp,0x22,0x59,0x04,4,00000100 sdp,0x22,0x5A,0x00,0,00000000 sdp,0x22,0x5B,0x44,68,01000100 sdp,0x22,0x5C,0x16,22,00010110 sdp,0x22,0x5D,0x1B,27,00011011 sdp,0x22,0x5E,0x02,2,00000010 sdp,0x22,0x5F,0xEA,234,11101010 sdp,0x22,0x60,0x68,104,01101000 sdp,0x22,0x61,0x06,6,00000110 sdp,0x22,0x62,0x00,0,00000000 sdp,0x22,0x63,0x60,96,01100000 sdp,0x22,0x64,0x01,1,00000001 sdp,0x22,0x65,0x53,83,01010011 sdp,0x22,0x66,0x00,0,00000000 sdp,0x22,0x67,0x9C,156,10011100 sdp,0x22,0x68,0x17,23,00010111 sdp,0x22,0x69,0x14,20,00010100 sdp,0x22,0x6A,0x77,119,01110111 sdp,0x22,0x6B,0xE1,225,11100001 sdp,0x22,0x6C,0x85,133,10000101 sdp,0x22,0x6D,0x83,131,10000011 sdp,0x22,0x6E,0x14,20,00010100 sdp,0x22,0x6F,0x0B,11,00001011 sdp,0x22,0x70,0xB8,184,10111000 sdp,0x22,0x71,0xB0,176,10110000 sdp,0x22,0x72,0xA4,164,10100100 sdp,0x22,0x73,0xF7,247,11110111 sdp,0x22,0x74,0x50,80,01010000 sdp,0x22,0x75,0x96,150,10010110 sdp,0x22,0x76,0x00,0,00000000 sdp,0x22,0x77,0x00,0,00000000 sdp,0x22,0x78,0x1F,31,00011111 sdp,0x22,0x79,0xF1,241,11110001 sdp,0x22,0x7A,0x7F,127,01111111 sdp,0x22,0x7B,0x69,105,01101001 sdp,0x22,0x7C,0xF8,248,11111000 sdp,0x22,0x7D,0xEA,234,11101010 sdp,0x22,0x7E,0x11,17,00010001 sdp,0x22,0x7F,0x3A,58,00111010 sdp,0x22,0x80,0xAA,170,10101010 sdp,0x22,0x81,0x22,34,00100010 sdp,0x22,0x82,0x08,8,00001000 sdp,0x22,0x83,0x3B,59,00111011 sdp,0x22,0x84,0xD3,211,11010011 sdp,0x22,0x85,0xF3,243,11110011 sdp,0x22,0x86,0x20,32,00100000 sdp,0x22,0x87,0xC1,193,11000001 sdp,0x22,0x88,0x41,65,01000001 sdp,0x22,0x89,0x03,3,00000011 sdp,0x22,0x8A,0x00,0,00000000 sdp,0x22,0x8B,0x02,2,00000010 sdp,0x22,0x8C,0x40,64,01000000 sdp,0x22,0x8D,0x08,8,00001000 sdp,0x22,0x8E,0x70,112,01110000 sdp,0x22,0x8F,0x02,2,00000010 sdp,0x22,0x90,0xEE,238,11101110 sdp,0x22,0x91,0x22,34,00100010 sdp,0x22,0x92,0x33,51,00110011 sdp,0x22,0x93,0x01,1,00000001 sdp,0x22,0x94,0x93,147,10010011 sdp,0x22,0x95,0x0D,13,00001101 sdp,0x22,0x96,0x14,20,00010100 sdp,0x22,0x97,0x14,20,00010100 sdp,0x22,0x98,0xBF,191,10111111 sdp,0x22,0x99,0x10,16,00010000 sdp,0x22,0x9A,0x01,1,00000001 sdp,0x22,0x9B,0x55,85,01010101 sdp,0x22,0x9C,0x03,3,00000011 sdp,0x22,0x9D,0x8A,138,10001010 sdp,0x22,0x9E,0x1E,30,00011110 sdp,0x22,0x9F,0x7F,127,01111111 sdp,0x22,0xA0,0x08,8,00001000 sdp,0x22,0xA1,0x50,80,01010000 sdp,0x22,0xA2,0xA0,160,10100000 sdp,0x22,0xA3,0xBE,190,10111110 sdp,0x22,0xA4,0xBF,191,10111111 sdp,0x22,0xA5,0xBF,191,10111111 sdp,0x22,0xA6,0x00,0,00000000 sdp,0x22,0xA7,0x04,4,00000100 sdp,0x22,0xA8,0x40,64,01000000 sdp,0x22,0xA9,0x88,136,10001000 sdp,0x22,0xAA,0x88,136,10001000 sdp,0x22,0xAB,0x00,0,00000000 sdp,0x22,0xAC,0x22,34,00100010 sdp,0x22,0xAD,0x22,34,00100010 sdp,0x22,0xAE,0xCF,207,11001111 sdp,0x22,0xAF,0x84,132,10000100 sdp,0x22,0xB0,0x28,40,00101000 sdp,0x22,0xB1,0x84,132,10000100 sdp,0x22,0xB2,0x14,20,00010100 sdp,0x22,0xB3,0x64,100,01100100 sdp,0x22,0xB4,0x24,36,00100100 sdp,0x22,0xB5,0x24,36,00100100 sdp,0x22,0xB6,0x1F,31,00011111 sdp,0x22,0xB7,0xA4,164,10100100 sdp,0x22,0xB8,0x44,68,01000100 sdp,0x22,0xB9,0x42,66,01000010 sdp,0x22,0xBA,0x12,18,00010010 sdp,0x22,0xBB,0x13,19,00010011 sdp,0x22,0xBC,0x20,32,00100000 sdp,0x22,0xBD,0x38,56,00111000 sdp,0x22,0xBE,0x2B,43,00101011 sdp,0x22,0xBF,0xA9,169,10101001 sdp,0x22,0xC0,0x52,82,01010010 sdp,0x22,0xC1,0x53,83,01010011 sdp,0x22,0xC2,0x24,36,00100100 sdp,0x22,0xC3,0x44,68,01000100 sdp,0x22,0xC4,0x0C,12,00001100 sdp,0x22,0xC5,0xD4,212,11010100 sdp,0x22,0xC6,0x72,114,01110010 sdp,0x22,0xC7,0xF1,241,11110001 sdp,0x22,0xC8,0x81,129,10000001 sdp,0x22,0xC9,0x89,137,10001001 sdp,0x22,0xCA,0x28,40,00101000 sdp,0x22,0xCB,0x00,0,00000000 sdp,0x22,0xCC,0x00,0,00000000 sdp,0x22,0xCD,0x00,0,00000000 sdp,0x22,0xCE,0x02,2,00000010 sdp,0x22,0xCF,0x00,0,00000000 sdp,0x22,0xD0,0x98,152,10011000 sdp,0x22,0xD1,0x41,65,01000001 sdp,0x22,0xD2,0x1E,30,00011110 sdp,0x22,0xD3,0xA2,162,10100010 sdp,0x22,0xD4,0x50,80,01010000 sdp,0x22,0xD5,0x10,16,00010000 sdp,0x22,0xD6,0xCC,204,11001100 sdp,0x22,0xD7,0x04,4,00000100 sdp,0x22,0xD8,0x00,0,00000000 sdp,0x22,0xD9,0x44,68,01000100 sdp,0x22,0xDA,0x00,0,00000000 sdp,0x22,0xDB,0x88,136,10001000 sdp,0x22,0xDC,0x02,2,00000010 sdp,0x22,0xDD,0xBC,188,10111100 sdp,0x22,0xDE,0x23,35,00100011 sdp,0x22,0xDF,0x7D,125,01111101 sdp,0x22,0xE0,0x04,4,00000100 sdp,0x22,0xE1,0x00,0,00000000 sdp,0x22,0xE2,0x48,72,01001000 sdp,0x22,0xE3,0x00,0,00000000 sdp,0x22,0xE4,0x00,0,00000000 sdp,0x22,0xE5,0x09,9,00001001 sdp,0x22,0xE6,0x3B,59,00111011 sdp,0x22,0xE7,0x00,0,00000000 sdp,0x22,0xE8,0x00,0,00000000 sdp,0x22,0xE9,0x84,132,10000100 sdp,0x22,0xEA,0x84,132,10000100 sdp,0x22,0xEB,0x4B,75,01001011 sdp,0x22,0xEC,0x4C,76,01001100 sdp,0x22,0xED,0xC0,192,11000000 sdp,0x22,0xEE,0xC0,192,11000000 sdp,0x22,0xEF,0x02,2,00000010 sdp,0x22,0xF0,0x82,130,10000010 sdp,0x22,0xF1,0x98,152,10011000 sdp,0x22,0xF2,0x18,24,00011000 sdp,0x22,0xF3,0xB0,176,10110000 sdp,0x22,0xF4,0x30,48,00110000 sdp,0x22,0xF5,0x1A,26,00011010 sdp,0x22,0xF6,0x1A,26,00011010 sdp,0x22,0xF7,0x1A,26,00011010 sdp,0x22,0xF8,0x1A,26,00011010 sdp,0x22,0xF9,0xBF,191,10111111 sdp,0x22,0xFA,0x18,24,00011000 sdp,0x22,0xFB,0x3F,63,00111111 sdp,0x22,0xFC,0x18,24,00011000 sdp,0x22,0xFD,0x29,41,00101001 sdp,0x22,0xFE,0x04,4,00000100 sdp,0x22,0xFF,0x93,147,10010011 sdpio,0x25,0x00,0x00,0,00000000 sdpio,0x25,0x01,0x00,0,00000000 sdpio,0x25,0x02,0x00,0,00000000 sdpio,0x25,0x03,0x00,0,00000000 sdpio,0x25,0x04,0x00,0,00000000 sdpio,0x25,0x05,0x00,0,00000000 sdpio,0x25,0x06,0x00,0,00000000 sdpio,0x25,0x07,0x00,0,00000000 sdpio,0x25,0x08,0x00,0,00000000 sdpio,0x25,0x09,0x00,0,00000000 sdpio,0x25,0x0A,0x00,0,00000000 sdpio,0x25,0x0B,0x00,0,00000000 sdpio,0x25,0x0C,0x00,0,00000000 sdpio,0x25,0x0D,0x00,0,00000000 sdpio,0x25,0x0E,0x00,0,00000000 sdpio,0x25,0x0F,0x00,0,00000000 sdpio,0x25,0x10,0x00,0,00000000 sdpio,0x25,0x11,0x00,0,00000000 sdpio,0x25,0x12,0x00,0,00000000 sdpio,0x25,0x13,0x00,0,00000000 sdpio,0x25,0x14,0x00,0,00000000 sdpio,0x25,0x15,0x00,0,00000000 sdpio,0x25,0x16,0x00,0,00000000 sdpio,0x25,0x17,0x00,0,00000000 sdpio,0x25,0x18,0x00,0,00000000 sdpio,0x25,0x19,0x00,0,00000000 sdpio,0x25,0x1A,0x00,0,00000000 sdpio,0x25,0x1B,0x00,0,00000000 sdpio,0x25,0x1C,0x00,0,00000000 sdpio,0x25,0x1D,0x00,0,00000000 sdpio,0x25,0x1E,0x00,0,00000000 sdpio,0x25,0x1F,0x00,0,00000000 sdpio,0x25,0x20,0x00,0,00000000 sdpio,0x25,0x21,0x00,0,00000000 sdpio,0x25,0x22,0x00,0,00000000 sdpio,0x25,0x23,0x00,0,00000000 sdpio,0x25,0x24,0x00,0,00000000 sdpio,0x25,0x25,0x00,0,00000000 sdpio,0x25,0x26,0x00,0,00000000 sdpio,0x25,0x27,0x08,8,00001000 sdpio,0x25,0x28,0x00,0,00000000 sdpio,0x25,0x29,0x00,0,00000000 sdpio,0x25,0x2A,0x00,0,00000000 sdpio,0x25,0x2B,0x00,0,00000000 sdpio,0x25,0x2C,0x00,0,00000000 sdpio,0x25,0x2D,0x00,0,00000000 sdpio,0x25,0x2E,0x00,0,00000000 sdpio,0x25,0x2F,0x00,0,00000000 sdpio,0x25,0x30,0x00,0,00000000 sdpio,0x25,0x31,0x00,0,00000000 sdpio,0x25,0x32,0x00,0,00000000 sdpio,0x25,0x33,0x00,0,00000000 sdpio,0x25,0x34,0x00,0,00000000 sdpio,0x25,0x35,0x00,0,00000000 sdpio,0x25,0x36,0x01,1,00000001 sdpio,0x25,0x37,0x00,0,00000000 sdpio,0x25,0x38,0x00,0,00000000 sdpio,0x25,0x39,0x00,0,00000000 sdpio,0x25,0x3A,0x00,0,00000000 sdpio,0x25,0x3B,0x00,0,00000000 sdpio,0x25,0x3C,0x00,0,00000000 sdpio,0x25,0x3D,0x00,0,00000000 sdpio,0x25,0x3E,0x00,0,00000000 sdpio,0x25,0x3F,0x00,0,00000000 sdpio,0x25,0x40,0x00,0,00000000 sdpio,0x25,0x41,0x00,0,00000000 sdpio,0x25,0x42,0x00,0,00000000 sdpio,0x25,0x43,0x00,0,00000000 sdpio,0x25,0x44,0x00,0,00000000 sdpio,0x25,0x45,0x00,0,00000000 sdpio,0x25,0x46,0x00,0,00000000 sdpio,0x25,0x47,0x00,0,00000000 sdpio,0x25,0x48,0x00,0,00000000 sdpio,0x25,0x49,0x00,0,00000000 sdpio,0x25,0x4A,0x00,0,00000000 sdpio,0x25,0x4B,0x00,0,00000000 sdpio,0x25,0x4C,0x00,0,00000000 sdpio,0x25,0x4D,0x00,0,00000000 sdpio,0x25,0x4E,0x00,0,00000000 sdpio,0x25,0x4F,0x00,0,00000000 sdpio,0x25,0x50,0x00,0,00000000 sdpio,0x25,0x51,0x00,0,00000000 sdpio,0x25,0x52,0x14,20,00010100 sdpio,0x25,0x53,0x00,0,00000000 sdpio,0x25,0x54,0x00,0,00000000 sdpio,0x25,0x55,0x00,0,00000000 sdpio,0x25,0x56,0x00,0,00000000 sdpio,0x25,0x57,0x00,0,00000000 sdpio,0x25,0x58,0x00,0,00000000 sdpio,0x25,0x59,0x00,0,00000000 sdpio,0x25,0x5A,0x00,0,00000000 sdpio,0x25,0x5B,0x00,0,00000000 sdpio,0x25,0x5C,0x00,0,00000000 sdpio,0x25,0x5D,0x52,82,01010010 sdpio,0x25,0x5E,0x68,104,01101000 sdpio,0x25,0x5F,0x00,0,00000000 sdpio,0x25,0x60,0x00,0,00000000 sdpio,0x25,0x61,0x06,6,00000110 sdpio,0x25,0x62,0x1A,26,00011010 sdpio,0x25,0x63,0x12,18,00010010 sdpio,0x25,0x64,0x00,0,00000000 sdpio,0x25,0x65,0x00,0,00000000 sdpio,0x25,0x66,0x01,1,00000001 sdpio,0x25,0x67,0x04,4,00000100 sdpio,0x25,0x68,0x00,0,00000000 sdpio,0x25,0x69,0x00,0,00000000 sdpio,0x25,0x6A,0x00,0,00000000 sdpio,0x25,0x6B,0x00,0,00000000 sdpio,0x25,0x6C,0x4B,75,01001011 sdpio,0x25,0x6D,0x32,50,00110010 sdpio,0x25,0x6E,0x00,0,00000000 sdpio,0x25,0x6F,0x00,0,00000000 sdpio,0x25,0x70,0xA7,167,10100111 sdpio,0x25,0x71,0x3A,58,00111010 sdpio,0x25,0x72,0x06,6,00000110 sdpio,0x25,0x73,0xEF,239,11101111 sdpio,0x25,0x74,0x10,16,00010000 sdpio,0x25,0x75,0x0A,10,00001010 sdpio,0x25,0x76,0x32,50,00110010 sdpio,0x25,0x77,0x23,35,00100011 sdpio,0x25,0x78,0x00,0,00000000 sdpio,0x25,0x79,0x63,99,01100011 sdpio,0x25,0x7A,0xAA,170,10101010 sdpio,0x25,0x7B,0x4F,79,01001111 sdpio,0x25,0x7C,0x58,88,01011000 sdpio,0x25,0x7D,0xA4,164,10100100 sdpio,0x25,0x7E,0x10,16,00010000 sdpio,0x25,0x7F,0x1F,31,00011111 sdpio,0x25,0x80,0x00,0,00000000 sdpio,0x25,0x81,0x00,0,00000000 sdpio,0x25,0x82,0x00,0,00000000 sdpio,0x25,0x83,0x00,0,00000000 sdpio,0x25,0x84,0x00,0,00000000 sdpio,0x25,0x85,0x00,0,00000000 sdpio,0x25,0x86,0xAA,170,10101010 sdpio,0x25,0x87,0x00,0,00000000 sdpio,0x25,0x88,0x44,68,01000100 sdpio,0x25,0x89,0x00,0,00000000 sdpio,0x25,0x8A,0x04,4,00000100 sdpio,0x25,0x8B,0x00,0,00000000 sdpio,0x25,0x8C,0x00,0,00000000 sdpio,0x25,0x8D,0x00,0,00000000 sdpio,0x25,0x8E,0x00,0,00000000 sdpio,0x25,0x8F,0x00,0,00000000 sdpio,0x25,0x90,0x00,0,00000000 sdpio,0x25,0x91,0x00,0,00000000 sdpio,0x25,0x92,0x00,0,00000000 sdpio,0x25,0x93,0x00,0,00000000 sdpio,0x25,0x94,0x00,0,00000000 sdpio,0x25,0x95,0x00,0,00000000 sdpio,0x25,0x96,0x00,0,00000000 sdpio,0x25,0x97,0x20,32,00100000 sdpio,0x25,0x98,0x00,0,00000000 sdpio,0x25,0x99,0x00,0,00000000 sdpio,0x25,0x9A,0x00,0,00000000 sdpio,0x25,0x9B,0x00,0,00000000 sdpio,0x25,0x9C,0x00,0,00000000 sdpio,0x25,0x9D,0x00,0,00000000 sdpio,0x25,0x9E,0x00,0,00000000 sdpio,0x25,0x9F,0x00,0,00000000 sdpio,0x25,0xA0,0x04,4,00000100 sdpio,0x25,0xA1,0x04,4,00000100 sdpio,0x25,0xA2,0x04,4,00000100 sdpio,0x25,0xA3,0x04,4,00000100 sdpio,0x25,0xA4,0x04,4,00000100 sdpio,0x25,0xA5,0x04,4,00000100 sdpio,0x25,0xA6,0x04,4,00000100 sdpio,0x25,0xA7,0x04,4,00000100 sdpio,0x25,0xA8,0x04,4,00000100 sdpio,0x25,0xA9,0x04,4,00000100 sdpio,0x25,0xAA,0x04,4,00000100 sdpio,0x25,0xAB,0x04,4,00000100 sdpio,0x25,0xAC,0x04,4,00000100 sdpio,0x25,0xAD,0x04,4,00000100 sdpio,0x25,0xAE,0x04,4,00000100 sdpio,0x25,0xAF,0x04,4,00000100 sdpio,0x25,0xB0,0xC0,192,11000000 sdpio,0x25,0xB1,0x7D,125,01111101 sdpio,0x25,0xB2,0x6C,108,01101100 sdpio,0x25,0xB3,0x20,32,00100000 sdpio,0x25,0xB4,0x04,4,00000100 sdpio,0x25,0xB5,0x04,4,00000100 sdpio,0x25,0xB6,0x04,4,00000100 sdpio,0x25,0xB7,0x04,4,00000100 sdpio,0x25,0xB8,0x04,4,00000100 sdpio,0x25,0xB9,0x04,4,00000100 sdpio,0x25,0xBA,0x04,4,00000100 sdpio,0x25,0xBB,0x04,4,00000100 sdpio,0x25,0xBC,0x04,4,00000100 sdpio,0x25,0xBD,0x04,4,00000100 sdpio,0x25,0xBE,0x04,4,00000100 sdpio,0x25,0xBF,0x04,4,00000100 sdpio,0x25,0xC0,0x00,0,00000000 sdpio,0x25,0xC1,0x00,0,00000000 sdpio,0x25,0xC2,0x04,4,00000100 sdpio,0x25,0xC3,0x04,4,00000100 sdpio,0x25,0xC4,0x04,4,00000100 sdpio,0x25,0xC5,0x04,4,00000100 sdpio,0x25,0xC6,0x04,4,00000100 sdpio,0x25,0xC7,0x04,4,00000100 sdpio,0x25,0xC8,0xEB,235,11101011 sdpio,0x25,0xC9,0x6C,108,01101100 sdpio,0x25,0xCA,0x00,0,00000000 sdpio,0x25,0xCB,0x02,2,00000010 sdpio,0x25,0xCC,0x00,0,00000000 sdpio,0x25,0xCD,0x00,0,00000000 sdpio,0x25,0xCE,0xFF,255,11111111 sdpio,0x25,0xCF,0xFE,254,11111110 sdpio,0x25,0xD0,0x00,0,00000000 sdpio,0x25,0xD1,0x00,0,00000000 sdpio,0x25,0xD2,0x00,0,00000000 sdpio,0x25,0xD3,0x00,0,00000000 sdpio,0x25,0xD4,0x00,0,00000000 sdpio,0x25,0xD5,0x00,0,00000000 sdpio,0x25,0xD6,0x00,0,00000000 sdpio,0x25,0xD7,0x00,0,00000000 sdpio,0x25,0xD8,0x00,0,00000000 sdpio,0x25,0xD9,0x00,0,00000000 sdpio,0x25,0xDA,0x00,0,00000000 sdpio,0x25,0xDB,0x00,0,00000000 sdpio,0x25,0xDC,0x00,0,00000000 sdpio,0x25,0xDD,0x84,132,10000100 sdpio,0x25,0xDE,0x00,0,00000000 sdpio,0x25,0xDF,0x00,0,00000000 sdpio,0x25,0xE0,0x47,71,01000111 sdpio,0x25,0xE1,0xD2,210,11010010 sdpio,0x25,0xE2,0x00,0,00000000 sdpio,0x25,0xE3,0x00,0,00000000 sdpio,0x25,0xE4,0x00,0,00000000 sdpio,0x25,0xE5,0x40,64,01000000 sdpio,0x25,0xE6,0x7F,127,01111111 sdpio,0x25,0xE7,0x00,0,00000000 sdpio,0x25,0xE8,0x00,0,00000000 sdpio,0x25,0xE9,0x00,0,00000000 sdpio,0x25,0xEA,0x09,9,00001001 sdpio,0x25,0xEB,0x26,38,00100110 sdpio,0x25,0xEC,0x00,0,00000000 sdpio,0x25,0xED,0x00,0,00000000 sdpio,0x25,0xEE,0x00,0,00000000 sdpio,0x25,0xEF,0x00,0,00000000 sdpio,0x25,0xF0,0x00,0,00000000 sdpio,0x25,0xF1,0x00,0,00000000 sdpio,0x25,0xF2,0x00,0,00000000 sdpio,0x25,0xF3,0x00,0,00000000 sdpio,0x25,0xF4,0x06,6,00000110 sdpio,0x25,0xF5,0x81,129,10000001 sdpio,0x25,0xF6,0x00,0,00000000 sdpio,0x25,0xF7,0x00,0,00000000 sdpio,0x25,0xF8,0x00,0,00000000 sdpio,0x25,0xF9,0x00,0,00000000 sdpio,0x25,0xFA,0x00,0,00000000 sdpio,0x25,0xFB,0x00,0,00000000 sdpio,0x25,0xFC,0x00,0,00000000 sdpio,0x25,0xFD,0x00,0,00000000 sdpio,0x25,0xFE,0x00,0,00000000 sdpio,0x25,0xFF,0x00,0,00000000
Edit Notes
Changed title / tags[edited by: superchromat at 3:32 AM (GMT -4) on 6 Jun 2026]