Post Go back to editing

ADV7842: Excess noise when capturing component video

Category: Hardware
Product Number: ADV7842

We have a design that incorporates an ADV7842 as a 12 bit per channel analog to digital converter for HD component video. When we supply an HD video signal at 1080p24 (pixel clock 74.25MHz) we see excessive broadband noise in the captured image data at ~12 LSB (12 bit). This is twice the level of noise that we've measured from a commercial device that also happens to use an ADV7842 in the same experimental setup.

The ADV7842 feeds its data over 36bit per pixel parallel single clock / single edge to another chip on the board from Macro Image Technologies (MIT), that outputs a TMDS stream which is captured by a BlackMagic Design UltraStudio as HDMI. We have verified that if I generate a test pattern within the MIT chip, the data captured by the UltraStudio is bit perfect. Likewise, I have verified that a test pattern generated internally by the ADV7842 shows no noise.

We have tested this with a variety of analog sources generating a 50% gray full frame field as Y/Pb/Pr with sync on Y. The Y signal has a tri-level sync pulse extending 300mV below and above blanking level. The video is 0-700mV above blanking. The peak to peak of sync + video is 1V. For the grey test image, Pb and Pr at at 0V (AC coupled) and Y is active at 350mV.

In the current measurement setup, the DAC is showing <900 uV RMS noise on each of those channels during the active video region.

The video signal goes into the ADC using the datasheet suggested divider network of 24R series, 51R shunt, AC coupled via 100nF. This is a 0.68x divider and provides the 75R termination to match the source impedance.

The ADV7842 is has clamping enabled, and configured for a 300mV sync tip for AGC. Capturing at 12bits for the range of 0-1V (sync tip clamp level referenced), the least significant bit is 244uV (1V / 2^12). With source noise at 900uV, it is scaled down by the divider to 0.68x, with 612uV of RMS noise reaching the AIN pin of the ADC. So, we would expect to see 2.5 LSB of noise.

Note, this assumes that the ADC is noiseless. Given that no noise figure is published, we'll go with that assumption - particularly given that we have another device from another manufacturer that uses an ADV7842, and it exhibits 2x less measured noise than my device. This implies that the noise is my fault, not that of the ADV7842 intrinsically. I have tested two of my boards, and they both show the same excess noise.

The ADV7842 is configured with Automatic Gain Control (AGC) enabled with sync tip tracking. Reading back CP_AGC_GAIN returns 0x30F or 1.53x. So the digital gain stage should take the 2.5 LSB of noise and multiply it up to 3.8 LSB. However, we are measuring over 3x that at 12 LSB.

Here is a zoomed in section of a capture of the 50% grey field (unsure how well this will survive compression, but you should see the random noise):

We have the MIT chip set up to output 12bit YUV 4:4:4 TMDS, as the UltraStudio is only capable of capturing 10bit 4:2:2. While it can capture RGB 12bit, the source into the ADV7842 is Y/Pb/Pr, so we want the channels in the captures to match the channels being input into the ADC. Loading a captured YUV lossless TIFF file into R to analyze the noise, we see the following output:

The main things to note is the width of the histograms compared to the source, with RMS readings of 2.9mV versus the ~900uV measured RMS noise from the source. The noise spectrum is flat for Y, with the expected rolloff seen for Pb/Pr given that this is a 4:2:2 capture.

This capture was taken with the internal anti-aliasing filter _disabled_ on the ADV7842. If we set the AA filter to a cutoff of 10MHz, the noise spectrum remains basically the same (with the addition of some spurs that don't meaningfully contribute to the overall RMS noise):

This suggests that the noise is coming from after the AA stage, and thus is not a reflection of noise present at the Analog In pins of the ADV7842.

The ADV7842 has separate low noise LDO's powering PVDD and AVDD. The noise measured on those lines is low, with less than 1uV noise in the 0-37MHz band. Furthermore, injecting orders of magnitude more broadband noise directly into PVDD or AVDD does not change the measured noise spectra. VDD and CVDD are supplied by the boards general 1V8 digital supply, and while that supply is noisy (16mV broadband AC RMS), again, injecting further noise into those rails does not change the measured noise spectrum of the ADC output. The board is a 6 layer board with a continuous power plane for 1V8 and continuous single ground planes. Decoupling for PVDD and AVDD is directly under the BGA on the back of the board. REFP/N are decoupled as per the datasheet, close to their pins.

So, in short, we am seeing 12LSB of broadband noise that doesn't reflect the noise in our sources. The noise is not impacted by AA filter settings and is not wholly explained by the 1.5x AGC digital gain. Nor can we see a source of the noise on the rails supplying the ADV7842.

We have included a full dump of the registers below.

What should I be looking at next?

# ADV7842 full register dump
map,map_i2c_7bit,reg,value_hex,value_dec,value_bin
io,0x20,0x00,0x1E,30,00011110
io,0x20,0x01,0x41,65,01000001
io,0x20,0x02,0x70,112,01110000
io,0x20,0x03,0x42,66,01000010
io,0x20,0x04,0x42,66,01000010
io,0x20,0x05,0x2C,44,00101100
io,0x20,0x06,0xB6,182,10110110
io,0x20,0x07,0x54,84,01010100
io,0x20,0x08,0x14,20,00010100
io,0x20,0x09,0x00,0,00000000
io,0x20,0x0A,0x90,144,10010000
io,0x20,0x0B,0x44,68,01000100
io,0x20,0x0C,0x00,0,00000000
io,0x20,0x0D,0x1E,30,00011110
io,0x20,0x0E,0x0F,15,00001111
io,0x20,0x0F,0x1E,30,00011110
io,0x20,0x10,0x00,0,00000000
io,0x20,0x11,0x00,0,00000000
io,0x20,0x12,0xC0,192,11000000
io,0x20,0x13,0x0D,13,00001101
io,0x20,0x14,0x6A,106,01101010
io,0x20,0x15,0x00,0,00000000
io,0x20,0x16,0x43,67,01000011
io,0x20,0x17,0x5A,90,01011010
io,0x20,0x18,0x34,52,00110100
io,0x20,0x19,0x9E,158,10011110
io,0x20,0x1A,0x02,2,00000010
io,0x20,0x1B,0x00,0,00000000
io,0x20,0x1C,0x00,0,00000000
io,0x20,0x1D,0x00,0,00000000
io,0x20,0x1E,0x00,0,00000000
io,0x20,0x1F,0x00,0,00000000
io,0x20,0x20,0xF0,240,11110000
io,0x20,0x21,0x00,0,00000000
io,0x20,0x22,0x00,0,00000000
io,0x20,0x23,0x03,3,00000011
io,0x20,0x24,0x00,0,00000000
io,0x20,0x25,0x00,0,00000000
io,0x20,0x26,0x00,0,00000000
io,0x20,0x27,0x00,0,00000000
io,0x20,0x28,0x00,0,00000000
io,0x20,0x29,0x00,0,00000000
io,0x20,0x2A,0x00,0,00000000
io,0x20,0x2B,0x00,0,00000000
io,0x20,0x2C,0x00,0,00000000
io,0x20,0x2D,0x00,0,00000000
io,0x20,0x2E,0x00,0,00000000
io,0x20,0x2F,0x00,0,00000000
io,0x20,0x30,0x88,136,10001000
io,0x20,0x31,0x00,0,00000000
io,0x20,0x32,0x00,0,00000000
io,0x20,0x33,0x40,64,01000000
io,0x20,0x34,0x00,0,00000000
io,0x20,0x35,0x00,0,00000000
io,0x20,0x36,0x00,0,00000000
io,0x20,0x37,0x00,0,00000000
io,0x20,0x38,0x00,0,00000000
io,0x20,0x39,0x00,0,00000000
io,0x20,0x3A,0x00,0,00000000
io,0x20,0x3B,0x00,0,00000000
io,0x20,0x3C,0x00,0,00000000
io,0x20,0x3D,0x00,0,00000000
io,0x20,0x3E,0x00,0,00000000
io,0x20,0x3F,0x00,0,00000000
io,0x20,0x40,0x20,32,00100000
io,0x20,0x41,0x30,48,00110000
io,0x20,0x42,0x94,148,10010100
io,0x20,0x43,0x00,0,00000000
io,0x20,0x44,0x00,0,00000000
io,0x20,0x45,0x00,0,00000000
io,0x20,0x46,0x00,0,00000000
io,0x20,0x47,0x00,0,00000000
io,0x20,0x48,0x00,0,00000000
io,0x20,0x49,0x00,0,00000000
io,0x20,0x4A,0x00,0,00000000
io,0x20,0x4B,0x00,0,00000000
io,0x20,0x4C,0x00,0,00000000
io,0x20,0x4D,0x00,0,00000000
io,0x20,0x4E,0x00,0,00000000
io,0x20,0x4F,0x00,0,00000000
io,0x20,0x50,0x00,0,00000000
io,0x20,0x51,0x00,0,00000000
io,0x20,0x52,0x00,0,00000000
io,0x20,0x53,0x00,0,00000000
io,0x20,0x54,0x00,0,00000000
io,0x20,0x55,0x00,0,00000000
io,0x20,0x56,0x85,133,10000101
io,0x20,0x57,0x00,0,00000000
io,0x20,0x58,0x00,0,00000000
io,0x20,0x59,0x00,0,00000000
io,0x20,0x5A,0x00,0,00000000
io,0x20,0x5B,0xBB,187,10111011
io,0x20,0x5C,0x00,0,00000000
io,0x20,0x5D,0x00,0,00000000
io,0x20,0x5E,0x00,0,00000000
io,0x20,0x5F,0x00,0,00000000
io,0x20,0x60,0x00,0,00000000
io,0x20,0x61,0x00,0,00000000
io,0x20,0x62,0x00,0,00000000
io,0x20,0x63,0x00,0,00000000
io,0x20,0x64,0x00,0,00000000
io,0x20,0x65,0x40,64,01000000
io,0x20,0x66,0x00,0,00000000
io,0x20,0x67,0x00,0,00000000
io,0x20,0x68,0x00,0,00000000
io,0x20,0x69,0x00,0,00000000
io,0x20,0x6A,0x00,0,00000000
io,0x20,0x6B,0x00,0,00000000
io,0x20,0x6C,0x00,0,00000000
io,0x20,0x6D,0x00,0,00000000
io,0x20,0x6E,0x00,0,00000000
io,0x20,0x6F,0x00,0,00000000
io,0x20,0x70,0x00,0,00000000
io,0x20,0x71,0x00,0,00000000
io,0x20,0x72,0x00,0,00000000
io,0x20,0x73,0x00,0,00000000
io,0x20,0x74,0x00,0,00000000
io,0x20,0x75,0x00,0,00000000
io,0x20,0x76,0x00,0,00000000
io,0x20,0x77,0x00,0,00000000
io,0x20,0x78,0x00,0,00000000
io,0x20,0x79,0x00,0,00000000
io,0x20,0x7A,0x00,0,00000000
io,0x20,0x7B,0x00,0,00000000
io,0x20,0x7C,0x00,0,00000000
io,0x20,0x7D,0x00,0,00000000
io,0x20,0x7E,0x00,0,00000000
io,0x20,0x7F,0x00,0,00000000
io,0x20,0x80,0x00,0,00000000
io,0x20,0x81,0x00,0,00000000
io,0x20,0x82,0x00,0,00000000
io,0x20,0x83,0x00,0,00000000
io,0x20,0x84,0x00,0,00000000
io,0x20,0x85,0x00,0,00000000
io,0x20,0x86,0x00,0,00000000
io,0x20,0x87,0x00,0,00000000
io,0x20,0x88,0x00,0,00000000
io,0x20,0x89,0x00,0,00000000
io,0x20,0x8A,0x00,0,00000000
io,0x20,0x8B,0x00,0,00000000
io,0x20,0x8C,0x00,0,00000000
io,0x20,0x8D,0x00,0,00000000
io,0x20,0x8E,0x00,0,00000000
io,0x20,0x8F,0x00,0,00000000
io,0x20,0x90,0x00,0,00000000
io,0x20,0x91,0x00,0,00000000
io,0x20,0x92,0x00,0,00000000
io,0x20,0x93,0x00,0,00000000
io,0x20,0x94,0x00,0,00000000
io,0x20,0x95,0x00,0,00000000
io,0x20,0x96,0x00,0,00000000
io,0x20,0x97,0x00,0,00000000
io,0x20,0x98,0x00,0,00000000
io,0x20,0x99,0x00,0,00000000
io,0x20,0x9A,0x00,0,00000000
io,0x20,0x9B,0x00,0,00000000
io,0x20,0x9C,0x00,0,00000000
io,0x20,0x9D,0x00,0,00000000
io,0x20,0x9E,0x00,0,00000000
io,0x20,0x9F,0x00,0,00000000
io,0x20,0xA0,0x00,0,00000000
io,0x20,0xA1,0x00,0,00000000
io,0x20,0xA2,0x00,0,00000000
io,0x20,0xA3,0x00,0,00000000
io,0x20,0xA4,0x00,0,00000000
io,0x20,0xA5,0x00,0,00000000
io,0x20,0xA6,0x00,0,00000000
io,0x20,0xA7,0x00,0,00000000
io,0x20,0xA8,0x00,0,00000000
io,0x20,0xA9,0x00,0,00000000
io,0x20,0xAA,0x00,0,00000000
io,0x20,0xAB,0x00,0,00000000
io,0x20,0xAC,0x00,0,00000000
io,0x20,0xAD,0x00,0,00000000
io,0x20,0xAE,0x00,0,00000000
io,0x20,0xAF,0x00,0,00000000
io,0x20,0xB0,0x00,0,00000000
io,0x20,0xB1,0x00,0,00000000
io,0x20,0xB2,0x00,0,00000000
io,0x20,0xB3,0x00,0,00000000
io,0x20,0xB4,0x00,0,00000000
io,0x20,0xB5,0x00,0,00000000
io,0x20,0xB6,0x00,0,00000000
io,0x20,0xB7,0x43,67,01000011
io,0x20,0xB8,0xE0,224,11100000
io,0x20,0xB9,0x00,0,00000000
io,0x20,0xBA,0x00,0,00000000
io,0x20,0xBB,0x00,0,00000000
io,0x20,0xBC,0x00,0,00000000
io,0x20,0xBD,0x00,0,00000000
io,0x20,0xBE,0x00,0,00000000
io,0x20,0xBF,0x00,0,00000000
io,0x20,0xC0,0x00,0,00000000
io,0x20,0xC1,0x0E,14,00001110
io,0x20,0xC2,0x00,0,00000000
io,0x20,0xC3,0x00,0,00000000
io,0x20,0xC4,0x00,0,00000000
io,0x20,0xC5,0x00,0,00000000
io,0x20,0xC6,0x00,0,00000000
io,0x20,0xC7,0x00,0,00000000
io,0x20,0xC8,0x00,0,00000000
io,0x20,0xC9,0x00,0,00000000
io,0x20,0xCA,0x00,0,00000000
io,0x20,0xCB,0x00,0,00000000
io,0x20,0xCC,0x00,0,00000000
io,0x20,0xCD,0x00,0,00000000
io,0x20,0xCE,0x00,0,00000000
io,0x20,0xCF,0x00,0,00000000
io,0x20,0xD0,0x00,0,00000000
io,0x20,0xD1,0x07,7,00000111
io,0x20,0xD2,0xEA,234,11101010
io,0x20,0xD3,0x82,130,10000010
io,0x20,0xD4,0x57,87,01010111
io,0x20,0xD5,0x00,0,00000000
io,0x20,0xD6,0x00,0,00000000
io,0x20,0xD7,0x00,0,00000000
io,0x20,0xD8,0x2D,45,00101101
io,0x20,0xD9,0x15,21,00010101
io,0x20,0xDA,0xF1,241,11110001
io,0x20,0xDB,0x5F,95,01011111
io,0x20,0xDC,0x40,64,01000000
io,0x20,0xDD,0x00,0,00000000
io,0x20,0xDE,0x00,0,00000000
io,0x20,0xDF,0x00,0,00000000
io,0x20,0xE0,0x00,0,00000000
io,0x20,0xE1,0x00,0,00000000
io,0x20,0xE2,0x04,4,00000100
io,0x20,0xE3,0x00,0,00000000
io,0x20,0xE4,0x01,1,00000001
io,0x20,0xE5,0x00,0,00000000
io,0x20,0xE6,0x00,0,00000000
io,0x20,0xE7,0x00,0,00000000
io,0x20,0xE8,0x04,4,00000100
io,0x20,0xE9,0x00,0,00000000
io,0x20,0xEA,0x20,32,00100000
io,0x20,0xEB,0x12,18,00010010
io,0x20,0xEC,0x00,0,00000000
io,0x20,0xED,0x00,0,00000000
io,0x20,0xEE,0x00,0,00000000
io,0x20,0xEF,0x00,0,00000000
io,0x20,0xF0,0x00,0,00000000
io,0x20,0xF1,0x44,68,01000100
io,0x20,0xF2,0x4A,74,01001010
io,0x20,0xF3,0x00,0,00000000
io,0x20,0xF4,0x00,0,00000000
io,0x20,0xF5,0x00,0,00000000
io,0x20,0xF6,0x00,0,00000000
io,0x20,0xF7,0x00,0,00000000
io,0x20,0xF8,0x48,72,01001000
io,0x20,0xF9,0x00,0,00000000
io,0x20,0xFA,0x00,0,00000000
io,0x20,0xFB,0x00,0,00000000
io,0x20,0xFC,0x00,0,00000000
io,0x20,0xFD,0x46,70,01000110
io,0x20,0xFE,0x00,0,00000000
io,0x20,0xFF,0x00,0,00000000
cp,0x23,0x00,0x00,0,00000000
cp,0x23,0x01,0x00,0,00000000
cp,0x23,0x02,0x00,0,00000000
cp,0x23,0x03,0x00,0,00000000
cp,0x23,0x04,0x00,0,00000000
cp,0x23,0x05,0x00,0,00000000
cp,0x23,0x06,0x00,0,00000000
cp,0x23,0x07,0x00,0,00000000
cp,0x23,0x08,0x00,0,00000000
cp,0x23,0x09,0x02,2,00000010
cp,0x23,0x0A,0x00,0,00000000
cp,0x23,0x0B,0x40,64,01000000
cp,0x23,0x0C,0x00,0,00000000
cp,0x23,0x0D,0x00,0,00000000
cp,0x23,0x0E,0x00,0,00000000
cp,0x23,0x0F,0x00,0,00000000
cp,0x23,0x10,0x08,8,00001000
cp,0x23,0x11,0x00,0,00000000
cp,0x23,0x12,0x00,0,00000000
cp,0x23,0x13,0x00,0,00000000
cp,0x23,0x14,0x00,0,00000000
cp,0x23,0x15,0x01,1,00000001
cp,0x23,0x16,0x00,0,00000000
cp,0x23,0x17,0x00,0,00000000
cp,0x23,0x18,0x00,0,00000000
cp,0x23,0x19,0x00,0,00000000
cp,0x23,0x1A,0x00,0,00000000
cp,0x23,0x1B,0x20,32,00100000
cp,0x23,0x1C,0x00,0,00000000
cp,0x23,0x1D,0x00,0,00000000
cp,0x23,0x1E,0x00,0,00000000
cp,0x23,0x1F,0x00,0,00000000
cp,0x23,0x20,0x20,32,00100000
cp,0x23,0x21,0x00,0,00000000
cp,0x23,0x22,0x00,0,00000000
cp,0x23,0x23,0x00,0,00000000
cp,0x23,0x24,0x00,0,00000000
cp,0x23,0x25,0x00,0,00000000
cp,0x23,0x26,0x00,0,00000000
cp,0x23,0x27,0x00,0,00000000
cp,0x23,0x28,0x00,0,00000000
cp,0x23,0x29,0x00,0,00000000
cp,0x23,0x2A,0x00,0,00000000
cp,0x23,0x2B,0x00,0,00000000
cp,0x23,0x2C,0x00,0,00000000
cp,0x23,0x2D,0x00,0,00000000
cp,0x23,0x2E,0x00,0,00000000
cp,0x23,0x2F,0x00,0,00000000
cp,0x23,0x30,0x00,0,00000000
cp,0x23,0x31,0x00,0,00000000
cp,0x23,0x32,0x00,0,00000000
cp,0x23,0x33,0x00,0,00000000
cp,0x23,0x34,0x00,0,00000000
cp,0x23,0x35,0x00,0,00000000
cp,0x23,0x36,0x00,0,00000000
cp,0x23,0x37,0x00,0,00000000
cp,0x23,0x38,0x00,0,00000000
cp,0x23,0x39,0x00,0,00000000
cp,0x23,0x3A,0x80,128,10000000
cp,0x23,0x3B,0x80,128,10000000
cp,0x23,0x3C,0x00,0,00000000
cp,0x23,0x3D,0x00,0,00000000
cp,0x23,0x3E,0x04,4,00000100
cp,0x23,0x3F,0x00,0,00000000
cp,0x23,0x40,0x82,130,10000010
cp,0x23,0x41,0x1A,26,00011010
cp,0x23,0x42,0x3B,59,00111011
cp,0x23,0x43,0xD4,212,11010100
cp,0x23,0x44,0x03,3,00000011
cp,0x23,0x45,0x33,51,00110011
cp,0x23,0x46,0x00,0,00000000
cp,0x23,0x47,0x00,0,00000000
cp,0x23,0x48,0x00,0,00000000
cp,0x23,0x49,0xA1,161,10100001
cp,0x23,0x4A,0x1C,28,00011100
cp,0x23,0x4B,0x2C,44,00101100
cp,0x23,0x4C,0x64,100,01100100
cp,0x23,0x4D,0x12,18,00010010
cp,0x23,0x4E,0x35,53,00110101
cp,0x23,0x4F,0xFF,255,11111111
cp,0x23,0x50,0xC0,192,11000000
cp,0x23,0x51,0x00,0,00000000
cp,0x23,0x52,0x40,64,01000000
cp,0x23,0x53,0x00,0,00000000
cp,0x23,0x54,0x00,0,00000000
cp,0x23,0x55,0x00,0,00000000
cp,0x23,0x56,0x00,0,00000000
cp,0x23,0x57,0x08,8,00001000
cp,0x23,0x58,0x00,0,00000000
cp,0x23,0x59,0x00,0,00000000
cp,0x23,0x5A,0x00,0,00000000
cp,0x23,0x5B,0x00,0,00000000
cp,0x23,0x5C,0x01,1,00000001
cp,0x23,0x5D,0x00,0,00000000
cp,0x23,0x5E,0x00,0,00000000
cp,0x23,0x5F,0x00,0,00000000
cp,0x23,0x60,0x00,0,00000000
cp,0x23,0x61,0x00,0,00000000
cp,0x23,0x62,0x20,32,00100000
cp,0x23,0x63,0x00,0,00000000
cp,0x23,0x64,0x00,0,00000000
cp,0x23,0x65,0x00,0,00000000
cp,0x23,0x66,0x00,0,00000000
cp,0x23,0x67,0x00,0,00000000
cp,0x23,0x68,0xF0,240,11110000
cp,0x23,0x69,0x04,4,00000100
cp,0x23,0x6A,0x00,0,00000000
cp,0x23,0x6B,0x00,0,00000000
cp,0x23,0x6C,0x10,16,00010000
cp,0x23,0x6D,0x00,0,00000000
cp,0x23,0x6E,0x00,0,00000000
cp,0x23,0x6F,0x00,0,00000000
cp,0x23,0x70,0x00,0,00000000
cp,0x23,0x71,0x00,0,00000000
cp,0x23,0x72,0x00,0,00000000
cp,0x23,0x73,0x50,80,01010000
cp,0x23,0x74,0x04,4,00000100
cp,0x23,0x75,0x01,1,00000001
cp,0x23,0x76,0x00,0,00000000
cp,0x23,0x77,0xFF,255,11111111
cp,0x23,0x78,0xFF,255,11111111
cp,0x23,0x79,0xFF,255,11111111
cp,0x23,0x7A,0xFF,255,11111111
cp,0x23,0x7B,0x05,5,00000101
cp,0x23,0x7C,0xC0,192,11000000
cp,0x23,0x7D,0x00,0,00000000
cp,0x23,0x7E,0x00,0,00000000
cp,0x23,0x7F,0x00,0,00000000
cp,0x23,0x80,0x00,0,00000000
cp,0x23,0x81,0xC0,192,11000000
cp,0x23,0x82,0x04,4,00000100
cp,0x23,0x83,0x00,0,00000000
cp,0x23,0x84,0x0C,12,00001100
cp,0x23,0x85,0x0B,11,00001011
cp,0x23,0x86,0x0B,11,00001011
cp,0x23,0x87,0x00,0,00000000
cp,0x23,0x88,0x00,0,00000000
cp,0x23,0x89,0x00,0,00000000
cp,0x23,0x8A,0x20,32,00100000
cp,0x23,0x8B,0x40,64,01000000
cp,0x23,0x8C,0x04,4,00000100
cp,0x23,0x8D,0x00,0,00000000
cp,0x23,0x8E,0x00,0,00000000
cp,0x23,0x8F,0x40,64,01000000
cp,0x23,0x90,0x00,0,00000000
cp,0x23,0x91,0x40,64,01000000
cp,0x23,0x92,0x00,0,00000000
cp,0x23,0x93,0x00,0,00000000
cp,0x23,0x94,0x00,0,00000000
cp,0x23,0x95,0x00,0,00000000
cp,0x23,0x96,0x00,0,00000000
cp,0x23,0x97,0xF0,240,11110000
cp,0x23,0x98,0x00,0,00000000
cp,0x23,0x99,0x00,0,00000000
cp,0x23,0x9A,0x00,0,00000000
cp,0x23,0x9B,0x00,0,00000000
cp,0x23,0x9C,0x00,0,00000000
cp,0x23,0x9D,0x00,0,00000000
cp,0x23,0x9E,0x00,0,00000000
cp,0x23,0x9F,0x00,0,00000000
cp,0x23,0xA0,0x00,0,00000000
cp,0x23,0xA1,0x00,0,00000000
cp,0x23,0xA2,0x00,0,00000000
cp,0x23,0xA3,0x00,0,00000000
cp,0x23,0xA4,0x00,0,00000000
cp,0x23,0xA5,0x00,0,00000000
cp,0x23,0xA6,0x00,0,00000000
cp,0x23,0xA7,0x00,0,00000000
cp,0x23,0xA8,0x00,0,00000000
cp,0x23,0xA9,0x00,0,00000000
cp,0x23,0xAA,0x00,0,00000000
cp,0x23,0xAB,0x00,0,00000000
cp,0x23,0xAC,0x00,0,00000000
cp,0x23,0xAD,0x00,0,00000000
cp,0x23,0xAE,0x60,96,01100000
cp,0x23,0xAF,0x00,0,00000000
cp,0x23,0xB0,0x00,0,00000000
cp,0x23,0xB1,0xA1,161,10100001
cp,0x23,0xB2,0x1C,28,00011100
cp,0x23,0xB3,0x2C,44,00101100
cp,0x23,0xB4,0x64,100,01100100
cp,0x23,0xB5,0xFD,253,11111101
cp,0x23,0xB6,0x00,0,00000000
cp,0x23,0xB7,0x4A,74,01001010
cp,0x23,0xB8,0x12,18,00010010
cp,0x23,0xB9,0x35,53,00110101
cp,0x23,0xBA,0x01,1,00000001
cp,0x23,0xBB,0x00,0,00000000
cp,0x23,0xBC,0x00,0,00000000
cp,0x23,0xBD,0x18,24,00011000
cp,0x23,0xBE,0x00,0,00000000
cp,0x23,0xBF,0x00,0,00000000
cp,0x23,0xC0,0x00,0,00000000
cp,0x23,0xC1,0x00,0,00000000
cp,0x23,0xC2,0x00,0,00000000
cp,0x23,0xC3,0x39,57,00111001
cp,0x23,0xC4,0x44,68,01000100
cp,0x23,0xC5,0x91,145,10010001
cp,0x23,0xC6,0x00,0,00000000
cp,0x23,0xC7,0x00,0,00000000
cp,0x23,0xC8,0x00,0,00000000
cp,0x23,0xC9,0x2C,44,00101100
cp,0x23,0xCA,0x00,0,00000000
cp,0x23,0xCB,0x60,96,01100000
cp,0x23,0xCC,0x42,66,01000010
cp,0x23,0xCD,0xFF,255,11111111
cp,0x23,0xCE,0x3F,63,00111111
cp,0x23,0xCF,0x00,0,00000000
cp,0x23,0xD0,0x00,0,00000000
cp,0x23,0xD1,0x00,0,00000000
cp,0x23,0xD2,0x00,0,00000000
cp,0x23,0xD3,0x00,0,00000000
cp,0x23,0xD4,0x00,0,00000000
cp,0x23,0xD5,0x00,0,00000000
cp,0x23,0xD6,0x00,0,00000000
cp,0x23,0xD7,0x00,0,00000000
cp,0x23,0xD8,0x00,0,00000000
cp,0x23,0xD9,0x00,0,00000000
cp,0x23,0xDA,0x00,0,00000000
cp,0x23,0xDB,0x19,25,00011001
cp,0x23,0xDC,0x64,100,01100100
cp,0x23,0xDD,0x12,18,00010010
cp,0x23,0xDE,0xC5,197,11000101
cp,0x23,0xDF,0x78,120,01111000
cp,0x23,0xE0,0x53,83,01010011
cp,0x23,0xE1,0xFF,255,11111111
cp,0x23,0xE2,0xFF,255,11111111
cp,0x23,0xE3,0x1C,28,00011100
cp,0x23,0xE4,0x00,0,00000000
cp,0x23,0xE5,0x00,0,00000000
cp,0x23,0xE6,0x99,153,10011001
cp,0x23,0xE7,0x02,2,00000010
cp,0x23,0xE8,0x33,51,00110011
cp,0x23,0xE9,0x01,1,00000001
cp,0x23,0xEA,0x03,3,00000011
cp,0x23,0xEB,0x09,9,00001001
cp,0x23,0xEC,0x3A,58,00111010
cp,0x23,0xED,0x10,16,00010000
cp,0x23,0xEE,0x0A,10,00001010
cp,0x23,0xEF,0x05,5,00000101
cp,0x23,0xF0,0x05,5,00000101
cp,0x23,0xF1,0x40,64,01000000
cp,0x23,0xF2,0x04,4,00000100
cp,0x23,0xF3,0xE4,228,11100100
cp,0x23,0xF4,0x00,0,00000000
cp,0x23,0xF5,0x00,0,00000000
cp,0x23,0xF6,0x00,0,00000000
cp,0x23,0xF7,0x15,21,00010101
cp,0x23,0xF8,0x03,3,00000011
cp,0x23,0xF9,0x33,51,00110011
cp,0x23,0xFA,0x06,6,00000110
cp,0x23,0xFB,0x57,87,01010111
cp,0x23,0xFC,0x04,4,00000100
cp,0x23,0xFD,0x65,101,01100101
cp,0x23,0xFE,0x03,3,00000011
cp,0x23,0xFF,0x08,8,00001000
afe,0x24,0x00,0x00,0,00000000
afe,0x24,0x01,0x06,6,00000110
afe,0x24,0x02,0xC0,192,11000000
afe,0x24,0x03,0x12,18,00010010
afe,0x24,0x04,0x30,48,00110000
afe,0x24,0x05,0x0F,15,00001111
afe,0x24,0x06,0x00,0,00000000
afe,0x24,0x07,0x1F,31,00011111
afe,0x24,0x08,0x00,0,00000000
afe,0x24,0x09,0x00,0,00000000
afe,0x24,0x0A,0x00,0,00000000
afe,0x24,0x0B,0x00,0,00000000
afe,0x24,0x0C,0x0D,13,00001101
afe,0x24,0x0D,0x13,19,00010011
afe,0x24,0x0E,0x00,0,00000000
afe,0x24,0x0F,0x90,144,10010000
afe,0x24,0x10,0x30,48,00110000
afe,0x24,0x11,0x82,130,10000010
afe,0x24,0x12,0xFF,255,11111111
afe,0x24,0x13,0x00,0,00000000
afe,0x24,0x14,0x09,9,00001001
afe,0x24,0x15,0x0A,10,00001010
afe,0x24,0x16,0x98,152,10011000
afe,0x24,0x17,0x00,0,00000000
afe,0x24,0x18,0x00,0,00000000
afe,0x24,0x19,0x00,0,00000000
afe,0x24,0x1A,0x00,0,00000000
afe,0x24,0x1B,0x00,0,00000000
afe,0x24,0x1C,0x00,0,00000000
afe,0x24,0x1D,0x6D,109,01101101
afe,0x24,0x1E,0x6D,109,01101101
afe,0x24,0x1F,0x6D,109,01101101
afe,0x24,0x20,0x6D,109,01101101
afe,0x24,0x21,0x6D,109,01101101
afe,0x24,0x22,0x6D,109,01101101
afe,0x24,0x23,0x6D,109,01101101
afe,0x24,0x24,0x6D,109,01101101
afe,0x24,0x25,0x00,0,00000000
afe,0x24,0x26,0x08,8,00001000
afe,0x24,0x27,0xFF,255,11111111
afe,0x24,0x28,0xFF,255,11111111
afe,0x24,0x29,0x00,0,00000000
afe,0x24,0x2A,0x00,0,00000000
afe,0x24,0x2B,0x00,0,00000000
afe,0x24,0x2C,0x00,0,00000000
afe,0x24,0x2D,0x00,0,00000000
afe,0x24,0x2E,0x00,0,00000000
afe,0x24,0x2F,0x00,0,00000000
afe,0x24,0x30,0x00,0,00000000
afe,0x24,0x31,0x00,0,00000000
afe,0x24,0x32,0x00,0,00000000
afe,0x24,0x33,0x00,0,00000000
afe,0x24,0x34,0x00,0,00000000
afe,0x24,0x35,0x00,0,00000000
afe,0x24,0x36,0x00,0,00000000
afe,0x24,0x37,0x00,0,00000000
afe,0x24,0x38,0x00,0,00000000
afe,0x24,0x39,0x00,0,00000000
afe,0x24,0x3A,0x00,0,00000000
afe,0x24,0x3B,0x00,0,00000000
afe,0x24,0x3C,0x00,0,00000000
afe,0x24,0x3D,0x00,0,00000000
afe,0x24,0x3E,0x00,0,00000000
afe,0x24,0x3F,0x00,0,00000000
afe,0x24,0x40,0x00,0,00000000
afe,0x24,0x41,0x00,0,00000000
afe,0x24,0x42,0x00,0,00000000
afe,0x24,0x43,0x00,0,00000000
afe,0x24,0x44,0x00,0,00000000
afe,0x24,0x45,0x00,0,00000000
afe,0x24,0x46,0x00,0,00000000
afe,0x24,0x47,0x00,0,00000000
afe,0x24,0x48,0x00,0,00000000
afe,0x24,0x49,0x00,0,00000000
afe,0x24,0x4A,0x00,0,00000000
afe,0x24,0x4B,0x00,0,00000000
afe,0x24,0x4C,0x00,0,00000000
afe,0x24,0x4D,0x00,0,00000000
afe,0x24,0x4E,0x00,0,00000000
afe,0x24,0x4F,0x00,0,00000000
afe,0x24,0x50,0x00,0,00000000
afe,0x24,0x51,0x00,0,00000000
afe,0x24,0x52,0x00,0,00000000
afe,0x24,0x53,0x00,0,00000000
afe,0x24,0x54,0x00,0,00000000
afe,0x24,0x55,0x00,0,00000000
afe,0x24,0x56,0x00,0,00000000
afe,0x24,0x57,0x00,0,00000000
afe,0x24,0x58,0x00,0,00000000
afe,0x24,0x59,0x00,0,00000000
afe,0x24,0x5A,0x00,0,00000000
afe,0x24,0x5B,0x00,0,00000000
afe,0x24,0x5C,0x00,0,00000000
afe,0x24,0x5D,0x00,0,00000000
afe,0x24,0x5E,0x00,0,00000000
afe,0x24,0x5F,0x00,0,00000000
afe,0x24,0x60,0x00,0,00000000
afe,0x24,0x61,0x00,0,00000000
afe,0x24,0x62,0x00,0,00000000
afe,0x24,0x63,0x00,0,00000000
afe,0x24,0x64,0x00,0,00000000
afe,0x24,0x65,0x00,0,00000000
afe,0x24,0x66,0x00,0,00000000
afe,0x24,0x67,0x00,0,00000000
afe,0x24,0x68,0x00,0,00000000
afe,0x24,0x69,0x00,0,00000000
afe,0x24,0x6A,0x00,0,00000000
afe,0x24,0x6B,0x00,0,00000000
afe,0x24,0x6C,0x00,0,00000000
afe,0x24,0x6D,0x00,0,00000000
afe,0x24,0x6E,0x00,0,00000000
afe,0x24,0x6F,0x00,0,00000000
afe,0x24,0x70,0x00,0,00000000
afe,0x24,0x71,0x00,0,00000000
afe,0x24,0x72,0x00,0,00000000
afe,0x24,0x73,0x00,0,00000000
afe,0x24,0x74,0x00,0,00000000
afe,0x24,0x75,0x00,0,00000000
afe,0x24,0x76,0x00,0,00000000
afe,0x24,0x77,0x00,0,00000000
afe,0x24,0x78,0x00,0,00000000
afe,0x24,0x79,0x00,0,00000000
afe,0x24,0x7A,0x00,0,00000000
afe,0x24,0x7B,0x00,0,00000000
afe,0x24,0x7C,0x00,0,00000000
afe,0x24,0x7D,0x00,0,00000000
afe,0x24,0x7E,0x00,0,00000000
afe,0x24,0x7F,0x00,0,00000000
afe,0x24,0x80,0x80,128,10000000
afe,0x24,0x81,0x20,32,00100000
afe,0x24,0x82,0x80,128,10000000
afe,0x24,0x83,0x02,2,00000010
afe,0x24,0x84,0x02,2,00000010
afe,0x24,0x85,0x0A,10,00001010
afe,0x24,0x86,0x0A,10,00001010
afe,0x24,0x87,0x0A,10,00001010
afe,0x24,0x88,0xF8,248,11111000
afe,0x24,0x89,0x66,102,01100110
afe,0x24,0x8A,0xFC,252,11111100
afe,0x24,0x8B,0x13,19,00010011
afe,0x24,0x8C,0xF8,248,11111000
afe,0x24,0x8D,0x15,21,00010101
afe,0x24,0x8E,0xDE,222,11011110
afe,0x24,0x8F,0x86,134,10000110
afe,0x24,0x90,0xC1,193,11000001
afe,0x24,0x91,0x91,145,10010001
afe,0x24,0x92,0x82,130,10000010
afe,0x24,0x93,0x70,112,01110000
afe,0x24,0x94,0x00,0,00000000
afe,0x24,0x95,0x00,0,00000000
afe,0x24,0x96,0x00,0,00000000
afe,0x24,0x97,0x00,0,00000000
afe,0x24,0x98,0xFF,255,11111111
afe,0x24,0x99,0x0F,15,00001111
afe,0x24,0x9A,0xFF,255,11111111
afe,0x24,0x9B,0x00,0,00000000
afe,0x24,0x9C,0x00,0,00000000
afe,0x24,0x9D,0x00,0,00000000
afe,0x24,0x9E,0x00,0,00000000
afe,0x24,0x9F,0x00,0,00000000
afe,0x24,0xA0,0x00,0,00000000
afe,0x24,0xA1,0x02,2,00000010
afe,0x24,0xA2,0x02,2,00000010
afe,0x24,0xA3,0xFF,255,11111111
afe,0x24,0xA4,0xFF,255,11111111
afe,0x24,0xA5,0xFF,255,11111111
afe,0x24,0xA6,0xF8,248,11111000
afe,0x24,0xA7,0x66,102,01100110
afe,0x24,0xA8,0xFC,252,11111100
afe,0x24,0xA9,0x13,19,00010011
afe,0x24,0xAA,0xF8,248,11111000
afe,0x24,0xAB,0x15,21,00010101
afe,0x24,0xAC,0xDE,222,11011110
afe,0x24,0xAD,0x86,134,10000110
afe,0x24,0xAE,0xC1,193,11000001
afe,0x24,0xAF,0x91,145,10010001
afe,0x24,0xB0,0x82,130,10000010
afe,0x24,0xB1,0x70,112,01110000
afe,0x24,0xB2,0xFF,255,11111111
afe,0x24,0xB3,0x0F,15,00001111
afe,0x24,0xB4,0xFF,255,11111111
afe,0x24,0xB5,0x01,1,00000001
afe,0x24,0xB6,0x00,0,00000000
afe,0x24,0xB7,0x00,0,00000000
afe,0x24,0xB8,0x00,0,00000000
afe,0x24,0xB9,0x00,0,00000000
afe,0x24,0xBA,0x00,0,00000000
afe,0x24,0xBB,0x00,0,00000000
afe,0x24,0xBC,0x00,0,00000000
afe,0x24,0xBD,0x6F,111,01101111
afe,0x24,0xBE,0x02,2,00000010
afe,0x24,0xBF,0xFA,250,11111010
afe,0x24,0xC0,0xC0,192,11000000
afe,0x24,0xC1,0x98,152,10011000
afe,0x24,0xC2,0x80,128,10000000
afe,0x24,0xC3,0x00,0,00000000
afe,0x24,0xC4,0x30,48,00110000
afe,0x24,0xC5,0x02,2,00000010
afe,0x24,0xC6,0x03,3,00000011
afe,0x24,0xC7,0x00,0,00000000
afe,0x24,0xC8,0x00,0,00000000
afe,0x24,0xC9,0x00,0,00000000
afe,0x24,0xCA,0x00,0,00000000
afe,0x24,0xCB,0x00,0,00000000
afe,0x24,0xCC,0x40,64,01000000
afe,0x24,0xCD,0x0A,10,00001010
afe,0x24,0xCE,0x96,150,10010110
afe,0x24,0xCF,0x00,0,00000000
afe,0x24,0xD0,0x25,37,00100101
afe,0x24,0xD1,0x23,35,00100011
afe,0x24,0xD2,0xE1,225,11100001
afe,0x24,0xD3,0xAE,174,10101110
afe,0x24,0xD4,0xFF,255,11111111
afe,0x24,0xD5,0xCC,204,11001100
afe,0x24,0xD6,0x05,5,00000101
afe,0x24,0xD7,0x00,0,00000000
afe,0x24,0xD8,0x00,0,00000000
afe,0x24,0xD9,0x1B,27,00011011
afe,0x24,0xDA,0x04,4,00000100
afe,0x24,0xDB,0x00,0,00000000
afe,0x24,0xDC,0x00,0,00000000
afe,0x24,0xDD,0x00,0,00000000
afe,0x24,0xDE,0x00,0,00000000
afe,0x24,0xDF,0x00,0,00000000
afe,0x24,0xE0,0x00,0,00000000
afe,0x24,0xE1,0x00,0,00000000
afe,0x24,0xE2,0x00,0,00000000
afe,0x24,0xE3,0x00,0,00000000
afe,0x24,0xE4,0x06,6,00000110
afe,0x24,0xE5,0x06,6,00000110
afe,0x24,0xE6,0x00,0,00000000
afe,0x24,0xE7,0x00,0,00000000
afe,0x24,0xE8,0x00,0,00000000
afe,0x24,0xE9,0x00,0,00000000
afe,0x24,0xEA,0x00,0,00000000
afe,0x24,0xEB,0x00,0,00000000
afe,0x24,0xEC,0x00,0,00000000
afe,0x24,0xED,0x00,0,00000000
afe,0x24,0xEE,0x00,0,00000000
afe,0x24,0xEF,0x00,0,00000000
afe,0x24,0xF0,0x00,0,00000000
afe,0x24,0xF1,0x00,0,00000000
afe,0x24,0xF2,0x00,0,00000000
afe,0x24,0xF3,0x00,0,00000000
afe,0x24,0xF4,0x00,0,00000000
afe,0x24,0xF5,0x00,0,00000000
afe,0x24,0xF6,0x00,0,00000000
afe,0x24,0xF7,0x00,0,00000000
afe,0x24,0xF8,0x00,0,00000000
afe,0x24,0xF9,0x00,0,00000000
afe,0x24,0xFA,0x00,0,00000000
afe,0x24,0xFB,0x00,0,00000000
afe,0x24,0xFC,0x00,0,00000000
afe,0x24,0xFD,0x00,0,00000000
afe,0x24,0xFE,0x00,0,00000000
afe,0x24,0xFF,0x00,0,00000000
sdp,0x22,0x00,0x02,2,00000010
sdp,0x22,0x01,0x36,54,00110110
sdp,0x22,0x02,0x27,39,00100111
sdp,0x22,0x03,0xC4,196,11000100
sdp,0x22,0x04,0x0B,11,00001011
sdp,0x22,0x05,0xC3,195,11000011
sdp,0x22,0x06,0xC0,192,11000000
sdp,0x22,0x07,0x8B,139,10001011
sdp,0x22,0x08,0x1A,26,00011010
sdp,0x22,0x09,0x00,0,00000000
sdp,0x22,0x0A,0xE5,229,11100101
sdp,0x22,0x0B,0xE5,229,11100101
sdp,0x22,0x0C,0xE5,229,11100101
sdp,0x22,0x0D,0xE4,228,11100100
sdp,0x22,0x0E,0x31,49,00110001
sdp,0x22,0x0F,0x00,0,00000000
sdp,0x22,0x10,0x01,1,00000001
sdp,0x22,0x11,0x10,16,00010000
sdp,0x22,0x12,0x01,1,00000001
sdp,0x22,0x13,0x80,128,10000000
sdp,0x22,0x14,0x00,0,00000000
sdp,0x22,0x15,0x80,128,10000000
sdp,0x22,0x16,0x00,0,00000000
sdp,0x22,0x17,0x00,0,00000000
sdp,0x22,0x18,0xFF,255,11111111
sdp,0x22,0x19,0xCD,205,11001101
sdp,0x22,0x1A,0x95,149,10010101
sdp,0x22,0x1B,0x1E,30,00011110
sdp,0x22,0x1C,0xC4,196,11000100
sdp,0x22,0x1D,0x02,2,00000010
sdp,0x22,0x1E,0x04,4,00000100
sdp,0x22,0x1F,0x12,18,00010010
sdp,0x22,0x20,0x00,0,00000000
sdp,0x22,0x21,0xFF,255,11111111
sdp,0x22,0x22,0x20,32,00100000
sdp,0x22,0x23,0x10,16,00010000
sdp,0x22,0x24,0x4C,76,01001100
sdp,0x22,0x25,0x00,0,00000000
sdp,0x22,0x26,0x8F,143,10001111
sdp,0x22,0x27,0xAA,170,10101010
sdp,0x22,0x28,0x02,2,00000010
sdp,0x22,0x29,0x00,0,00000000
sdp,0x22,0x2A,0x00,0,00000000
sdp,0x22,0x2B,0x00,0,00000000
sdp,0x22,0x2C,0x00,0,00000000
sdp,0x22,0x2D,0x3D,61,00111101
sdp,0x22,0x2E,0x00,0,00000000
sdp,0x22,0x2F,0x00,0,00000000
sdp,0x22,0x30,0x00,0,00000000
sdp,0x22,0x31,0x04,4,00000100
sdp,0x22,0x32,0x00,0,00000000
sdp,0x22,0x33,0x80,128,10000000
sdp,0x22,0x34,0xA0,160,10100000
sdp,0x22,0x35,0x4E,78,01001110
sdp,0x22,0x36,0x42,66,01000010
sdp,0x22,0x37,0x5A,90,01011010
sdp,0x22,0x38,0x49,73,01001001
sdp,0x22,0x39,0x00,0,00000000
sdp,0x22,0x3A,0x00,0,00000000
sdp,0x22,0x3B,0x40,64,01000000
sdp,0x22,0x3C,0x30,48,00110000
sdp,0x22,0x3D,0x0E,14,00001110
sdp,0x22,0x3E,0x8A,138,10001010
sdp,0x22,0x3F,0x73,115,01110011
sdp,0x22,0x40,0x4C,76,01001100
sdp,0x22,0x41,0xC6,198,11000110
sdp,0x22,0x42,0x33,51,00110011
sdp,0x22,0x43,0xA0,160,10100000
sdp,0x22,0x44,0x14,20,00010100
sdp,0x22,0x45,0x43,67,01000011
sdp,0x22,0x46,0x73,115,01110011
sdp,0x22,0x47,0xB3,179,10110011
sdp,0x22,0x48,0x01,1,00000001
sdp,0x22,0x49,0x40,64,01000000
sdp,0x22,0x4A,0x4B,75,01001011
sdp,0x22,0x4B,0xDF,223,11011111
sdp,0x22,0x4C,0x00,0,00000000
sdp,0x22,0x4D,0x00,0,00000000
sdp,0x22,0x4E,0x00,0,00000000
sdp,0x22,0x4F,0x00,0,00000000
sdp,0x22,0x50,0x00,0,00000000
sdp,0x22,0x51,0x00,0,00000000
sdp,0x22,0x52,0x00,0,00000000
sdp,0x22,0x53,0x00,0,00000000
sdp,0x22,0x54,0x04,4,00000100
sdp,0x22,0x55,0x00,0,00000000
sdp,0x22,0x56,0x78,120,01111000
sdp,0x22,0x57,0x10,16,00010000
sdp,0x22,0x58,0x00,0,00000000
sdp,0x22,0x59,0x04,4,00000100
sdp,0x22,0x5A,0x00,0,00000000
sdp,0x22,0x5B,0x44,68,01000100
sdp,0x22,0x5C,0x16,22,00010110
sdp,0x22,0x5D,0x1B,27,00011011
sdp,0x22,0x5E,0x02,2,00000010
sdp,0x22,0x5F,0xEA,234,11101010
sdp,0x22,0x60,0x68,104,01101000
sdp,0x22,0x61,0x06,6,00000110
sdp,0x22,0x62,0x00,0,00000000
sdp,0x22,0x63,0x60,96,01100000
sdp,0x22,0x64,0x01,1,00000001
sdp,0x22,0x65,0x53,83,01010011
sdp,0x22,0x66,0x00,0,00000000
sdp,0x22,0x67,0x9C,156,10011100
sdp,0x22,0x68,0x17,23,00010111
sdp,0x22,0x69,0x14,20,00010100
sdp,0x22,0x6A,0x77,119,01110111
sdp,0x22,0x6B,0xE1,225,11100001
sdp,0x22,0x6C,0x85,133,10000101
sdp,0x22,0x6D,0x83,131,10000011
sdp,0x22,0x6E,0x14,20,00010100
sdp,0x22,0x6F,0x0B,11,00001011
sdp,0x22,0x70,0xB8,184,10111000
sdp,0x22,0x71,0xB0,176,10110000
sdp,0x22,0x72,0xA4,164,10100100
sdp,0x22,0x73,0xF7,247,11110111
sdp,0x22,0x74,0x50,80,01010000
sdp,0x22,0x75,0x96,150,10010110
sdp,0x22,0x76,0x00,0,00000000
sdp,0x22,0x77,0x00,0,00000000
sdp,0x22,0x78,0x1F,31,00011111
sdp,0x22,0x79,0xF1,241,11110001
sdp,0x22,0x7A,0x7F,127,01111111
sdp,0x22,0x7B,0x69,105,01101001
sdp,0x22,0x7C,0xF8,248,11111000
sdp,0x22,0x7D,0xEA,234,11101010
sdp,0x22,0x7E,0x11,17,00010001
sdp,0x22,0x7F,0x3A,58,00111010
sdp,0x22,0x80,0xAA,170,10101010
sdp,0x22,0x81,0x22,34,00100010
sdp,0x22,0x82,0x08,8,00001000
sdp,0x22,0x83,0x3B,59,00111011
sdp,0x22,0x84,0xD3,211,11010011
sdp,0x22,0x85,0xF3,243,11110011
sdp,0x22,0x86,0x20,32,00100000
sdp,0x22,0x87,0xC1,193,11000001
sdp,0x22,0x88,0x41,65,01000001
sdp,0x22,0x89,0x03,3,00000011
sdp,0x22,0x8A,0x00,0,00000000
sdp,0x22,0x8B,0x02,2,00000010
sdp,0x22,0x8C,0x40,64,01000000
sdp,0x22,0x8D,0x08,8,00001000
sdp,0x22,0x8E,0x70,112,01110000
sdp,0x22,0x8F,0x02,2,00000010
sdp,0x22,0x90,0xEE,238,11101110
sdp,0x22,0x91,0x22,34,00100010
sdp,0x22,0x92,0x33,51,00110011
sdp,0x22,0x93,0x01,1,00000001
sdp,0x22,0x94,0x93,147,10010011
sdp,0x22,0x95,0x0D,13,00001101
sdp,0x22,0x96,0x14,20,00010100
sdp,0x22,0x97,0x14,20,00010100
sdp,0x22,0x98,0xBF,191,10111111
sdp,0x22,0x99,0x10,16,00010000
sdp,0x22,0x9A,0x01,1,00000001
sdp,0x22,0x9B,0x55,85,01010101
sdp,0x22,0x9C,0x03,3,00000011
sdp,0x22,0x9D,0x8A,138,10001010
sdp,0x22,0x9E,0x1E,30,00011110
sdp,0x22,0x9F,0x7F,127,01111111
sdp,0x22,0xA0,0x08,8,00001000
sdp,0x22,0xA1,0x50,80,01010000
sdp,0x22,0xA2,0xA0,160,10100000
sdp,0x22,0xA3,0xBE,190,10111110
sdp,0x22,0xA4,0xBF,191,10111111
sdp,0x22,0xA5,0xBF,191,10111111
sdp,0x22,0xA6,0x00,0,00000000
sdp,0x22,0xA7,0x04,4,00000100
sdp,0x22,0xA8,0x40,64,01000000
sdp,0x22,0xA9,0x88,136,10001000
sdp,0x22,0xAA,0x88,136,10001000
sdp,0x22,0xAB,0x00,0,00000000
sdp,0x22,0xAC,0x22,34,00100010
sdp,0x22,0xAD,0x22,34,00100010
sdp,0x22,0xAE,0xCF,207,11001111
sdp,0x22,0xAF,0x84,132,10000100
sdp,0x22,0xB0,0x28,40,00101000
sdp,0x22,0xB1,0x84,132,10000100
sdp,0x22,0xB2,0x14,20,00010100
sdp,0x22,0xB3,0x64,100,01100100
sdp,0x22,0xB4,0x24,36,00100100
sdp,0x22,0xB5,0x24,36,00100100
sdp,0x22,0xB6,0x1F,31,00011111
sdp,0x22,0xB7,0xA4,164,10100100
sdp,0x22,0xB8,0x44,68,01000100
sdp,0x22,0xB9,0x42,66,01000010
sdp,0x22,0xBA,0x12,18,00010010
sdp,0x22,0xBB,0x13,19,00010011
sdp,0x22,0xBC,0x20,32,00100000
sdp,0x22,0xBD,0x38,56,00111000
sdp,0x22,0xBE,0x2B,43,00101011
sdp,0x22,0xBF,0xA9,169,10101001
sdp,0x22,0xC0,0x52,82,01010010
sdp,0x22,0xC1,0x53,83,01010011
sdp,0x22,0xC2,0x24,36,00100100
sdp,0x22,0xC3,0x44,68,01000100
sdp,0x22,0xC4,0x0C,12,00001100
sdp,0x22,0xC5,0xD4,212,11010100
sdp,0x22,0xC6,0x72,114,01110010
sdp,0x22,0xC7,0xF1,241,11110001
sdp,0x22,0xC8,0x81,129,10000001
sdp,0x22,0xC9,0x89,137,10001001
sdp,0x22,0xCA,0x28,40,00101000
sdp,0x22,0xCB,0x00,0,00000000
sdp,0x22,0xCC,0x00,0,00000000
sdp,0x22,0xCD,0x00,0,00000000
sdp,0x22,0xCE,0x02,2,00000010
sdp,0x22,0xCF,0x00,0,00000000
sdp,0x22,0xD0,0x98,152,10011000
sdp,0x22,0xD1,0x41,65,01000001
sdp,0x22,0xD2,0x1E,30,00011110
sdp,0x22,0xD3,0xA2,162,10100010
sdp,0x22,0xD4,0x50,80,01010000
sdp,0x22,0xD5,0x10,16,00010000
sdp,0x22,0xD6,0xCC,204,11001100
sdp,0x22,0xD7,0x04,4,00000100
sdp,0x22,0xD8,0x00,0,00000000
sdp,0x22,0xD9,0x44,68,01000100
sdp,0x22,0xDA,0x00,0,00000000
sdp,0x22,0xDB,0x88,136,10001000
sdp,0x22,0xDC,0x02,2,00000010
sdp,0x22,0xDD,0xBC,188,10111100
sdp,0x22,0xDE,0x23,35,00100011
sdp,0x22,0xDF,0x7D,125,01111101
sdp,0x22,0xE0,0x04,4,00000100
sdp,0x22,0xE1,0x00,0,00000000
sdp,0x22,0xE2,0x48,72,01001000
sdp,0x22,0xE3,0x00,0,00000000
sdp,0x22,0xE4,0x00,0,00000000
sdp,0x22,0xE5,0x09,9,00001001
sdp,0x22,0xE6,0x3B,59,00111011
sdp,0x22,0xE7,0x00,0,00000000
sdp,0x22,0xE8,0x00,0,00000000
sdp,0x22,0xE9,0x84,132,10000100
sdp,0x22,0xEA,0x84,132,10000100
sdp,0x22,0xEB,0x4B,75,01001011
sdp,0x22,0xEC,0x4C,76,01001100
sdp,0x22,0xED,0xC0,192,11000000
sdp,0x22,0xEE,0xC0,192,11000000
sdp,0x22,0xEF,0x02,2,00000010
sdp,0x22,0xF0,0x82,130,10000010
sdp,0x22,0xF1,0x98,152,10011000
sdp,0x22,0xF2,0x18,24,00011000
sdp,0x22,0xF3,0xB0,176,10110000
sdp,0x22,0xF4,0x30,48,00110000
sdp,0x22,0xF5,0x1A,26,00011010
sdp,0x22,0xF6,0x1A,26,00011010
sdp,0x22,0xF7,0x1A,26,00011010
sdp,0x22,0xF8,0x1A,26,00011010
sdp,0x22,0xF9,0xBF,191,10111111
sdp,0x22,0xFA,0x18,24,00011000
sdp,0x22,0xFB,0x3F,63,00111111
sdp,0x22,0xFC,0x18,24,00011000
sdp,0x22,0xFD,0x29,41,00101001
sdp,0x22,0xFE,0x04,4,00000100
sdp,0x22,0xFF,0x93,147,10010011
sdpio,0x25,0x00,0x00,0,00000000
sdpio,0x25,0x01,0x00,0,00000000
sdpio,0x25,0x02,0x00,0,00000000
sdpio,0x25,0x03,0x00,0,00000000
sdpio,0x25,0x04,0x00,0,00000000
sdpio,0x25,0x05,0x00,0,00000000
sdpio,0x25,0x06,0x00,0,00000000
sdpio,0x25,0x07,0x00,0,00000000
sdpio,0x25,0x08,0x00,0,00000000
sdpio,0x25,0x09,0x00,0,00000000
sdpio,0x25,0x0A,0x00,0,00000000
sdpio,0x25,0x0B,0x00,0,00000000
sdpio,0x25,0x0C,0x00,0,00000000
sdpio,0x25,0x0D,0x00,0,00000000
sdpio,0x25,0x0E,0x00,0,00000000
sdpio,0x25,0x0F,0x00,0,00000000
sdpio,0x25,0x10,0x00,0,00000000
sdpio,0x25,0x11,0x00,0,00000000
sdpio,0x25,0x12,0x00,0,00000000
sdpio,0x25,0x13,0x00,0,00000000
sdpio,0x25,0x14,0x00,0,00000000
sdpio,0x25,0x15,0x00,0,00000000
sdpio,0x25,0x16,0x00,0,00000000
sdpio,0x25,0x17,0x00,0,00000000
sdpio,0x25,0x18,0x00,0,00000000
sdpio,0x25,0x19,0x00,0,00000000
sdpio,0x25,0x1A,0x00,0,00000000
sdpio,0x25,0x1B,0x00,0,00000000
sdpio,0x25,0x1C,0x00,0,00000000
sdpio,0x25,0x1D,0x00,0,00000000
sdpio,0x25,0x1E,0x00,0,00000000
sdpio,0x25,0x1F,0x00,0,00000000
sdpio,0x25,0x20,0x00,0,00000000
sdpio,0x25,0x21,0x00,0,00000000
sdpio,0x25,0x22,0x00,0,00000000
sdpio,0x25,0x23,0x00,0,00000000
sdpio,0x25,0x24,0x00,0,00000000
sdpio,0x25,0x25,0x00,0,00000000
sdpio,0x25,0x26,0x00,0,00000000
sdpio,0x25,0x27,0x08,8,00001000
sdpio,0x25,0x28,0x00,0,00000000
sdpio,0x25,0x29,0x00,0,00000000
sdpio,0x25,0x2A,0x00,0,00000000
sdpio,0x25,0x2B,0x00,0,00000000
sdpio,0x25,0x2C,0x00,0,00000000
sdpio,0x25,0x2D,0x00,0,00000000
sdpio,0x25,0x2E,0x00,0,00000000
sdpio,0x25,0x2F,0x00,0,00000000
sdpio,0x25,0x30,0x00,0,00000000
sdpio,0x25,0x31,0x00,0,00000000
sdpio,0x25,0x32,0x00,0,00000000
sdpio,0x25,0x33,0x00,0,00000000
sdpio,0x25,0x34,0x00,0,00000000
sdpio,0x25,0x35,0x00,0,00000000
sdpio,0x25,0x36,0x01,1,00000001
sdpio,0x25,0x37,0x00,0,00000000
sdpio,0x25,0x38,0x00,0,00000000
sdpio,0x25,0x39,0x00,0,00000000
sdpio,0x25,0x3A,0x00,0,00000000
sdpio,0x25,0x3B,0x00,0,00000000
sdpio,0x25,0x3C,0x00,0,00000000
sdpio,0x25,0x3D,0x00,0,00000000
sdpio,0x25,0x3E,0x00,0,00000000
sdpio,0x25,0x3F,0x00,0,00000000
sdpio,0x25,0x40,0x00,0,00000000
sdpio,0x25,0x41,0x00,0,00000000
sdpio,0x25,0x42,0x00,0,00000000
sdpio,0x25,0x43,0x00,0,00000000
sdpio,0x25,0x44,0x00,0,00000000
sdpio,0x25,0x45,0x00,0,00000000
sdpio,0x25,0x46,0x00,0,00000000
sdpio,0x25,0x47,0x00,0,00000000
sdpio,0x25,0x48,0x00,0,00000000
sdpio,0x25,0x49,0x00,0,00000000
sdpio,0x25,0x4A,0x00,0,00000000
sdpio,0x25,0x4B,0x00,0,00000000
sdpio,0x25,0x4C,0x00,0,00000000
sdpio,0x25,0x4D,0x00,0,00000000
sdpio,0x25,0x4E,0x00,0,00000000
sdpio,0x25,0x4F,0x00,0,00000000
sdpio,0x25,0x50,0x00,0,00000000
sdpio,0x25,0x51,0x00,0,00000000
sdpio,0x25,0x52,0x14,20,00010100
sdpio,0x25,0x53,0x00,0,00000000
sdpio,0x25,0x54,0x00,0,00000000
sdpio,0x25,0x55,0x00,0,00000000
sdpio,0x25,0x56,0x00,0,00000000
sdpio,0x25,0x57,0x00,0,00000000
sdpio,0x25,0x58,0x00,0,00000000
sdpio,0x25,0x59,0x00,0,00000000
sdpio,0x25,0x5A,0x00,0,00000000
sdpio,0x25,0x5B,0x00,0,00000000
sdpio,0x25,0x5C,0x00,0,00000000
sdpio,0x25,0x5D,0x52,82,01010010
sdpio,0x25,0x5E,0x68,104,01101000
sdpio,0x25,0x5F,0x00,0,00000000
sdpio,0x25,0x60,0x00,0,00000000
sdpio,0x25,0x61,0x06,6,00000110
sdpio,0x25,0x62,0x1A,26,00011010
sdpio,0x25,0x63,0x12,18,00010010
sdpio,0x25,0x64,0x00,0,00000000
sdpio,0x25,0x65,0x00,0,00000000
sdpio,0x25,0x66,0x01,1,00000001
sdpio,0x25,0x67,0x04,4,00000100
sdpio,0x25,0x68,0x00,0,00000000
sdpio,0x25,0x69,0x00,0,00000000
sdpio,0x25,0x6A,0x00,0,00000000
sdpio,0x25,0x6B,0x00,0,00000000
sdpio,0x25,0x6C,0x4B,75,01001011
sdpio,0x25,0x6D,0x32,50,00110010
sdpio,0x25,0x6E,0x00,0,00000000
sdpio,0x25,0x6F,0x00,0,00000000
sdpio,0x25,0x70,0xA7,167,10100111
sdpio,0x25,0x71,0x3A,58,00111010
sdpio,0x25,0x72,0x06,6,00000110
sdpio,0x25,0x73,0xEF,239,11101111
sdpio,0x25,0x74,0x10,16,00010000
sdpio,0x25,0x75,0x0A,10,00001010
sdpio,0x25,0x76,0x32,50,00110010
sdpio,0x25,0x77,0x23,35,00100011
sdpio,0x25,0x78,0x00,0,00000000
sdpio,0x25,0x79,0x63,99,01100011
sdpio,0x25,0x7A,0xAA,170,10101010
sdpio,0x25,0x7B,0x4F,79,01001111
sdpio,0x25,0x7C,0x58,88,01011000
sdpio,0x25,0x7D,0xA4,164,10100100
sdpio,0x25,0x7E,0x10,16,00010000
sdpio,0x25,0x7F,0x1F,31,00011111
sdpio,0x25,0x80,0x00,0,00000000
sdpio,0x25,0x81,0x00,0,00000000
sdpio,0x25,0x82,0x00,0,00000000
sdpio,0x25,0x83,0x00,0,00000000
sdpio,0x25,0x84,0x00,0,00000000
sdpio,0x25,0x85,0x00,0,00000000
sdpio,0x25,0x86,0xAA,170,10101010
sdpio,0x25,0x87,0x00,0,00000000
sdpio,0x25,0x88,0x44,68,01000100
sdpio,0x25,0x89,0x00,0,00000000
sdpio,0x25,0x8A,0x04,4,00000100
sdpio,0x25,0x8B,0x00,0,00000000
sdpio,0x25,0x8C,0x00,0,00000000
sdpio,0x25,0x8D,0x00,0,00000000
sdpio,0x25,0x8E,0x00,0,00000000
sdpio,0x25,0x8F,0x00,0,00000000
sdpio,0x25,0x90,0x00,0,00000000
sdpio,0x25,0x91,0x00,0,00000000
sdpio,0x25,0x92,0x00,0,00000000
sdpio,0x25,0x93,0x00,0,00000000
sdpio,0x25,0x94,0x00,0,00000000
sdpio,0x25,0x95,0x00,0,00000000
sdpio,0x25,0x96,0x00,0,00000000
sdpio,0x25,0x97,0x20,32,00100000
sdpio,0x25,0x98,0x00,0,00000000
sdpio,0x25,0x99,0x00,0,00000000
sdpio,0x25,0x9A,0x00,0,00000000
sdpio,0x25,0x9B,0x00,0,00000000
sdpio,0x25,0x9C,0x00,0,00000000
sdpio,0x25,0x9D,0x00,0,00000000
sdpio,0x25,0x9E,0x00,0,00000000
sdpio,0x25,0x9F,0x00,0,00000000
sdpio,0x25,0xA0,0x04,4,00000100
sdpio,0x25,0xA1,0x04,4,00000100
sdpio,0x25,0xA2,0x04,4,00000100
sdpio,0x25,0xA3,0x04,4,00000100
sdpio,0x25,0xA4,0x04,4,00000100
sdpio,0x25,0xA5,0x04,4,00000100
sdpio,0x25,0xA6,0x04,4,00000100
sdpio,0x25,0xA7,0x04,4,00000100
sdpio,0x25,0xA8,0x04,4,00000100
sdpio,0x25,0xA9,0x04,4,00000100
sdpio,0x25,0xAA,0x04,4,00000100
sdpio,0x25,0xAB,0x04,4,00000100
sdpio,0x25,0xAC,0x04,4,00000100
sdpio,0x25,0xAD,0x04,4,00000100
sdpio,0x25,0xAE,0x04,4,00000100
sdpio,0x25,0xAF,0x04,4,00000100
sdpio,0x25,0xB0,0xC0,192,11000000
sdpio,0x25,0xB1,0x7D,125,01111101
sdpio,0x25,0xB2,0x6C,108,01101100
sdpio,0x25,0xB3,0x20,32,00100000
sdpio,0x25,0xB4,0x04,4,00000100
sdpio,0x25,0xB5,0x04,4,00000100
sdpio,0x25,0xB6,0x04,4,00000100
sdpio,0x25,0xB7,0x04,4,00000100
sdpio,0x25,0xB8,0x04,4,00000100
sdpio,0x25,0xB9,0x04,4,00000100
sdpio,0x25,0xBA,0x04,4,00000100
sdpio,0x25,0xBB,0x04,4,00000100
sdpio,0x25,0xBC,0x04,4,00000100
sdpio,0x25,0xBD,0x04,4,00000100
sdpio,0x25,0xBE,0x04,4,00000100
sdpio,0x25,0xBF,0x04,4,00000100
sdpio,0x25,0xC0,0x00,0,00000000
sdpio,0x25,0xC1,0x00,0,00000000
sdpio,0x25,0xC2,0x04,4,00000100
sdpio,0x25,0xC3,0x04,4,00000100
sdpio,0x25,0xC4,0x04,4,00000100
sdpio,0x25,0xC5,0x04,4,00000100
sdpio,0x25,0xC6,0x04,4,00000100
sdpio,0x25,0xC7,0x04,4,00000100
sdpio,0x25,0xC8,0xEB,235,11101011
sdpio,0x25,0xC9,0x6C,108,01101100
sdpio,0x25,0xCA,0x00,0,00000000
sdpio,0x25,0xCB,0x02,2,00000010
sdpio,0x25,0xCC,0x00,0,00000000
sdpio,0x25,0xCD,0x00,0,00000000
sdpio,0x25,0xCE,0xFF,255,11111111
sdpio,0x25,0xCF,0xFE,254,11111110
sdpio,0x25,0xD0,0x00,0,00000000
sdpio,0x25,0xD1,0x00,0,00000000
sdpio,0x25,0xD2,0x00,0,00000000
sdpio,0x25,0xD3,0x00,0,00000000
sdpio,0x25,0xD4,0x00,0,00000000
sdpio,0x25,0xD5,0x00,0,00000000
sdpio,0x25,0xD6,0x00,0,00000000
sdpio,0x25,0xD7,0x00,0,00000000
sdpio,0x25,0xD8,0x00,0,00000000
sdpio,0x25,0xD9,0x00,0,00000000
sdpio,0x25,0xDA,0x00,0,00000000
sdpio,0x25,0xDB,0x00,0,00000000
sdpio,0x25,0xDC,0x00,0,00000000
sdpio,0x25,0xDD,0x84,132,10000100
sdpio,0x25,0xDE,0x00,0,00000000
sdpio,0x25,0xDF,0x00,0,00000000
sdpio,0x25,0xE0,0x47,71,01000111
sdpio,0x25,0xE1,0xD2,210,11010010
sdpio,0x25,0xE2,0x00,0,00000000
sdpio,0x25,0xE3,0x00,0,00000000
sdpio,0x25,0xE4,0x00,0,00000000
sdpio,0x25,0xE5,0x40,64,01000000
sdpio,0x25,0xE6,0x7F,127,01111111
sdpio,0x25,0xE7,0x00,0,00000000
sdpio,0x25,0xE8,0x00,0,00000000
sdpio,0x25,0xE9,0x00,0,00000000
sdpio,0x25,0xEA,0x09,9,00001001
sdpio,0x25,0xEB,0x26,38,00100110
sdpio,0x25,0xEC,0x00,0,00000000
sdpio,0x25,0xED,0x00,0,00000000
sdpio,0x25,0xEE,0x00,0,00000000
sdpio,0x25,0xEF,0x00,0,00000000
sdpio,0x25,0xF0,0x00,0,00000000
sdpio,0x25,0xF1,0x00,0,00000000
sdpio,0x25,0xF2,0x00,0,00000000
sdpio,0x25,0xF3,0x00,0,00000000
sdpio,0x25,0xF4,0x06,6,00000110
sdpio,0x25,0xF5,0x81,129,10000001
sdpio,0x25,0xF6,0x00,0,00000000
sdpio,0x25,0xF7,0x00,0,00000000
sdpio,0x25,0xF8,0x00,0,00000000
sdpio,0x25,0xF9,0x00,0,00000000
sdpio,0x25,0xFA,0x00,0,00000000
sdpio,0x25,0xFB,0x00,0,00000000
sdpio,0x25,0xFC,0x00,0,00000000
sdpio,0x25,0xFD,0x00,0,00000000
sdpio,0x25,0xFE,0x00,0,00000000
sdpio,0x25,0xFF,0x00,0,00000000

Edit Notes

Changed title / tags
[edited by: superchromat at 3:32 AM (GMT -4) on 6 Jun 2026]
  • Oh - I should also note that the noise is uncorrelated between the channels. 

  • Unsure if this help, but here is a photo of one of the chips I’m seeing this issue with. 

  • Hi,

       Could you please evaluate the same format in our EVAL-ADV7842 evaluation board and let us know ?

       Kindly note that, as per the ADV7842 specifications, the component interface supports 1080p24 with a pixel clock of 74.25 MHz.

    Thanks,

    Poornima S

  • We don't own the eval board, but can purchase one, but I'm not sure what more information that would provide given that we do have a commercial device using an ADV7842 in the same role as an analog component capture device and it performs with lower noise. We have analyzed its analog front end and it isn't doing anything particularly special. 

    I'm not sure if I follow your note regarding 1080p24, as that is the format we are using.

  • I also note that the commercial device that I'm comparing it to appears to be using an older ADV7842 manufactured in 2011 in Singapore, versus the 2025 Korea chips that our supplier provided. Is it possibly due to different dies / manufacturing processes?

  • Hi,

      We have validated the 1080p24 format on our evaluation board and did not observe any issues. Please find the register dump below and compare it with your current settings to identify any differences.

    ; Register dump
    ; Device ADV7842
    ; AVES3
    ; 11-06-2026 16:09:20
    ; 
    ; IO
    40 00 1E
    40 01 C1
    40 02 F4
    40 03 82
    40 04 62
    40 05 28
    40 06 A7
    40 07 55
    40 08 14
    40 0B 44
    40 0C 42
    40 12 C0 ; read only
    40 13 C3 ; read only
    40 14 6A
    40 15 A0
    40 16 43
    40 17 5A
    40 19 85
    40 1A 02
    40 20 F0
    40 21 0F ; read only
    40 30 88
    40 33 43
    40 3F 02 ; read only
    40 40 E1
    40 41 FD
    40 42 94 ; read only
    40 43 00 ; read only
    40 44 00
    40 45 00
    40 46 50
    40 47 00 ; read only
    40 48 00 ; read only
    40 49 00
    40 4A 00
    40 4B 60
    40 4C 00 ; read only
    40 4D 00 ; read only
    40 4E 00
    40 4F 00
    40 50 00
    40 51 00 ; read only
    40 52 00 ; read only
    40 53 00
    40 54 00
    40 55 00
    40 56 85 ; read only
    40 57 00 ; read only
    40 58 00
    40 59 00
    40 5A 00
    40 5B 5B ; read only
    40 5C 0C ; read only
    40 5D 00
    40 5E 00
    40 5F 0C
    40 60 00 ; read only
    40 61 00 ; read only
    40 62 00
    40 63 00
    40 64 FF
    40 65 40 ; read only
    40 66 00 ; read only
    40 67 00
    40 68 00
    40 69 F9
    40 6A 00 ; read only
    40 6B 00 ; read only
    40 6C 00
    40 6D 00
    40 6E 33
    40 6F 00 ; read only
    40 70 00 ; read only
    40 71 00
    40 72 00
    40 73 33
    40 74 00 ; read only
    40 75 00 ; read only
    40 76 00
    40 77 00
    40 78 03
    40 79 00 ; read only
    40 7A 00 ; read only
    40 7B 00
    40 7C 00
    40 7D FF
    40 7E 00 ; read only
    40 7F 00 ; read only
    40 80 00
    40 81 00
    40 82 E9
    40 83 40 ; read only
    40 84 00 ; read only
    40 85 00
    40 86 00
    40 87 A9
    40 88 00 ; read only
    40 89 00 ; read only
    40 8A 00
    40 8B 00
    40 8C 03
    40 8D 00 ; read only
    40 8E 00 ; read only
    40 8F 00
    40 90 00
    40 91 00
    40 92 00 ; read only
    40 93 00 ; read only
    40 94 00
    40 95 00
    40 96 0F
    40 97 00 ; read only
    40 98 00 ; read only
    40 99 00
    40 9A 00
    40 9B 00
    40 9C 04 ; read only
    40 9D 00 ; read only
    40 9E 00
    40 9F 00
    40 A0 00
    40 D6 00
    40 D7 00
    40 D8 2D
    40 D9 15
    40 DA F1
    40 DB 5F
    40 DC 40
    40 DD 00
    40 E0 00
    40 E7 00
    40 EA 20 ; read only
    40 EB 12 ; read only
    40 F1 90
    40 F2 94
    40 F3 84
    40 F4 80
    40 F5 7C
    40 F8 4C
    40 F9 64
    40 FA 6C
    40 FB 68
    40 FD 44
    40 FE 48
    40 FF 00
    ; 
    ; CP
    44 0B 40 ; read only
    44 0C 00 ; read only
    44 0D 00 ; read only
    44 0E 00 ; read only
    44 0F 00 ; read only
    44 10 08 ; read only
    44 11 00 ; read only
    44 12 00 ; read only
    44 13 00 ; read only
    44 14 00 ; read only
    44 15 01 ; read only
    44 16 00 ; read only
    44 17 00 ; read only
    44 18 00 ; read only
    44 19 00 ; read only
    44 1A 00 ; read only
    44 1B 20 ; read only
    44 1C 00 ; read only
    44 1D 00 ; read only
    44 1E 00 ; read only
    44 1F 00 ; read only
    44 22 00
    44 23 00
    44 24 00
    44 25 00
    44 26 00
    44 27 00
    44 28 00
    44 29 00
    44 2A 00
    44 2B 00
    44 2C 00
    44 2D 00
    44 2E 00
    44 2F 00
    44 30 00
    44 31 00
    44 36 00
    44 3A 80
    44 3B 80
    44 3C 00
    44 3D 00
    44 3E 04
    44 40 5C
    44 41 02
    44 42 3B
    44 43 D4
    44 46 00
    44 47 00
    44 48 00
    44 49 3F ; read only
    44 4A FF ; read only
    44 4B 00 ; read only
    44 4C 00 ; read only
    44 4D 0F ; read only
    44 4E 65 ; read only
    44 4F 83 ; read only
    44 52 40
    44 53 00
    44 54 00
    44 55 00
    44 56 00
    44 57 08
    44 58 00
    44 59 00
    44 5A 00
    44 5B 00
    44 5C 01
    44 5D 00
    44 5E 00
    44 5F 00
    44 60 00
    44 61 00
    44 62 20
    44 63 00
    44 64 00
    44 65 00
    44 66 00
    44 67 00
    44 68 F7
    44 69 14
    44 6C 10
    44 6D 00
    44 6E 00
    44 6F 00
    44 70 00
    44 71 00
    44 72 00
    44 73 E9
    44 74 3A
    44 75 4E
    44 76 93
    44 77 FF
    44 78 FF
    44 79 FF
    44 7A FF
    44 7B 05
    44 7C C0
    44 7D 00
    44 7E 00
    44 7F 00
    44 80 00
    44 81 C0
    44 82 04
    44 83 00
    44 84 0C
    44 85 1B
    44 86 0B
    44 88 00
    44 89 00
    44 8A 20
    44 8B 40
    44 8C 00
    44 8D 00
    44 8E 00
    44 8F 40
    44 90 00
    44 91 40
    44 9A 00
    44 9B 00
    44 9C 00
    44 9D 00
    44 9E 00
    44 9F 00
    44 A0 00
    44 A1 00
    44 A5 00
    44 A6 00
    44 A7 00
    44 A8 00
    44 A9 00
    44 AA 00
    44 AB 00
    44 AC 00
    44 B1 A1 ; read only
    44 B2 1C ; read only
    44 B3 2C ; read only
    44 B4 64 ; read only
    44 B5 83 ; read only
    44 B6 00 ; read only
    44 B7 00 ; read only
    44 B8 12 ; read only
    44 B9 34 ; read only
    44 BA 01
    44 BD 18
    44 BE 00
    44 BF 16
    44 C0 00
    44 C1 00
    44 C2 00
    44 C5 91
    44 C6 00
    44 C7 00
    44 C8 00
    44 C9 2D
    44 CA 00
    44 CB 60
    44 DA 00
    44 DB 19
    44 DC 64
    44 DD 12
    44 DE C5
    44 DF 78
    44 E0 D3 ; read only
    44 E1 FF ; read only
    44 E2 2C ; read only
    44 E3 0C ; read only
    44 E4 3D ; read only
    44 E5 3C ; read only
    44 E6 FF ; read only
    44 E7 02 ; read only
    44 E8 FD ; read only
    44 E9 03 ; read only
    44 EA 01 ; read only
    44 EB 0A ; read only
    44 EC 7C ; read only
    44 ED 10 ; read only
    44 EE A4 ; read only
    44 EF 04 ; read only
    44 F0 04 ; read only
    44 F2 04
    44 F3 D4
    44 F4 00 ; read only
    44 F5 00
    44 FF 08 ; read only
    ; 
    ; VDP
    48 3C 00 ; read only
    48 3D 00 ; read only
    48 3E 00 ; read only
    48 3F 00 ; read only
    48 40 00 ; read only
    48 41 00 ; read only
    48 42 00 ; read only
    48 43 00 ; read only
    48 44 00 ; read only
    48 45 00 ; read only
    48 47 00 ; read only
    48 48 00 ; read only
    48 49 00 ; read only
    48 4A 00 ; read only
    48 4B 00 ; read only
    48 4C 00 ; read only
    48 4D 00 ; read only
    48 4E 00 ; read only
    48 4F 00 ; read only
    48 50 00 ; read only
    48 51 00 ; read only
    48 52 00 ; read only
    48 53 00 ; read only
    48 55 00 ; read only
    48 56 00 ; read only
    48 57 00 ; read only
    48 58 00 ; read only
    48 59 00 ; read only
    48 5A 00 ; read only
    48 5B 00 ; read only
    48 5C 00 ; read only
    48 5D 00 ; read only
    48 5E 00 ; read only
    48 60 08
    48 61 18
    48 62 15
    48 63 2A
    48 64 00
    48 65 00
    48 66 00
    48 67 00
    48 68 00
    48 69 00
    48 6A 00
    48 6B 00
    48 6C 00
    48 6D 00
    48 6E 00
    48 6F 00
    48 70 00
    48 71 00
    48 72 00
    48 73 00
    48 74 00
    48 75 00
    48 76 00
    48 77 00
    48 78 00
    48 98 88
    48 99 DD
    48 9C 20
    48 9D 02
    48 9E 00
    48 A5 90
    48 A6 00
    48 A8 08
    48 AC C8
    48 C0 00
    48 C2 00 ; read only
    48 C3 00 ; read only
    48 C4 00 ; read only
    48 C5 00 ; read only
    48 C6 00 ; read only
    48 C7 00 ; read only
    48 C8 00 ; read only
    48 C9 00 ; read only
    48 CA 00 ; read only
    48 CB 00 ; read only
    48 CC 00 ; read only
    48 CD 00 ; read only
    48 CE 00 ; read only
    48 CF 00 ; read only
    48 D0 00 ; read only
    48 D1 00 ; read only
    48 D2 00 ; read only
    48 D3 00 ; read only
    48 D4 00 ; read only
    48 D5 00 ; read only
    48 D6 00 ; read only
    48 D7 00 ; read only
    48 D8 00 ; read only
    48 D9 00 ; read only
    48 DA 00 ; read only
    48 DB 00 ; read only
    48 DC 00 ; read only
    48 DD 00 ; read only
    48 DE 00 ; read only
    48 DF 00 ; read only
    48 E0 00 ; read only
    48 E1 00 ; read only
    48 E2 00 ; read only
    48 E3 00 ; read only
    48 E4 00 ; read only
    48 E5 00 ; read only
    48 E6 00 ; read only
    48 E7 00 ; read only
    48 E8 00 ; read only
    48 E9 00 ; read only
    48 EA 00 ; read only
    48 EB 00 ; read only
    48 EC 00 ; read only
    48 ED 00 ; read only
    48 EE 00 ; read only
    48 EF 00 ; read only
    48 F0 00 ; read only
    ; 
    ; AFE
    4C 00 08
    4C 02 C0
    4C 03 45
    4C 04 60
    4C 05 0F
    4C 06 00
    4C 07 5F
    4C 14 00
    4C 15 4A
    4C 16 98
    4C 17 00
    4C 18 00
    4C 19 00
    4C 1A 00
    4C 1B 00 ; read only
    4C 1C 00 ; read only
    4C 1D 6D
    4C 1E 6D
    4C 1F 6D
    4C 20 6D
    4C 21 6D
    4C 22 6D
    4C 23 6D
    4C 24 6D
    4C 27 FF ; read only
    4C 28 FF ; read only
    ; 
    ; SDP
    90 00 02
    90 01 36
    90 02 27
    90 03 C4
    90 04 0B
    90 05 C3
    90 06 C0
    90 07 8B
    90 08 1A
    90 0A E5
    90 0B E5
    90 0C E5
    90 0D E4
    90 0E 31
    90 0F 00
    90 10 01
    90 11 10
    90 12 01
    90 13 80
    90 14 00
    90 15 80
    90 16 00
    90 17 00
    90 18 FF
    90 19 CD
    90 1A 95
    90 1B 1E
    90 1C C4
    90 1D 02
    90 1E 04
    90 1F 12
    90 20 00
    90 21 FF
    90 22 20
    90 23 10
    90 24 4C
    90 25 00
    90 26 8F
    90 27 AA
    90 28 02
    90 2A 00
    90 34 A0
    90 4C 00 ; read only
    90 4D 00 ; read only
    90 4E 00 ; read only
    90 4F 00 ; read only
    90 50 00 ; read only
    90 51 00 ; read only
    90 52 00 ; read only
    90 53 00 ; read only
    90 54 04 ; read only
    90 55 00 ; read only
    90 56 78 ; read only
    90 57 18 ; read only
    90 58 00 ; read only
    90 59 04 ; read only
    90 5A 40 ; read only
    90 7B 69
    90 89 03
    90 98 BF
    90 99 10
    90 9A 01
    90 A1 50
    90 A2 A0
    90 A3 BE
    90 A4 BF
    90 A5 BF
    90 A8 40
    90 A9 88
    90 AA 88
    90 D9 44
    90 DB 88
    90 DC 02
    90 DD BC
    90 DE 23
    90 DF 7D
    ; 
    ; CEC
    80 00 5F
    80 01 84
    80 02 10
    80 03 00
    80 04 05
    80 05 00
    80 06 00
    80 07 00
    80 08 00
    80 09 00
    80 0A 00
    80 0B 00
    80 0C 00
    80 0D 00
    80 0E 00
    80 0F 00
    80 10 05
    80 11 01
    80 12 33
    80 13 57
    80 14 00 ; read only
    80 15 00 ; read only
    80 16 00 ; read only
    80 17 00 ; read only
    80 18 00 ; read only
    80 19 00 ; read only
    80 1A 00 ; read only
    80 1B 00 ; read only
    80 1C 00 ; read only
    80 1D 00 ; read only
    80 1E 00 ; read only
    80 1F 00 ; read only
    80 20 00 ; read only
    80 21 00 ; read only
    80 22 00 ; read only
    80 23 00 ; read only
    80 24 00 ; read only
    80 25 00 ; read only
    80 27 10
    80 28 05
    80 29 00
    80 2A 3D
    80 2B 07
    80 2C 00
    80 4C 00
    80 53 00 ; read only
    80 54 00 ; read only
    80 55 00 ; read only
    80 56 00 ; read only
    80 57 00 ; read only
    80 58 00 ; read only
    80 59 00 ; read only
    80 5A 00 ; read only
    80 5B 00 ; read only
    80 5C 00 ; read only
    80 5D 00 ; read only
    80 5E 00 ; read only
    80 5F 00 ; read only
    80 60 00 ; read only
    80 61 00 ; read only
    80 62 00 ; read only
    80 63 00 ; read only
    80 64 00 ; read only
    80 65 00 ; read only
    80 66 00 ; read only
    80 67 00 ; read only
    80 68 00 ; read only
    80 69 00 ; read only
    80 6A 00 ; read only
    80 6B 00 ; read only
    80 6C 00 ; read only
    80 6D 00 ; read only
    80 6E 00 ; read only
    80 6F 00 ; read only
    80 70 00 ; read only
    80 71 00 ; read only
    80 72 00 ; read only
    80 73 00 ; read only
    80 74 00 ; read only
    80 75 00 ; read only
    80 76 00 ; read only
    80 77 00
    80 78 6D
    80 79 8F
    80 7A 82
    80 7B 04
    80 7C 0D
    80 7D 70
    80 7E 42
    80 7F 41
    ; 
    ; AVLINK
    84 00 00
    84 01 00
    84 02 00
    84 03 00
    84 04 00
    84 05 00
    84 06 00
    84 07 00
    84 08 00
    84 09 00
    84 0A 00
    84 0B 00
    84 0C 00
    84 0D 00
    84 0E 00
    84 0F 00
    84 10 00
    84 11 1C
    84 12 75
    84 13 09
    84 14 00 ; read only
    84 15 03 ; read only
    84 16 00 ; read only
    84 17 00 ; read only
    84 18 00 ; read only
    84 19 00 ; read only
    84 1A 00 ; read only
    84 1B 00 ; read only
    84 1C 00 ; read only
    84 1D 00 ; read only
    84 1E 00 ; read only
    84 1F 00 ; read only
    84 20 00 ; read only
    84 21 00 ; read only
    84 22 00 ; read only
    84 23 00 ; read only
    84 24 00 ; read only
    84 25 00
    84 26 10
    84 27 00
    84 28 07
    84 29 00
    84 2A FF
    84 2B 0F
    84 2C 0F
    84 2D BB
    84 2E 0E
    84 2F DB
    84 30 10
    84 31 9B
    84 32 0C
    84 33 EF
    84 34 0C
    84 35 0F
    84 36 0D
    84 37 CF
    84 38 08
    84 39 64
    84 3A 06
    84 3B FE
    84 3C 09
    84 3D CA
    84 3E 02
    84 3F 19
    84 40 01
    84 41 39
    84 42 02
    84 43 F9
    84 44 05
    84 45 3E
    84 46 05
    84 47 F1
    84 48 04
    84 49 8B
    84 4A 03
    84 4B AC
    84 4C 0C
    84 4D 96
    84 4E 00
    84 4F 70
    84 50 00
    84 51 00
    84 52 00
    84 53 00
    84 54 00
    84 55 3F
    84 56 00 ; read only
    84 58 7C
    ; 
    ; SDP_IO
    94 29 00
    94 51 00
    94 60 00
    94 66 01
    94 67 04
    94 6F 00
    94 8C 00
    94 8D 00
    94 8E 00
    94 8F 00
    94 90 00
    94 91 00
    94 92 00
    94 93 00
    94 94 00
    94 95 00
    94 96 00
    94 97 20
    94 98 00
    94 99 00
    94 9A 00
    94 9B 00
    94 9C 00
    94 9D 00
    94 9E 00
    94 9F 00
    94 A0 04
    94 A1 04
    94 A2 04
    94 A3 04
    94 A4 04
    94 A5 04
    94 A6 04
    94 A7 04
    94 A8 04
    94 A9 04
    94 AA 04
    94 AB 04
    94 AC 04
    94 AD 04
    94 AE 04
    94 AF 04
    94 B0 C0
    94 B1 7D
    94 B2 6C
    94 B3 20
    94 B4 04
    94 B5 04
    94 B6 04
    94 B7 04
    94 B8 04
    94 B9 04
    94 C2 04
    94 C3 04
    94 C4 04
    94 C5 04
    94 C6 04
    94 C7 04
    94 C8 EB
    94 C9 6C
    94 E0 47
    94 E1 D2
    94 E2 00
    94 E3 00
    94 E4 00
    94 E5 40
    94 E6 7F
    94 E7 00
    94 E8 00
    94 E9 00
    94 EA 09
    94 EB 26
    94 EC 00
    94 ED 00
    94 EE 00
    94 EF 00
    94 F0 00
    94 F1 00
    94 F2 00
    94 F3 00
    94 F4 06
    94 F5 81
    94 F6 00
    94 F7 00
    ; 
    ; HDMI
    68 00 32
    68 01 18
    68 02 00
    68 03 18
    68 04 20 ; read only
    68 05 00 ; read only
    68 07 00 ; read only
    68 08 00 ; read only
    68 09 00 ; read only
    68 0A 00 ; read only
    68 0B 00 ; read only
    68 0C 00 ; read only
    68 0D 34
    68 0F 1F
    68 10 25
    68 11 7D
    68 12 02
    68 13 7F
    68 14 1D
    68 15 FF
    68 16 FF
    68 18 00 ; read only
    68 19 00 ; read only
    68 1A 4C
    68 1B 18
    68 1C 00 ; read only
    68 1D 00
    68 1E 00 ; read only
    68 1F 01 ; read only
    68 20 00 ; read only
    68 21 00 ; read only
    68 22 00 ; read only
    68 23 01 ; read only
    68 24 00 ; read only
    68 25 00 ; read only
    68 26 00 ; read only
    68 27 02 ; read only
    68 28 00 ; read only
    68 29 02 ; read only
    68 2A 00 ; read only
    68 2B 02 ; read only
    68 2C 00 ; read only
    68 2D 02 ; read only
    68 2E 00 ; read only
    68 2F 02 ; read only
    68 30 00 ; read only
    68 31 02 ; read only
    68 32 3F ; read only
    68 33 FE ; read only
    68 34 3F ; read only
    68 35 FE ; read only
    68 36 00 ; read only
    68 37 00 ; read only
    68 38 00 ; read only
    68 39 00 ; read only
    68 3A 00 ; read only
    68 40 00
    68 41 40
    68 47 06
    68 48 06
    68 50 04
    68 51 00 ; read only
    68 52 00 ; read only
    68 53 00 ; read only
    68 56 58
    68 5A 00
    68 5B 00 ; read only
    68 5C 00 ; read only
    68 5D 00 ; read only
    68 5E 00 ; read only
    68 5F 00 ; read only
    68 69 A3
    68 6A 00
    68 6B 04
    68 72 04
    68 73 00
    68 8C A3
    68 8D 04
    68 8E 1E
    68 90 04
    68 91 1E
    68 93 04
    68 94 1E
    68 96 00
    68 E0 00 ; read only
    68 E1 00 ; read only
    68 E2 00 ; read only
    68 E3 00 ; read only
    68 E4 00 ; read only
    68 E5 01 ; read only
    68 E6 00 ; read only
    68 E7 00 ; read only
    68 E8 00 ; read only
    68 E9 01 ; read only
    68 EA 00 ; read only
    68 EB 00 ; read only
    ; 
    ; Repeater
    64 00 7C ; read only
    64 01 A8 ; read only
    64 02 07 ; read only
    64 03 DB ; read only
    64 04 8A ; read only
    64 08 00 ; read only
    64 09 00 ; read only
    64 0A 00 ; read only
    64 10 00
    64 11 00
    64 12 00
    64 13 00
    64 14 00
    64 15 00
    64 18 00
    64 19 00
    64 1A 00
    64 1B 00
    64 1C 00
    64 1D 00
    64 1E 00
    64 1F 00
    64 20 00
    64 21 00
    64 22 00
    64 23 00
    64 24 00
    64 25 00
    64 26 00
    64 27 00
    64 28 00
    64 29 00
    64 2A 00
    64 2B 00
    64 2C 00
    64 2D 00
    64 2E 00
    64 2F 00
    64 30 00
    64 31 00
    64 32 00
    64 33 00
    64 40 80
    64 41 00
    64 42 00
    64 72 11
    64 73 00
    64 74 12
    64 75 00
    64 76 9E
    64 77 0C
    64 78 01
    64 79 20 ; read only
    64 7B B0
    64 7C AF
    64 7D 0C ; read only
    64 7E 00
    64 7F 82
    64 80 00
    64 81 00
    64 82 00
    64 83 00
    64 84 00
    64 85 00
    64 86 00
    64 87 00
    64 88 00
    64 89 00
    64 8A 00
    64 8B 00
    64 8C 00
    64 8D 00
    64 8E 00
    64 8F 00
    64 90 00
    64 91 00
    64 92 00
    64 93 00
    64 94 00
    64 95 00
    64 96 00
    64 97 00
    64 98 00
    64 99 00
    64 9A 00
    64 9B 00
    64 9C 00
    64 9D 00
    64 9E 00
    64 9F 00
    64 A0 00
    64 A1 00
    64 A2 00
    64 A3 00
    64 A4 00
    64 A5 00
    64 A6 00
    64 A7 00
    64 A8 00
    64 A9 00
    64 AA 00
    64 AB 00
    64 AC 00
    64 AD 00
    64 AE 00
    64 AF 00
    64 B0 00
    64 B1 00
    64 B2 00
    64 B3 00
    64 B4 00
    64 B5 00
    64 B6 00
    64 B7 00
    64 B8 00
    64 B9 00
    64 BA 00
    64 BB 00
    64 BC 00
    64 BD 00
    64 BE 00
    64 BF 00
    64 C0 00
    64 C1 00
    64 C2 00
    64 C3 00
    64 C4 00
    64 C5 00
    64 C6 00
    64 C7 00
    64 C8 00
    64 C9 00
    64 CA 00
    64 CB 00
    64 CC 00
    64 CD 00
    64 CE 00
    64 CF 00
    64 D0 00
    64 D1 00
    64 D2 00
    64 D3 00
    64 D4 00
    64 D5 00
    64 D6 00
    64 D7 00
    64 D8 00
    64 D9 00
    64 DA 00
    64 DB 00
    64 DC 00
    64 DD 00
    64 DE 00
    64 DF 00
    64 E0 00
    64 E1 00
    64 E2 00
    64 E3 00
    64 E4 00
    64 E5 00
    64 E6 00
    64 E7 00
    64 E8 00
    64 E9 00
    64 EA 00
    64 EB 00
    64 EC 00
    64 ED 00
    64 EE 00
    64 EF 00
    64 F0 00
    64 F1 00
    64 F2 00
    64 F3 00
    64 F4 00
    64 F5 00
    64 F6 00
    64 F7 00
    ; 
    ; InfoFrame
    7C 00 00 ; read only
    7C 01 00 ; read only
    7C 02 00 ; read only
    7C 03 00 ; read only
    7C 04 00 ; read only
    7C 05 00 ; read only
    7C 06 00 ; read only
    7C 07 00 ; read only
    7C 08 00 ; read only
    7C 09 00 ; read only
    7C 0A 00 ; read only
    7C 0B 00 ; read only
    7C 0C 00 ; read only
    7C 0D 00 ; read only
    7C 0E 00 ; read only
    7C 0F 00 ; read only
    7C 10 00 ; read only
    7C 11 00 ; read only
    7C 12 00 ; read only
    7C 13 00 ; read only
    7C 14 00 ; read only
    7C 15 00 ; read only
    7C 16 00 ; read only
    7C 17 00 ; read only
    7C 18 00 ; read only
    7C 19 00 ; read only
    7C 1A 00 ; read only
    7C 1B 00 ; read only
    7C 1C 00 ; read only
    7C 1D 00 ; read only
    7C 1E 00 ; read only
    7C 1F 00 ; read only
    7C 20 00 ; read only
    7C 21 00 ; read only
    7C 22 00 ; read only
    7C 23 00 ; read only
    7C 24 00 ; read only
    7C 25 00 ; read only
    7C 26 00 ; read only
    7C 27 00 ; read only
    7C 28 00 ; read only
    7C 29 00 ; read only
    7C 2A 00 ; read only
    7C 2B 00 ; read only
    7C 2C 00 ; read only
    7C 2D 00 ; read only
    7C 2E 00 ; read only
    7C 2F 00 ; read only
    7C 30 00 ; read only
    7C 31 00 ; read only
    7C 32 00 ; read only
    7C 33 00 ; read only
    7C 34 00 ; read only
    7C 35 00 ; read only
    7C 36 00 ; read only
    7C 37 00 ; read only
    7C 38 00 ; read only
    7C 39 00 ; read only
    7C 3A 00 ; read only
    7C 3B 00 ; read only
    7C 3C 00 ; read only
    7C 3D 00 ; read only
    7C 3E 00 ; read only
    7C 3F 00 ; read only
    7C 40 00 ; read only
    7C 41 00 ; read only
    7C 42 00 ; read only
    7C 43 00 ; read only
    7C 44 00 ; read only
    7C 45 00 ; read only
    7C 46 00 ; read only
    7C 47 00 ; read only
    7C 48 00 ; read only
    7C 49 00 ; read only
    7C 4A 00 ; read only
    7C 4B 00 ; read only
    7C 4C 00 ; read only
    7C 4D 00 ; read only
    7C 4E 00 ; read only
    7C 4F 00 ; read only
    7C 50 00 ; read only
    7C 51 00 ; read only
    7C 52 00 ; read only
    7C 53 00 ; read only
    7C 54 00 ; read only
    7C 55 00 ; read only
    7C 56 00 ; read only
    7C 57 00 ; read only
    7C 58 00 ; read only
    7C 59 00 ; read only
    7C 5A 00 ; read only
    7C 5B 00 ; read only
    7C 5C 00 ; read only
    7C 5D 00 ; read only
    7C 5E 00 ; read only
    7C 5F 00 ; read only
    7C 60 00 ; read only
    7C 61 00 ; read only
    7C 62 00 ; read only
    7C 63 00 ; read only
    7C 64 00 ; read only
    7C 65 00 ; read only
    7C 66 00 ; read only
    7C 67 00 ; read only
    7C 68 00 ; read only
    7C 69 00 ; read only
    7C 6A 00 ; read only
    7C 6B 00 ; read only
    7C 6C 00 ; read only
    7C 6D 00 ; read only
    7C 6E 00 ; read only
    7C 6F 00 ; read only
    7C 70 00 ; read only
    7C 71 00 ; read only
    7C 72 00 ; read only
    7C 73 00 ; read only
    7C 74 00 ; read only
    7C 75 00 ; read only
    7C 76 00 ; read only
    7C 77 00 ; read only
    7C 78 00 ; read only
    7C 79 00 ; read only
    7C 7A 00 ; read only
    7C 7B 00 ; read only
    7C 7C 00 ; read only
    7C 7D 00 ; read only
    7C 7E 00 ; read only
    7C 7F 00 ; read only
    7C 80 00 ; read only
    7C 81 00 ; read only
    7C 82 00 ; read only
    7C 83 00 ; read only
    7C 84 00 ; read only
    7C 85 00 ; read only
    7C 86 00 ; read only
    7C 87 00 ; read only
    7C 88 00 ; read only
    7C 89 00 ; read only
    7C 8A 00 ; read only
    7C 8B 00 ; read only
    7C 8C 00 ; read only
    7C 8D 00 ; read only
    7C 8E 00 ; read only
    7C 8F 00 ; read only
    7C 90 00 ; read only
    7C 91 00 ; read only
    7C 92 00 ; read only
    7C 93 00 ; read only
    7C 94 00 ; read only
    7C 95 00 ; read only
    7C 96 00 ; read only
    7C 97 00 ; read only
    7C 98 00 ; read only
    7C 99 00 ; read only
    7C 9A 00 ; read only
    7C 9B 00 ; read only
    7C 9C 00 ; read only
    7C 9D 00 ; read only
    7C 9E 00 ; read only
    7C 9F 00 ; read only
    7C A0 00 ; read only
    7C A1 00 ; read only
    7C A2 00 ; read only
    7C A3 00 ; read only
    7C A4 00 ; read only
    7C A5 00 ; read only
    7C A6 00 ; read only
    7C A7 00 ; read only
    7C A8 00 ; read only
    7C A9 00 ; read only
    7C AA 00 ; read only
    7C AB 00 ; read only
    7C AC 00 ; read only
    7C AD 00 ; read only
    7C AE 00 ; read only
    7C AF 00 ; read only
    7C B0 00 ; read only
    7C B1 00 ; read only
    7C B2 00 ; read only
    7C B3 00 ; read only
    7C B4 00 ; read only
    7C B5 00 ; read only
    7C B6 00 ; read only
    7C B7 00 ; read only
    7C B8 00 ; read only
    7C B9 00 ; read only
    7C BA 00 ; read only
    7C BB 00 ; read only
    7C BC 00 ; read only
    7C BD 00 ; read only
    7C BE 00 ; read only
    7C BF 00 ; read only
    7C C0 00 ; read only
    7C C1 00 ; read only
    7C C2 00 ; read only
    7C C3 00 ; read only
    7C C4 00 ; read only
    7C C5 00 ; read only
    7C C6 00 ; read only
    7C C7 00 ; read only
    7C C8 00 ; read only
    7C C9 00 ; read only
    7C CA 00 ; read only
    7C CB 00 ; read only
    7C CC 00 ; read only
    7C CD 00 ; read only
    7C CE 00 ; read only
    7C CF 00 ; read only
    7C D0 00 ; read only
    7C D1 00 ; read only
    7C D2 00 ; read only
    7C D3 00 ; read only
    7C D4 00 ; read only
    7C D5 00 ; read only
    7C D6 00 ; read only
    7C D7 00 ; read only
    7C D8 00 ; read only
    7C D9 00 ; read only
    7C DA 00 ; read only
    7C DB 00 ; read only
    7C DC 00 ; read only
    7C DD 00 ; read only
    7C DE 00 ; read only
    7C DF 00 ; read only
    7C E0 82
    7C E1 00 ; read only
    7C E2 00 ; read only
    7C E3 84
    7C E4 00 ; read only
    7C E5 00 ; read only
    7C E6 83
    7C E7 00 ; read only
    7C E8 00 ; read only
    7C E9 85
    7C EA 00 ; read only
    7C EB 00 ; read only
    7C EC 81
    7C ED 00 ; read only
    7C EE 00 ; read only
    7C EF 04
    7C F0 00 ; read only
    7C F1 00 ; read only
    7C F2 05
    7C F3 00 ; read only
    7C F4 00 ; read only
    7C F5 06
    7C F6 00 ; read only
    7C F7 00 ; read only
    7C F8 0A
    7C F9 00 ; read only
    7C FA 00 ; read only
    ; 
    ; DPLL
    4C A0 00
    4C B5 01
    4C C8 00
    4C C9 00
    ; 
    ; EDID
    6C 00 00 ; read only
    6C 01 FF ; read only
    6C 02 FF ; read only
    6C 03 FF ; read only
    6C 04 FF ; read only
    6C 05 FF ; read only
    6C 06 FF ; read only
    6C 07 00 ; read only
    6C 08 1E ; read only
    6C 09 6D ; read only
    6C 0A 01 ; read only
    6C 0B 00 ; read only
    6C 0C 01 ; read only
    6C 0D 01 ; read only
    6C 0E 01 ; read only
    6C 0F 01 ; read only
    6C 10 01 ; read only
    6C 11 15 ; read only
    6C 12 01 ; read only
    6C 13 03 ; read only
    6C 14 80 ; read only
    6C 15 10 ; read only
    6C 16 09 ; read only
    6C 17 78 ; read only
    6C 18 0A ; read only
    6C 19 EE ; read only
    6C 1A 91 ; read only
    6C 1B A3 ; read only
    6C 1C 54 ; read only
    6C 1D 4C ; read only
    6C 1E 99 ; read only
    6C 1F 26 ; read only
    6C 20 0F ; read only
    6C 21 50 ; read only
    6C 22 54 ; read only
    6C 23 A1 ; read only
    6C 24 08 ; read only
    6C 25 00 ; read only
    6C 26 71 ; read only
    6C 27 4F ; read only
    6C 28 81 ; read only
    6C 29 80 ; read only
    6C 2A 01 ; read only
    6C 2B 01 ; read only
    6C 2C 01 ; read only
    6C 2D 01 ; read only
    6C 2E 01 ; read only
    6C 2F 01 ; read only
    6C 30 01 ; read only
    6C 31 01 ; read only
    6C 32 01 ; read only
    6C 33 01 ; read only
    6C 34 01 ; read only
    6C 35 01 ; read only
    6C 36 02 ; read only
    6C 37 3A ; read only
    6C 38 80 ; read only
    6C 39 18 ; read only
    6C 3A 71 ; read only
    6C 3B 38 ; read only
    6C 3C 2D ; read only
    6C 3D 40 ; read only
    6C 3E 58 ; read only
    6C 3F 2C ; read only
    6C 40 45 ; read only
    6C 41 00 ; read only
    6C 42 A0 ; read only
    6C 43 5A ; read only
    6C 44 00 ; read only
    6C 45 00 ; read only
    6C 46 00 ; read only
    6C 47 1E ; read only
    6C 48 1B ; read only
    6C 49 21 ; read only
    6C 4A 50 ; read only
    6C 4B A0 ; read only
    6C 4C 51 ; read only
    6C 4D 00 ; read only
    6C 4E 1E ; read only
    6C 4F 30 ; read only
    6C 50 48 ; read only
    6C 51 88 ; read only
    6C 52 35 ; read only
    6C 53 00 ; read only
    6C 54 A0 ; read only
    6C 55 5A ; read only
    6C 56 00 ; read only
    6C 57 00 ; read only
    6C 58 00 ; read only
    6C 59 1C ; read only
    6C 5A 00 ; read only
    6C 5B 00 ; read only
    6C 5C 00 ; read only
    6C 5D FD ; read only
    6C 5E 00 ; read only
    6C 5F 3A ; read only
    6C 60 3E ; read only
    6C 61 1E ; read only
    6C 62 53 ; read only
    6C 63 10 ; read only
    6C 64 00 ; read only
    6C 65 0A ; read only
    6C 66 20 ; read only
    6C 67 20 ; read only
    6C 68 20 ; read only
    6C 69 20 ; read only
    6C 6A 20 ; read only
    6C 6B 20 ; read only
    6C 6C 00 ; read only
    6C 6D 00 ; read only
    6C 6E 00 ; read only
    6C 6F FC ; read only
    6C 70 00 ; read only
    6C 71 4C ; read only
    6C 72 47 ; read only
    6C 73 20 ; read only
    6C 74 54 ; read only
    6C 75 56 ; read only
    6C 76 0A ; read only
    6C 77 20 ; read only
    6C 78 20 ; read only
    6C 79 20 ; read only
    6C 7A 20 ; read only
    6C 7B 20 ; read only
    6C 7C 20 ; read only
    6C 7D 20 ; read only
    6C 7E 01 ; read only
    6C 7F E2 ; read only
    6C 80 02 ; read only
    6C 81 03 ; read only
    6C 82 37 ; read only
    6C 83 F1 ; read only
    6C 84 4E ; read only
    6C 85 10 ; read only
    6C 86 1F ; read only
    6C 87 04 ; read only
    6C 88 13 ; read only
    6C 89 05 ; read only
    6C 8A 14 ; read only
    6C 8B 03 ; read only
    6C 8C 02 ; read only
    6C 8D 12 ; read only
    6C 8E 20 ; read only
    6C 8F 21 ; read only
    6C 90 22 ; read only
    6C 91 15 ; read only
    6C 92 01 ; read only
    6C 93 26 ; read only
    6C 94 15 ; read only
    6C 95 07 ; read only
    6C 96 50 ; read only
    6C 97 09 ; read only
    6C 98 57 ; read only
    6C 99 07 ; read only
    6C 9A 78 ; read only
    6C 9B 03 ; read only
    6C 9C 0C ; read only
    6C 9D 00 ; read only
    6C 9E 11 ; read only
    6C 9F 00 ; read only
    6C A0 B8 ; read only
    6C A1 2D ; read only
    6C A2 20 ; read only
    6C A3 C0 ; read only
    6C A4 0E ; read only
    6C A5 01 ; read only
    6C A6 40 ; read only
    6C A7 0A ; read only
    6C A8 3C ; read only
    6C A9 08 ; read only
    6C AA 10 ; read only
    6C AB 18 ; read only
    6C AC 10 ; read only
    6C AD 98 ; read only
    6C AE 10 ; read only
    6C AF 58 ; read only
    6C B0 10 ; read only
    6C B1 38 ; read only
    6C B2 10 ; read only
    6C B3 E3 ; read only
    6C B4 05 ; read only
    6C B5 03 ; read only
    6C B6 01 ; read only
    6C B7 01 ; read only
    6C B8 1D ; read only
    6C B9 80 ; read only
    6C BA 18 ; read only
    6C BB 71 ; read only
    6C BC 1C ; read only
    6C BD 16 ; read only
    6C BE 20 ; read only
    6C BF 58 ; read only
    6C C0 2C ; read only
    6C C1 25 ; read only
    6C C2 00 ; read only
    6C C3 A0 ; read only
    6C C4 5A ; read only
    6C C5 00 ; read only
    6C C6 00 ; read only
    6C C7 00 ; read only
    6C C8 9E ; read only
    6C C9 01 ; read only
    6C CA 1D ; read only
    6C CB 00 ; read only
    6C CC 72 ; read only
    6C CD 51 ; read only
    6C CE D0 ; read only
    6C CF 1E ; read only
    6C D0 20 ; read only
    6C D1 6E ; read only
    6C D2 28 ; read only
    6C D3 55 ; read only
    6C D4 00 ; read only
    6C D5 A0 ; read only
    6C D6 5A ; read only
    6C D7 00 ; read only
    6C D8 00 ; read only
    6C D9 00 ; read only
    6C DA 1E ; read only
    6C DB 02 ; read only
    6C DC 3A ; read only
    6C DD 80 ; read only
    6C DE 18 ; read only
    6C DF 71 ; read only
    6C E0 38 ; read only
    6C E1 2D ; read only
    6C E2 40 ; read only
    6C E3 58 ; read only
    6C E4 2C ; read only
    6C E5 45 ; read only
    6C E6 00 ; read only
    6C E7 A0 ; read only
    6C E8 5A ; read only
    6C E9 00 ; read only
    6C EA 00 ; read only
    6C EB 00 ; read only
    6C EC 1E ; read only
    6C ED 00 ; read only
    6C EE 00 ; read only
    6C EF 00 ; read only
    6C F0 00 ; read only
    6C F1 00 ; read only
    6C F2 00 ; read only
    6C F3 00 ; read only
    6C F4 00 ; read only
    6C F5 00 ; read only
    6C F6 00 ; read only
    6C F7 00 ; read only
    6C F8 00 ; read only
    6C F9 00 ; read only
    6C FA 00 ; read only
    6C FB 00 ; read only
    6C FC 00 ; read only
    6C FD 00 ; read only
    6C FE 00 ; read only
    6C FF B0 ; read only
    

    Thanks,

    Poornima S

  • Hi Poornima,

    I appreciate you sharing this. I've worked through all the differences and am not able to reproduce the lower noise output with your register settings.

    Are you able to provide any expected noise figures for the ADV7842 at 1080p24? Is what I am seeing unusual?

    I also note that the commercial device that I am comparing against uses an earlier revision of the ADV7842 manufactured in 2011 in Singapore, versus the 2025 Korea chip that I am using. Is there an expected variance in the ENOB across these two different dies?

    Thanks,

    Josh

  • Hi,

      To validate the chip, regardless of whether it is an older or newer version, Please check the free-run feature in the ADV7842 (The chip generates its own output video pattern internally).

      Also by using the free-run mode, we can determine whether the issue is related to clock generation or PLL lock. It also allows us to confirm that the pixel output interface is operating correctly.

    Thanks,

    Poornima S

  • When I use Free Run to output a solid color, the data is bit perfect. I only see the noise when an external analog signal is applied.

    I have swept all the DLL phase offsets, but that doesn't change the noise. I had considered phase noise issues but my thought process was to test with a solid grey field input, as a non-varying analog input signal should be immune to sampling clock issues.

  • Hi,

    Could you please probe the pixel data output pins to check whether the issue is coming from the ADV7842 or the SoC ?

    Kindly note that, the pixel bus should be stable.

    Thanks,

    Poornima S

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.