ADV7182A
Recommended for New Designs
The ADV7182A has the same pinout and is software
compatible with the ADV7182.
The ADV7182A is a versatile, one chip, multiformat video
decoder that automatically...
Datasheet
ADV7182A on Analog.com
ADV7511
Recommended for New Designs
The ADV7511 is a 225 MHz High-Definition Multimedia Interface (HDMI®) transmitter, which is ideal for home entertainment products including DVD players...
Datasheet
ADV7511 on Analog.com

Hi,
Kindly note that, In the manual pixel repeat selection case, the VIC sent in the AVI info frame will need to be set in register '0x3C'. The multiplication of the input clock must be programmed in 0x3B[6:5], and the pixel repeat value sent to the Rx must be programmed in 0x3B[4:3], Please ensure below registers at your end and let us know at https://www.analog.com/media/en/technical-documentation/evaluation-documentation/ADV7511W-Programming-Guide.pdf


Also readback using register '0x3D' and '0x3F'
Thanks,
Poornima S