KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADV7282A
Not Recommended for New Designs
The ADV7282A has the same pinout as and is software compatible with the ADV7282. The mobile industry processor interface (MIPI®) model of the ADV7282A...
Datasheet
ADV7282A on Analog.com
ADV7842
Recommended for New Designs
The ADV7842 is a dual HDMI 1.4 fast switching rReceiver with 12-Bit, 170 MHz video and graphics digitizer and 3D comb filter decoder. It is a highly flexible...
Datasheet
ADV7842 on Analog.com


Hi ,
The ADV7282A does not provide an equivalent gain adjustment option to that available in the ADV7842.
For gain adjustment on the ADV7282A, please refer to the Gain operation/ Filter section in the ADV728x Hardware Reference Manual (UG-637), which describes the luma and chroma gain control registers and their operation.
Thanks,
Ebin
Hi ,
The ADV7282A does not provide an equivalent gain adjustment option to that available in the ADV7842.
For gain adjustment on the ADV7282A, please refer to the Gain operation/ Filter section in the ADV728x Hardware Reference Manual (UG-637), which describes the luma and chroma gain control registers and their operation.
Thanks,
Ebin
Hi ADI Engineer Team ,
//For gain adjustment on the ADV7282A, please refer to the Gain operation/ Filter section in the ADV728x Hardware //Reference Manual (UG-637), which describes the luma and chroma gain control registers and their operation.
I think this your suggestion and response would not improve our our problem , please find the illustration below

We think the problem is not from Gain operation/ Filter section , we assume problem should be from sync extraction and something else .
Let me explain our encountered problem again
We are using the ADV7282A to decode an analog CVBS video stream from an FPV drone wireless receiver. The digital video is outputted via an 8-bit parallel ITU-R BT.656 interface to our backend SoC.
In our application, when the drone flies far away, the CVBS signal experiences severe static noise (snow noise) and low SNR. We noticed that a standard monitor can still show the noisy image with OSD data, but the ADV7282A frequently unstable EAV/SAV outputs to backend SoC (as shown in our attached illustrations below , left side is our benchmark , right side is using ADV7282A monitor ). This frequent switching severely disrupts the BT.656 EAV/SAV timing sequence, causing synchronization issues on our backend SoC.
Our goal: We want the ADV7282A can keep stable BT.656 EAV/SAV as much as possbile . We prefer the decoder to output pure snow/noise rather than blanking out the video stream ,keeping the BT.656 sync codes continuous.
#1 Left side : Benchmark monitor, Right side: Using ADV7282A monitor
ADV7282A monitor is kept to display noisy image ----> Okay

#2 ADV7282A outputs unstable to our backend SoC and then leads to black screen --> NG

Current key setting as below :
//DEF_VAL_AUTO_EN set to 0
//VID_SEL[3:0] set to NTSC
This problem has been troubling us for a while,we hope ADI team can give us specific recommendations as soon as you can so that we can try to see if any improvement .